Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum overheating resistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 422 subscribers
  • Views 4677 views
  • Users 0 members are here
  • help
  • overheating
  • arduino
  • relay
Related

overheating resistors

dirtdiver
dirtdiver over 14 years ago

Hi, im using the arduino to turn on a relay and complete a curcuit connecting the USB to a curcuit like this one :

 

    The IR's are TSHA203  , 100mA , Vr -5V, 180mW,image

Now one thig i dont understand is how 5 * 0.1 = 0.5 W and not 0.18 W, so I assumed that it could work on lower values like 2 volts or 50 mA and these are the maximum ones.

...But i guess i was wrong couse the resistors are overheating.Can you guys point me in the right direction?

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago +1
    You need to ask yourself "Do I need to drive with 100ma or not?". 100ma is the maximum non pulsed current allowed. As you already know, then the resistors need to dissipate about 500 mW. If the answer…
  • billabott
    billabott over 14 years ago +1
    Having watched this YouTube Video in order to learn what a "freetrack helmet" is; I have a suggestion in the form of a question. Why not use a single LED and 3 bundles of optical fiber(s)? These LEDs:…
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver +1
    interesting idea indeed, but if i use optical fiber first I would have to find optical fiber , http://www.mouser.com/Search/Refine.aspx?N=11203177
Parents
  • dirtdiver
    dirtdiver over 14 years ago

    P.S. with the Vr=5V , so if that is the maxi Voltage , i wont need a resistor, so is it? image ..I cant even find the datasheet

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    Vr is reverse voltage max, and yes - you do need the resitor.

     

    I will assume the voltage drop of the Ir's is about 2 volts, so that leaves 3 volts droped across the resistor, so 3v / 30r = 100ma, 100ma * 3v = 300mw. What size are your resistors? For this they will need to be a half watt (half  500 mw and 1/4 is 250 mw). So I can see why they may be over heating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    dirtdiver wrote:

     

    Each one should be the same? why?

    Each group, so each resitor should meassure 3.9 v drop, assumeing each resistor is identical. And each Ir should messure 1.7, again assuming they are the same values. IN your first drawing you have 3 in parallel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to R_Phoenix

    oh, yeah ok image i thought that you meant the IR and the resistor should have the same Vdrop, in my case they are identical so all 3 readings are the same

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to dirtdiver

    yes i am powering it off of the USB port, but isnt it drawing as much current as it needs (i thought that its ok as long as i dont draw more current that it can provide)

    And isnt that the resistors job here- to limit the current , how to limit the current going trough the resistor?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    dirtdiver wrote:

     

    And isnt that the resistors job here- to limit the current , how to limit the current going trough the resistor?

    Yes, you are limiting the current the LED is allowed to draw.

     

    dirtdiver wrote:

     

    well if I use a 120ohm resistor the current going trought the LED will be about 20mA , right?

    then .25mW resistors are perfect?

    Give it a try and see image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to R_Phoenix

    it seems to be rowking fine with .25W, 150 ohm resistors.Its not as bright as before image but i hope it does the trick (im making  "freetrack helmet")

    if it doesnt work i will try the 1W 30 ohm resistors and see if they preform better.But for now im happy about the fact that im powering the leds form a usb port and the computer is still on image

    Thanks for the help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    Right, the higher the resistance the less current is alowed to flow and the dimmer the LED. However it will reach a point to where it will just go out. Usually less than 15ma LEDs don't want to light, depending on the LED.

     

    Also note that to truely dim LEDs you should use PWM as mentioned by someone else. You can only dim so far with resistors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 14 years ago in reply to dirtdiver

    sorry about the post earlier dirtdiver after i read it it clearly didnt make any sense the way i worded it. image   yes the resistor regulates current.  what i was trying to say is that you should up the wattage of your resistor since the mw calculated was in the ballpark of the max for the resistor to something on the line of 2 watts or bigger.   This would allow the heat being generated from removing the current to dissipate better but keep the ohms to what ever you calculate based on your current needs.  like you stated earlier upping the ohms will decrease the brightness.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to Nate1616

    It works ok with 150 ohm, 0.25 W resistors, it gets detected by a  web cam (i havent tested it with a visible light filter yet, but i think they are bright enough as it is).

    I will post a video with the final project image - A head tracking system for PC games-it allows you to look around with your head as a controller.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 14 years ago in reply to dirtdiver

    nice project dirtdiver let us know how it goes.  post a video when its done.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to Nate1616

    http://www.youtube.com/watch?v=qTUmQz5iWOQ here is the "beta" version , the camera doent have a IR-pass filter yet and its still good without direct light coming on it

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dirtdiver
    dirtdiver over 14 years ago in reply to Nate1616

    http://www.youtube.com/watch?v=qTUmQz5iWOQ here is the "beta" version , the camera doent have a IR-pass filter yet and its still good without direct light coming on it

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    Very cool. Good job.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 14 years ago in reply to R_Phoenix

    very impressive!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to Nate1616

    thank you! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rhughes-uk
    rhughes-uk over 14 years ago in reply to dirtdiver

    Thats a terrific job. I'm off to order some parts right now.:) Please keep this forum informed of your progress.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to rhughes-uk

    Thanks, i will soon upload the video with the Leds on a hat i made, but right now im working on a DIY guitar hero drums , guitar , microphone, and ....wait for it... image  a laser harp for the guitar hero

    im also working on a cell phone detonator (not like the one on youtube couse that one WILL kill you image)