Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum overheating resistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 422 subscribers
  • Views 4693 views
  • Users 0 members are here
  • help
  • overheating
  • arduino
  • relay
Related

overheating resistors

dirtdiver
dirtdiver over 14 years ago

Hi, im using the arduino to turn on a relay and complete a curcuit connecting the USB to a curcuit like this one :

 

    The IR's are TSHA203  , 100mA , Vr -5V, 180mW,image

Now one thig i dont understand is how 5 * 0.1 = 0.5 W and not 0.18 W, so I assumed that it could work on lower values like 2 volts or 50 mA and these are the maximum ones.

...But i guess i was wrong couse the resistors are overheating.Can you guys point me in the right direction?

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago +1
    You need to ask yourself "Do I need to drive with 100ma or not?". 100ma is the maximum non pulsed current allowed. As you already know, then the resistors need to dissipate about 500 mW. If the answer…
  • billabott
    billabott over 14 years ago +1
    Having watched this YouTube Video in order to learn what a "freetrack helmet" is; I have a suggestion in the form of a question. Why not use a single LED and 3 bundles of optical fiber(s)? These LEDs:…
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver +1
    interesting idea indeed, but if i use optical fiber first I would have to find optical fiber , http://www.mouser.com/Search/Refine.aspx?N=11203177
Parents
  • billabott
    billabott over 14 years ago

    I have loaded the Freetrack v2.2 onto my Win 7 and it is running.   My CAM is a Creative Live! Cam Vista IM Webcam.  I have some Sony EyeToys around here some where.


    Initial tests indicate that in a darkened room the TSAL7400 IR LED is approx. HALF as bright as the SMD Bright Blue LED (power on) of the MC-MINI.  The skull tracks the LEDs very nicely. 

     

    Seems like it might be time to get the MS Flight Sim X re-installed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to billabott

    yes image in a dark room its great, what im going to do is put some Fully exposed and developed photographic film or Magnetic medium in floppy disks in front of the camera to block all the visible light so that the IR leds are visible on a low threshold  image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dirtdiver
    dirtdiver over 14 years ago in reply to billabott

    yes image in a dark room its great, what im going to do is put some Fully exposed and developed photographic film or Magnetic medium in floppy disks in front of the camera to block all the visible light so that the IR leds are visible on a low threshold  image