Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum overheating resistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 422 subscribers
  • Views 4661 views
  • Users 0 members are here
  • help
  • overheating
  • arduino
  • relay
Related

overheating resistors

dirtdiver
dirtdiver over 14 years ago

Hi, im using the arduino to turn on a relay and complete a curcuit connecting the USB to a curcuit like this one :

 

    The IR's are TSHA203  , 100mA , Vr -5V, 180mW,image

Now one thig i dont understand is how 5 * 0.1 = 0.5 W and not 0.18 W, so I assumed that it could work on lower values like 2 volts or 50 mA and these are the maximum ones.

...But i guess i was wrong couse the resistors are overheating.Can you guys point me in the right direction?

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago +1
    You need to ask yourself "Do I need to drive with 100ma or not?". 100ma is the maximum non pulsed current allowed. As you already know, then the resistors need to dissipate about 500 mW. If the answer…
  • billabott
    billabott over 14 years ago +1
    Having watched this YouTube Video in order to learn what a "freetrack helmet" is; I have a suggestion in the form of a question. Why not use a single LED and 3 bundles of optical fiber(s)? These LEDs:…
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver +1
    interesting idea indeed, but if i use optical fiber first I would have to find optical fiber , http://www.mouser.com/Search/Refine.aspx?N=11203177
  • e14 Contributor
    e14 Contributor over 14 years ago

    You need to ask yourself "Do I need to drive with 100ma or not?". 100ma is the maximum non pulsed current allowed. As you already know, then the resistors need to dissipate about 500 mW. If the answer is "Yes", then buy ceramic resistors of the value required, but with at least a 2 watt rating.....they will still get warm though and may need some cooling if enclosed.

     

    The Arduino should be able to pulse the output pin and use a PWM method to control the brightness and to actually reduce the power needed to go through the LED.

     

    To learm more look here:- http://arduino.cc/it/Tutorial/PWM

     

    This may or not be appropiate for your application of course, only you know that.

     

    regards

     

    Andy

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to R_Phoenix

    oh, yeah ok image i thought that you meant the IR and the resistor should have the same Vdrop, in my case they are identical so all 3 readings are the same

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to e14 Contributor

    Do you mean that i could drive the ir led with  ..say..50mA , which would mean that the voltage drop is going to be about 3.6V, given the 180mW of the LED,wont that hurt the LED?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    Depending on your needs, but you don't always have to power your LEDs with the max amount of current specified in the sheet - just don't go over.

     

    For example I have several projects that I use 2K 1/8 watt resistors on my power indicator LEDs simply because using the calculated resistor of 680 ohm 1/2 watt makes the LED way to bright. Plus I like to consume as little power as possible, allowing me to use smaller wattage resistors.

    Like a mentioned earlier, try a 100 ohm or even a 500 ohm resistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to dirtdiver

    yes i am powering it off of the USB port, but isnt it drawing as much current as it needs (i thought that its ok as long as i dont draw more current that it can provide)

    And isnt that the resistors job here- to limit the current , how to limit the current going trough the resistor?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to R_Phoenix

    well if I use a 120ohm resistor the current going trought the LED will be about 20mA , right?

    then .25mW resistors are perfect?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    dirtdiver wrote:

     

    And isnt that the resistors job here- to limit the current , how to limit the current going trough the resistor?

    Yes, you are limiting the current the LED is allowed to draw.

     

    dirtdiver wrote:

     

    well if I use a 120ohm resistor the current going trought the LED will be about 20mA , right?

    then .25mW resistors are perfect?

    Give it a try and see image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to R_Phoenix

    it seems to be rowking fine with .25W, 150 ohm resistors.Its not as bright as before image but i hope it does the trick (im making  "freetrack helmet")

    if it doesnt work i will try the 1W 30 ohm resistors and see if they preform better.But for now im happy about the fact that im powering the leds form a usb port and the computer is still on image

    Thanks for the help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    Right, the higher the resistance the less current is alowed to flow and the dimmer the LED. However it will reach a point to where it will just go out. Usually less than 15ma LEDs don't want to light, depending on the LED.

     

    Also note that to truely dim LEDs you should use PWM as mentioned by someone else. You can only dim so far with resistors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 14 years ago in reply to dirtdiver

    sorry about the post earlier dirtdiver after i read it it clearly didnt make any sense the way i worded it. image   yes the resistor regulates current.  what i was trying to say is that you should up the wattage of your resistor since the mw calculated was in the ballpark of the max for the resistor to something on the line of 2 watts or bigger.   This would allow the heat being generated from removing the current to dissipate better but keep the ohms to what ever you calculate based on your current needs.  like you stated earlier upping the ohms will decrease the brightness.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>