Arduino Forum Have a question on Arduino? Ask our expert Simon Monk
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
  • Replies 437 replies
  • Subscribers 430 subscribers
  • Views 15293 views
  • Users 0 members are here
Related

Have a question on Arduino? Ask our expert Simon Monk

patkelly
patkelly over 13 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

 

 

 

Expertise: imageArduino, .NET Gadgeteer, IOIO, embedded computing, open source hardware


About Simon: Simon is an author, writing books for TAB/McGraw-Hill and O'Reilly. He is best known for his Arduino books: 'Programming Arduino' and '30 Arduino Projects for the Evil Genius'.

 

Simon has a BSc. in Cybernetics and Computer Science and a PhD. in Software Engineering. He spent several years as an academic before he returned to industry, co-founding the mobile software company Momote Ltd.

 

If you need help on anything about Arduino, please post your question here!


 

If your not already, you'll need to login or register to ask your question - just click reply

 

The specified item was not found.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 12 years ago in reply to aml +2
    Aml I presume you have set the board to UNO under tools, along with the Com port. Have you tried at least the first 10 bullet point s under the link see http:// (You can also select it under hlep on the…
  • simon.monk
    simon.monk over 13 years ago in reply to Former Member +1
    @ jagadeshwaran http://arduino.cc/en/Hacking/Bootloader?from=Main.Bootloader
  • simon.monk
    simon.monk over 13 years ago in reply to Former Member +1
    @ang. This isn't really a task for an Arduino. It does not have nearly enough memory to store a whole image and manipulate it like that. I would not be surprised to find some PC application that would…
Parents
  • Former Member
    Former Member over 13 years ago

    I am converting my remote controlled golf cart to follow me on golf course.

    It is exactly like the build that Benjamin Heck did on episode 38, Robo luggage.

    I already have Adruino uno, transducers and receivers and Mosef. I am a

    automotive technician for 20 years now. But new to putting electronics together

    and coding. Any help on the build would be greatly appreciated. Carl

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    I need to know how to interface with an ultrasonic sound sensor and the program to write to use it in Arduino Uno.

    i want to build a robotic car, can you give me any ideas?

    thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    what are shift registers? how to use them ? what are the applications?

    what is a flip-flop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    how to use the uln 2003 darlington transistor array?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dmaruska
    dmaruska over 13 years ago in reply to Former Member

    To use the ULN2003 (http://www.ti.com/product/uln2003a) you will drive the inputs (1 - 7) with a digital line from Arduino or other MCU.  Matching output pins will interface with hi voltage/current device.  Pin 8 is ground (DC).  Pin 9 is a Test/Turn on ALL pin.  THis must be left floating (No connect) or pulled HI. or connect to a pull up and toggle with a digital pin or pushbutton to ground.  Be aware of the current limitations of each channel and entire package.  If you need more current draw than one channel can handle, you can tie two or more port together.

     

    Regards,

     

    Dave M.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 13 years ago in reply to Former Member

    Hi Shelton,

    I bought an HC-SR04 ultrasonic sound sensor off eBay a while back and found that I could just connect up the lines (gnd=gnd, vcc=5v, trig=D12 and echo=D13) and run the demo. super easy. I think the listing included a link to download the library.

    Here is a place to buy it too, and they include a link to the library, as well as a bit of an explanation: http://letsmakerobots.com/node/30209

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • simon.monk
    simon.monk over 13 years ago in reply to Former Member

    Any question that starts 'what is' probably just needs a trip to Wikipedia image

     

    As far as shift registers go, a common usage with an Arduino is to have a serial-in-parallel out shift register to drive lots of LEDs.

     

    See this: http://www.codeproject.com/Articles/144606/Arduino-Platform-Working-with-Shift-Registers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to simon.monk

    how about I start off with a simple line following robot?

    what do i need to know to make one?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 13 years ago in reply to Former Member

    Hi Shelton,

     

    I noticed that you can buy a line follower sensor on eBay: http://www.ebay.ca/itm/Arduino-Infrared-Line-Track-Follower-Sensor-Shield-/200659792466?pt=LH_DefaultDomain_0&hash=item2eb8417252

    You can probably buy similar things in many other places too.

     

    You would still need the basic drivable base, which can be bought in kits as well, or you can hack a remote controlled toy car, which is often a lot more affordable.

    Here is someone who did that: http://www.instructables.com/id/Arduino-motor-drives-cheap-toy-car/

     

    I bought a toy RC Hummer a few months ago for just 9 bucks for exactly that reason image

     

    So maybe step one could be to get an Arduino controlled car going. You could even just follow that instructable to get to that point. And then add the line following bit.

     

    Good luck, hope it goes well. post some pictures image

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sheltoncyril
    sheltoncyril over 13 years ago in reply to ntewinkel

    I actually live in India so these are worth a lot of cash,for the price of one line follower sensor i could byy an arduino so are there any ways to make it cheaper??

    like build it using ldrs and leds?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • sheltoncyril
    sheltoncyril over 13 years ago in reply to ntewinkel

    I actually live in India so these are worth a lot of cash,for the price of one line follower sensor i could byy an arduino so are there any ways to make it cheaper??

    like build it using ldrs and leds?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • sheltoncyril
    sheltoncyril over 13 years ago in reply to sheltoncyril

    btw what is a flip-flop in computer terms?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dmaruska
    dmaruska over 13 years ago in reply to sheltoncyril

    A Flip Flop is a IC (Chip) that will have two states for a given input.  When toggled, the output pins will trade states or Flip Flop states. Switch from hi to lo or one to zero, and vice versa.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 13 years ago in reply to sheltoncyril

    Hi Shelton,

     

    Yes, it should be possible to build your own.

    This blog shows details on what they did to make a line following robot, and includes a diagram of how the sensor works, with a circuit diagram.

    http://www.ermicro.com/blog/?p=1097

     

    Hope that helps image

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sheltoncyril
    sheltoncyril over 13 years ago in reply to ntewinkel

    thanks a lot !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sheltoncyril
    sheltoncyril over 13 years ago in reply to sheltoncyril

    i also have an arduino, can it be used to make a line followin robot??

    an arduino uno