Arduino
  • Products
  • More
Arduino
Arduino Forum Have a question on Arduino? Ask our expert Simon Monk
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 437 replies
  • Subscribers 445 subscribers
  • Views 20494 views
  • Users 0 members are here
Related

Have a question on Arduino? Ask our expert Simon Monk

patkelly
patkelly over 14 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

 

 

 

Expertise: imageArduino, .NET Gadgeteer, IOIO, embedded computing, open source hardware


About Simon: Simon is an author, writing books for TAB/McGraw-Hill and O'Reilly. He is best known for his Arduino books: 'Programming Arduino' and '30 Arduino Projects for the Evil Genius'.

 

Simon has a BSc. in Cybernetics and Computer Science and a PhD. in Software Engineering. He spent several years as an academic before he returned to industry, co-founding the mobile software company Momote Ltd.

 

If you need help on anything about Arduino, please post your question here!


 

If your not already, you'll need to login or register to ask your question - just click reply

 

The specified item was not found.

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 13 years ago in reply to aml +2
    Aml I presume you have set the board to UNO under tools, along with the Com port. Have you tried at least the first 10 bullet point s under the link see http:// (You can also select it under hlep on the…
  • simon.monk
    simon.monk over 14 years ago in reply to e14 Contributor +1
    @ jagadeshwaran http://arduino.cc/en/Hacking/Bootloader?from=Main.Bootloader
  • simon.monk
    simon.monk over 14 years ago in reply to e14 Contributor +1
    @ang. This isn't really a task for an Arduino. It does not have nearly enough memory to store a whole image and manipulate it like that. I would not be surprised to find some PC application that would…
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    About Arduino IDE

    I am using:

    Ubuntu with Arduino IDE 1.0.1.

     

    I have an Arduino ethernet board.

     

    Loading the "webserver" sketch and compiling I get a couple failures:

    Quote

    /usr/share/arduino/libraries/Ethernet/Ethernet.cpp: In member function ‘void EthernetClass::begin(uint8_t*, IPAddress, IPAddress, IPAddress, IPAddress)’:

    /usr/share/arduino/libraries/Ethernet/Ethernet.cpp:64: fout: no matching function for call to ‘W5100Class::setIPAddress(IPAddress::<anonymous union>&)’

    /usr/share/arduino/libraries/Ethernet/utility/w5100.h:392: note: kandidaten zijn: void W5100Class::setIPAddress(uint8_t*)

    /usr/share/arduino/libraries/Ethernet/Ethernet.cpp:65: fout: no matching function for call to ‘W5100Class::setGatewayIp(IPAddress::<anonymous union>&)’

    /usr/share/arduino/libraries/Ethernet/utility/w5100.h:368: note: kandidaten zijn: void W5100Class::setGatewayIp(uint8_t*)

    /usr/share/arduino/libraries/Ethernet/Ethernet.cpp:66: fout: no matching function for call to ‘W5100Class::setSubnetMask(IPAddress::<anonymous union>&)’

    /usr/share/arduino/libraries/Ethernet/utility/w5100.h:376: note: kandidaten zijn: void W5100Class::setSubnetMask(uint8_t*)

    quote

     

    What is gone wrong. I have not make changes to the sketch. I just install that IDE including all other files.

    The same problem with other ethernet sketches.

     

    Thanks for your time.

    Happy sunday.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I dont understand the concept of booleans and how to use them.and also can you explain to me how to use a 7 segment display??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • simon.monk
    simon.monk over 14 years ago in reply to e14 Contributor

    @shelton. Well, Booleans are values that can only have a value of either true or false.

     

    so (a > 10) is called a Boolean expression because if 'a' is greater than 10, it gives you a true otherwise it gives you a false.

     

    you might use that in an 'if' like this:

     

    if (a > 10)

    {

       Serial.println("Too Big");

    }

     

    In Arduino C, you can get away with using ints instead of the 'boolean' type, in which case 'true' is represented as 1 and 'false' as 0.

     

    so the following statement would always get inside the 'if'

     

    if (1)

    {

      Serial.println("Too Big");

    }

     

    and is the same as writing:

     

    if (true)

    {

      Serial.println("Too Big");

    }

     

    For chapter and verse on this, see http://en.wikipedia.org/wiki/Boolean_data_type

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • simon.monk
    simon.monk over 14 years ago in reply to e14 Contributor

    @shelton. Well, Booleans are values that can only have a value of either true or false.

     

    so (a > 10) is called a Boolean expression because if 'a' is greater than 10, it gives you a true otherwise it gives you a false.

     

    you might use that in an 'if' like this:

     

    if (a > 10)

    {

       Serial.println("Too Big");

    }

     

    In Arduino C, you can get away with using ints instead of the 'boolean' type, in which case 'true' is represented as 1 and 'false' as 0.

     

    so the following statement would always get inside the 'if'

     

    if (1)

    {

      Serial.println("Too Big");

    }

     

    and is the same as writing:

     

    if (true)

    {

      Serial.println("Too Big");

    }

     

    For chapter and verse on this, see http://en.wikipedia.org/wiki/Boolean_data_type