Arduino
  • Products
  • More
Arduino
Arduino Forum Hacking Power Supply
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 419 subscribers
  • Views 1385 views
  • Users 0 members are here
Related

Hacking Power Supply

billabott
billabott over 14 years ago

I am taking the plunge and building a Work Bench Power Supply from a PC Desktop power supply.

The guy in the video suggest that a approximate 0.5 amp load be put on the 5 volt rail (12 volt rail on newer) of the switching PS in order to stabilize it.

 

This diagram shows how he suggests putting it together.

 

What say you?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago in reply to billabott +2
    Of the dozens of PC ATX-type power supplies I've used in analog, digital, and electrochemical circuits, I've never needed to add a "stabilizing" resistor. Basically, ground out the green wire, and the…
  • R_Phoenix
    R_Phoenix over 14 years ago +2
    The resistor isn't to stabilize the PSU, but rather give the system a dummy load on the 5v that helps "pull up" the 12. Taking the green wire to ground will still turn it on, but then messure the voltage…
  • terryking
    terryking over 14 years ago in reply to R_Phoenix +1
    Power resistors are hard to find. Just use a 12V Automotive tail light / side light bulb on the 5V supply. It will be bright enough to function as a "Pilot light" and will last almost forever at 5V...…
Parents
  • R_Phoenix
    R_Phoenix over 14 years ago

    The resistor isn't to stabilize the PSU, but rather give the system a dummy load on the 5v that helps "pull up" the 12.

    Taking the green wire to ground will still turn it on, but then messure the voltage with a meter. It will most likly be under 12 volts, something like 11.7 volts instead. Also you will notice that about an amp of draw on the 12 volt will trigger the crowbar and shut it down with no load on the 5v rail.

     

    The resistor isn't "needed", but it is suggested.

     

    Here's mine,

    http://www.jassper.com/other/project.pdf

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • terryking
    terryking over 14 years ago in reply to R_Phoenix

    Power resistors are hard to find. Just use a 12V Automotive tail light / side light bulb on the 5V supply.

     

    It will be bright enough to function as a "Pilot light" and will last almost forever at 5V... 

     

    ...works on every AT / ATX supply I've used....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Anonymous-58970
    Anonymous-58970 over 14 years ago in reply to terryking

    12v automotive tail light iv never thought of that terry king il do that to my project and give it old tube circuits feel as well

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Anonymous-58970
    Anonymous-58970 over 14 years ago in reply to terryking

    12v automotive tail light iv never thought of that terry king il do that to my project and give it old tube circuits feel as well

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • billabott
    billabott over 14 years ago in reply to Anonymous-58970

    Q:  What is the normal range (or average) for current draw on a vacuum tube heater element.

    I am trying to determine if there is a potential of using the VTs in lieu of power resistors.

     

    A:  Wikipedia states that tubes like 12BA6, 12BE6 are 12.6 volts.

     

    Here is a fun Vacuum Tube site that indicates the heater of  12B4A draws 12.6/6.3 V, 0.3/0.6 A.

     

    Conclusion: I would need 2 vacuum tubes and sockets to put the approx. 0.6 amp load on the  12 volt rail of  my "Steam Punk" power supply.

    ( I have plenty of tubes; so I will have to find some new/nos sockets for them.)