Arduino Forum Hacking Power Supply
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
  • Replies 9 replies
  • Subscribers 404 subscribers
  • Views 936 views
  • Users 0 members are here
Related

Hacking Power Supply

billabott
billabott over 13 years ago

I am taking the plunge and building a Work Bench Power Supply from a PC Desktop power supply.

The guy in the video suggest that a approximate 0.5 amp load be put on the 5 volt rail (12 volt rail on newer) of the switching PS in order to stabilize it.

 

This diagram shows how he suggests putting it together.

 

What say you?

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 13 years ago in reply to billabott +2
    Of the dozens of PC ATX-type power supplies I've used in analog, digital, and electrochemical circuits, I've never needed to add a "stabilizing" resistor. Basically, ground out the green wire, and the…
  • R_Phoenix
    R_Phoenix over 13 years ago +2
    The resistor isn't to stabilize the PSU, but rather give the system a dummy load on the 5v that helps "pull up" the 12. Taking the green wire to ground will still turn it on, but then messure the voltage…
  • terryking
    terryking over 13 years ago in reply to R_Phoenix +1
    Power resistors are hard to find. Just use a 12V Automotive tail light / side light bulb on the 5V supply. It will be bright enough to function as a "Pilot light" and will last almost forever at 5V...…
Parents
  • billabott
    billabott over 13 years ago

    Hooray for Harbor Freight and Ryobi Power tools!

    I finally used my Ryobi DP120 drill press and knock out punch kit.

    First I had to drill a 1/2" hole in the power supply lid, then knock it out

    to 3/4", then dremeled down the rough edge.  It is perfect.  Looked thru my TV repairman's collection of V-tubes to find a good looking Tung-Sol (even says Made in the USA) 9 pin 12xx7.  I am only going to hook up the heater.  It will light up when the switch is on!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • billabott
    billabott over 13 years ago

    Hooray for Harbor Freight and Ryobi Power tools!

    I finally used my Ryobi DP120 drill press and knock out punch kit.

    First I had to drill a 1/2" hole in the power supply lid, then knock it out

    to 3/4", then dremeled down the rough edge.  It is perfect.  Looked thru my TV repairman's collection of V-tubes to find a good looking Tung-Sol (even says Made in the USA) 9 pin 12xx7.  I am only going to hook up the heater.  It will light up when the switch is on!