Arduino
  • Products
  • More
Arduino
Arduino Forum Hacking Power Supply
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 419 subscribers
  • Views 1383 views
  • Users 0 members are here
Related

Hacking Power Supply

billabott
billabott over 14 years ago

I am taking the plunge and building a Work Bench Power Supply from a PC Desktop power supply.

The guy in the video suggest that a approximate 0.5 amp load be put on the 5 volt rail (12 volt rail on newer) of the switching PS in order to stabilize it.

 

This diagram shows how he suggests putting it together.

 

What say you?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago in reply to billabott +2
    Of the dozens of PC ATX-type power supplies I've used in analog, digital, and electrochemical circuits, I've never needed to add a "stabilizing" resistor. Basically, ground out the green wire, and the…
  • R_Phoenix
    R_Phoenix over 14 years ago +2
    The resistor isn't to stabilize the PSU, but rather give the system a dummy load on the 5v that helps "pull up" the 12. Taking the green wire to ground will still turn it on, but then messure the voltage…
  • terryking
    terryking over 14 years ago in reply to R_Phoenix +1
    Power resistors are hard to find. Just use a 12V Automotive tail light / side light bulb on the 5V supply. It will be bright enough to function as a "Pilot light" and will last almost forever at 5V...…
Parents
  • billabott
    billabott over 14 years ago

    New Question:  The inrush current for the 12xx7 valve heater is too large and the PC power supply is shutting itself down.  I have some NTC thermistors (100 ohm, 450mW max.) which (according to my understanding of the data sheet) cannot handle the power when the heater is full on:  12.6V @ 150mA.

     

    I have two options that I know of:

    Opt A:  Replace with a 6.3V @ 300mA valve and series resistor ~20 ohms (three 60 ohm 5 watt in parallel)

    Opt B:  Purchase something like a 3 watt 10 ohm NTC thermistor and put it in series with the heater.

     

    Exactly what use is made of these low power thermistors?  Please tell me there is a way to use it with a power transistor to accomplish my goal and describe that circuit if you please.  Maybe the only answer is use as a temperature monitor.

     

    P.S.  While attempting to work this out for myself I came up with the following:  low power thermistor with series 1/4 watt resistor feeding the base of a PNP transistor which controls the current thru the heater coil.  Let's assume the power PNP (has to deliver 2 watts Max.) has an  gain factor of only 10 then the most current that needs to come up thru the base is 15 mA. Thus, the base leg  would have a minimum resistance of about 800 ohms.   Do I want the starting resistance to be 900  or 1800 ohms (using 1K thermistor)?  I cannot imagine 15mA heating the thermistor up very quickly ( I could be wrong about that and it would be a good thing.) and find it even harder thinking that 7 mA would have any effect at all.  Seems like a good time to experiment! 

     

    P.P.S. Found some interesting thermistor application notes here.              

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • billabott
    billabott over 14 years ago

    New Question:  The inrush current for the 12xx7 valve heater is too large and the PC power supply is shutting itself down.  I have some NTC thermistors (100 ohm, 450mW max.) which (according to my understanding of the data sheet) cannot handle the power when the heater is full on:  12.6V @ 150mA.

     

    I have two options that I know of:

    Opt A:  Replace with a 6.3V @ 300mA valve and series resistor ~20 ohms (three 60 ohm 5 watt in parallel)

    Opt B:  Purchase something like a 3 watt 10 ohm NTC thermistor and put it in series with the heater.

     

    Exactly what use is made of these low power thermistors?  Please tell me there is a way to use it with a power transistor to accomplish my goal and describe that circuit if you please.  Maybe the only answer is use as a temperature monitor.

     

    P.S.  While attempting to work this out for myself I came up with the following:  low power thermistor with series 1/4 watt resistor feeding the base of a PNP transistor which controls the current thru the heater coil.  Let's assume the power PNP (has to deliver 2 watts Max.) has an  gain factor of only 10 then the most current that needs to come up thru the base is 15 mA. Thus, the base leg  would have a minimum resistance of about 800 ohms.   Do I want the starting resistance to be 900  or 1800 ohms (using 1K thermistor)?  I cannot imagine 15mA heating the thermistor up very quickly ( I could be wrong about that and it would be a good thing.) and find it even harder thinking that 7 mA would have any effect at all.  Seems like a good time to experiment! 

     

    P.P.S. Found some interesting thermistor application notes here.