Arduino
  • Products
  • More
Arduino
Arduino Forum Error in sketch code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 418 subscribers
  • Views 4964 views
  • Users 0 members are here
Related

Error in sketch code

e14 Contributor
e14 Contributor over 13 years ago

I am trying to learn to write some code for my BCD clock project.  Before doing the actual clock code I wired up 7 LEDs on my breadboard with 7 resistors.

Then I ran wires from each LED to a digital pin on the Arduino UNO. Specifically pins 7 to 13.

 

Then I wrote some code and tried to upload it but it is flagging 3 errors and I can't see where it is wrong. Probably something that I am missing as a newbie. The errors are as follows:

 

BoardTest:57: error: expected `;' before '{' token

BoardTest:64: error: expected `;' before '{' token

BoardTest:68: error: expected `;' before '{' token

 

The code is as follows:

 

 

// Short sketch to see if breadboard and UNO is properly wired.

 

int led1=7;

int led2=8;

int led3=9;

int led4=10;

int led5=11;

int led6=12;

int led7=13;

 

int seconds=0

 

void setup(){

  ledMode(led1, OUTPUT);

  ledMode(led2, OUTPUT);

  ledMode(led3, OUTPUT);

  ledMode(led4, OUTPUT);

  ledMode(led5, OUTPUT);

  ledMode(led6, OUTPUT);

  ledMode(led7 OUTPUT);

}

 

void loop(){

  seconds++;

    If(seconds == 1){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 2){

      digitalWrite(led2, HIGH);

      digitalWrite(led1, LOW);

      delay(1000);

    }

  If(seconds == 3){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 4){

      digitalWrite(led3, HIGH);

      digitalWrite(led2, LOW);

      digitalWrite(led1, LOW);

      delay(1000);

    }

    If(seconds == 5){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 6){

      digitalWrite(led2, HIGH);

      digitalWrite(led1, LOW);

      delay(1000);

    }

    If(seconds == 7){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 8){

      digitalWrite(led4, HIGH);

      digitalWrite(led3, LOW);

      digitalWrite(led2, LOW);

      digitalWrite(led1, LOW);

      delay(1000);

    }

    If(seconds == 9){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 10){

      digitalWrite(led2, HIGH);

      digitalWrite(led1, LOW);

      delay(1000);

      digitalWrite(led1, LOW);

      digitalWrite(led2, LOW);

      digitalWrite(led3, LOW);

      digitalWrite(led4, LOW);

  seconds=0;

    }

}

 

 

 

Any help appreciated.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    John, Are those the only errors you're seeing? It looks to me that on line 11, you are missing a semicolon at the end of the line: int seconds=0 and on line 20, you are missing a comma after led7 ledMode…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor +1
    John, A table is just a fancy name for array, although in some languages it might be a fancy type of array such as an associative array. If you have 10 digits, each involving 4 led settings, you might…
  • billabott
    billabott over 13 years ago

    Hi JohnC.  Good attempt.  In respect to the current limits of each I/O pin,  I would suggest the need to multiplex the LEDs (only one on at a time.)  As a more correct example:

    void setup(){

    ledMode(led1, OUTPUT);

    ledMode(led2, INPUT);   // look up about writing a 1 to the input pin to put it in high impedance mode.

    ledMode(led3, INPUT);

    ledMode(led4, INPUT);   // it was stated that pinMode is preferred;  I don't know

    ledMode(led5, INPUT);   // and don't want to look it up right now.  sorry. 

    ledMode(led6, INPUT);

    ledMode(led7, OUTPUT);   //  this is the source of one of your errors  led7,

    }

     

    void loop(){

    seconds++;

     

    while(1){

       if (seconds == 1){

          digitalWrite(led1, HIGH);

          digitalWrite(led7, LOW);

          delay(10);

          digitalWrite(led7, HIGH);    //  in theory this will probably work

                                                     // use at your own risk since it is being adapted from PIC techniques

          delay(10);

          }  // fi     * really?  I am the first to note/share this technique

             //                  of marking what this closing brace matches  !?!

    ...

    if (timeToUpdateDisplay) break;

    }  // elihw     * ditto

     

    }  // pool       * ICNBI

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    John,

      Are those the only errors you're seeing?

    It looks to me that on line 11, you are missing a semicolon

    at the end of the line:

       int seconds=0

     

    and on line 20, you are missing a comma after led7

        ledMode(led7 OUTPUT);

     

    and all your "if" statements should use lowercase "if"

    instead of "If".

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to billabott

    Thanks billabott,

     

    When it comes to the actual BCD clock code it will have to have more than 1 led on at a time so I'm not sure how that would work with multiplexing. 

    You say that ledMode(led7, OUTPUT); is the problem but I don't see what the problem is?  It is writen the same as all of the other ledMode statements.

    Should I be using pinMode() rather than ledMode()?

     

     

    I was also wondering if it would be better to use the switch statement rather than multiple if statements?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Yes Coder27, you are correct.  I didn't notice the other errors because they had scrolled up and were not visible.

    This is my first attempt using the Arduino IDE and coding in 'C'.

     

    I have added the semi colon after 'seconds=0' and the comma after the (led7, OUTPUT).  As well I have changed all of the If to if.

     

    Thanks for pointing these out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    John,

      Yes, it's almost always better to use a switch statement than a long

    list of if statements that test consecutive values like you have.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Ok,  that's great!  I'll change them to the switch statement and see how that works.

     

    In my code, should I have used the pinMode() statement rather than ledMode() statement?

     

    Thanks for your help and patience.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    John,

      Yes, I believe pinMode() is what you want.

    (also be sure to remember the break statement in each branch

    of the switch statement).

     

    I would also note that sometimes there is a better way than

    a switch statement.  If all the branches of a switch statement

    are similar, or if they are all computing the value of the same

    variable, it may be better to use a table lookup rather than a

    switch statement.  This doesn't seem to apply in your example,

    but it may be helpful in the future.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 13 years ago in reply to e14 Contributor

    JohnC,

    Couple of things since you are not using a MAX7219EWGMAX7219EWG or the like, which is what most 'Duino projects will tell you to use.  I happen to have a bag of 10 of those ICs in front of me today.  To drive the LEDs the ATMEGA328 has to do all the work that the display driver chip would normally do.  You can do this without the driver chip or over heating the UNO due to excess current demands thanks to an effect called Persistance of Vision.  Have you seen those spinning LED sticks on a bicycle wheel spoke that make readable displays by turning the LEDs on and off in a controlled sequence?  Check on YouTube if you need to.

     

    You may want to familiarize yourself with the barGraph.pde example in the IDE and its tutorial on arduino.cc.

     

    The way I envision it is that the loop() does the following things:

    1. determine/acquire the digit values to be displayed,

    2. configures the pins that are required to be ON,

    3. go into a loop turning the I/O pins on and off in sequence to provide the appropriate display on the output.

    Item #3 is were a switch statements would be of use.   An interrupt (or conditional break;) upon new data available would allow the execution sequence to escape from the while(1) code block and the new digit values to be processed.  I assume you are going for a clock type output display  and that is what will cause multiple switch statements within the while(1) code block.  There are many choices to make about how best to arrange the process so it runs efficiently with the goal to minimize observable flicker.  If you don't like the nesting of code blocks then move the while(1) block into a new void DisplayDigits() function and call it.  Your choice.

     

    PS  When you want to make your project more permanent after the bugs are worked out, I recommend using strip board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 13 years ago in reply to billabott

    FYI

     

    ArduinoX: IDE for Arduino

    ArduinoX (pending a better name) is an alternative IDE for Arduino. It focuses on having a better out of the box experience than the standard IDE. It is more attractive, easier to use, and has better support for 3rd party boards.

    ArduinoX is still very alpha, but it can edit, compile, and download to several standard boards already.

    Current features include:

    • new code editor with line numbers, better color scheme, anti-aliasing, and a better default font   
    • !!!  I can't wait until everyone is using it.

     

     

    -=SyntaxMatters=-      image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 13 years ago in reply to e14 Contributor

    One thing you seem to have overlooked JohnC.

    That tiny little number in the lowest left hand corner of the IDE is the line number of the .pde being edited.  Moving the cursor to a different line changes the number.  Good for seeking out the location the error message pertains to.  Don't you agree?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>