Arduino
  • Products
  • More
Arduino
Arduino Forum Error in sketch code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 418 subscribers
  • Views 4939 views
  • Users 0 members are here
Related

Error in sketch code

e14 Contributor
e14 Contributor over 13 years ago

I am trying to learn to write some code for my BCD clock project.  Before doing the actual clock code I wired up 7 LEDs on my breadboard with 7 resistors.

Then I ran wires from each LED to a digital pin on the Arduino UNO. Specifically pins 7 to 13.

 

Then I wrote some code and tried to upload it but it is flagging 3 errors and I can't see where it is wrong. Probably something that I am missing as a newbie. The errors are as follows:

 

BoardTest:57: error: expected `;' before '{' token

BoardTest:64: error: expected `;' before '{' token

BoardTest:68: error: expected `;' before '{' token

 

The code is as follows:

 

 

// Short sketch to see if breadboard and UNO is properly wired.

 

int led1=7;

int led2=8;

int led3=9;

int led4=10;

int led5=11;

int led6=12;

int led7=13;

 

int seconds=0

 

void setup(){

  ledMode(led1, OUTPUT);

  ledMode(led2, OUTPUT);

  ledMode(led3, OUTPUT);

  ledMode(led4, OUTPUT);

  ledMode(led5, OUTPUT);

  ledMode(led6, OUTPUT);

  ledMode(led7 OUTPUT);

}

 

void loop(){

  seconds++;

    If(seconds == 1){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 2){

      digitalWrite(led2, HIGH);

      digitalWrite(led1, LOW);

      delay(1000);

    }

  If(seconds == 3){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 4){

      digitalWrite(led3, HIGH);

      digitalWrite(led2, LOW);

      digitalWrite(led1, LOW);

      delay(1000);

    }

    If(seconds == 5){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 6){

      digitalWrite(led2, HIGH);

      digitalWrite(led1, LOW);

      delay(1000);

    }

    If(seconds == 7){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 8){

      digitalWrite(led4, HIGH);

      digitalWrite(led3, LOW);

      digitalWrite(led2, LOW);

      digitalWrite(led1, LOW);

      delay(1000);

    }

    If(seconds == 9){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 10){

      digitalWrite(led2, HIGH);

      digitalWrite(led1, LOW);

      delay(1000);

      digitalWrite(led1, LOW);

      digitalWrite(led2, LOW);

      digitalWrite(led3, LOW);

      digitalWrite(led4, LOW);

  seconds=0;

    }

}

 

 

 

Any help appreciated.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    John, Are those the only errors you're seeing? It looks to me that on line 11, you are missing a semicolon at the end of the line: int seconds=0 and on line 20, you are missing a comma after led7 ledMode…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor +1
    John, A table is just a fancy name for array, although in some languages it might be a fancy type of array such as an associative array. If you have 10 digits, each involving 4 led settings, you might…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to billabott

    I think the problem here is that the error message indicating a missing

    semicolon was misleading.  The problem was a mis-capitalized keyword,

    rather than a missing semicolon.  It didn't help that previous error messages

    had scrolled off the screen, since that might lead one to believe that the

    previous if-statements were OK.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 13 years ago in reply to e14 Contributor

    http://ecx.images-amazon.com/images/I/41w7lABe%2B%2BL._SL500_AA300_.jpg

    Merry Kiss-a-Gir.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks Coder27,

     

    I have fixed all errors, converted to a switch statement and added more code so it will run from 0 seconds up to 1 minute. It compiles with no problems now.  All LEDs are working in the proper sequence and turns on the 1 minute LED when it hits 60 seconds.  Then the seconds counter drops back to zero and it starts over counting up to the next minute.

     

    This part of the project was done using the UNO because I was just trying to get some idea of coding in 'C'.

    Now that I have fugured out how to get that part of the code working I will start using my ArduinoMega2560 because it has more pins and more memory as well.

     

    Writing the code to handle the seconds, minutes and hours all the way up to 24 hours would make that switch statement quite long so I would be very interested in learning more about this table lookup that you mentioned. Where would I find a tutorial on how to code such a lookup table?

     

    Thanks.  You have been very helpful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to billabott

    Thanks billabott,

     

    I grabbed the code for that bargraph.pde and will take a look at it.  I did, in fact, notice the line counter at the bottom left and I have downloaded the ArduinoX IDE that you recommended.  I will install it tomorrow.  As I mentioned in my reply to Coder27, now that I have fugured out how to get these LEDs working in proper sequence, I am going to move it over to my ArduinoMega2560.

     

    Before going too far with it though, I am going to see if there is a way to shorten the code a bit. I'm sure that since I am just learning to coding in 'C', my sketch is probably larger than an experienced 'C' programmer would have.

     

    Thanks for all your help billabott, much appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    John,

      A table is just a fancy name for array, although in

    some languages it might be a fancy type of array such

    as an associative array.

      If you have 10 digits, each involving 4 led settings,

    you might have a struct that contains 4 boolean values for

    those leds, and then an array of 10 of these structs.

    To find the led settings for digit n, you would use n to index

    the array to lookup the struct with the 4 led settings for n.

    This would take the place of the switch statement.

     

    Here are two tutorials:

    http://embeddedgurus.com/stack-overflow/2010/01/a-tutorial-on-lookup-tables-in-c/

    http://stackoverflow.com/questions/2641473/initialize-static-array-of-structs-in-c

     

    The reason a table lookup is preferable to a switch statement

    is that it makes your code simpler, so there are fewer things

    that can go wrong.  For example, you can't forget a break statement.

    It also makes it easier to check that all the values in the table are correct

    since they are in one place rather than scattered in the switch statement.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 13 years ago in reply to e14 Contributor

    You are welcome.  You seem to be adapting and advancing quite quickly.  Feel free to read my blog  "BP 0x0004".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks Coder27,

     

    When you mentioned a 'lookup table' the first thing that came to my mind was a 'lookup table' such as in dBase which is held in a database but of course that wouldn't be possible in Arduino so it got me wondering what it was.

     

    I will take a look at those tutorials that you rcommended and see what I can come up with.  Keeping the code as short as possible is always a good thing.  image

     

    Thanks again, and have a very Merry Christmas and a Great New Year.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to billabott

    Thanks billabott,

     

    I find that choosing a project and actually trying to get it to work is a lot easier for me to learn rather than just reading a book.  Books and tutorials are very helpful of course, but hands-on gets your mind working and understanding it better.  I'm going to make a number of errors along the way but that's part of the learning process,... as long as you learn from your mistakes.  image  Certainly having some experienced people here on Element14 who are so willing to take the time and patience to help others is priceless.

     

    Merry Christmas to you and yours from my house.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Coder27,

     

    I am reading up a bit on those arrays and I have a question for you if you don't mind?

     

    Is it possible to use an array element in digitalWrite() like in the following example?

     

    digitalWrite(myArray[2], HIGH);  or   digitalWrite(myArray[2], myArray[3]);

     

    Or,... if a multi-dimensional array was used such as myArray[8][8] with, say, myArray[2] holding the pin number and the second dimension of the array [3] holding the HIGH or LOW, how would the syntax for that work?  I would think that the syntax would be incorrect to write it as

    digitalWrite(myArray[2], [3]);

     

    Don't know if my question is clear or not but,.... you might get the picture of what I am trying to do here.  I am looking at having separate arrays for seconds, minutes and hours.

     

     

    Thanks,

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    John,

      Yes, you can use an array element in digitalWrite, either as the first

    or second parameter (or both), essentially anywhere you might otherwise

    use a simple number or variable or algebraic expression.

      As you seem to understand, you can either have more than one

    single-dimensional array, sometimes called parallel arrays, or you

    can have an array of structs, or an array of arrays.

       

    > digitalWrite(myArray[2], [3]);

     

    The "[3]" isn't right.  Each parameter to digitalWrite is treated separately,

    so the "[3]" needs to have the name of the array variable in front of it,

    like you have for myArray[2], except it would probably have a different array name,

    because the second parameter of digitalWrite is the LOW/HIGH setting,

    rather than the pin number.  Read up on arrays so you are clear how it works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>