Arduino
  • Products
  • More
Arduino
Arduino Forum LX-328 - 8 Bit Digital Logic Processor with two ATmega328P MCU's
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 419 subscribers
  • Views 3209 views
  • Users 0 members are here
  • avr
  • atmega328
  • avr32
  • arduino
  • atmel
Related

LX-328 - 8 Bit Digital Logic Processor with two ATmega328P MCU's

iexpress
iexpress over 11 years ago

Hi Everyone!

 

I've been making a digital logic processor that has two ATmega328p MCU's on-board.

 

So far, I have the unit working through USB using a USB CDC protocol and have the

board processing digital logic through 7400 series logic.

 

I just got the firmware programmed into the MCU's today using a UC3A3 Xplained as the ISP through SPI

 

The board also has an LCD display, and I've started programming up a game for it called Super Micro Man

where the character is one character in size. https://www.youtube.com/watch?v=WD7Nmx1yU0E

 

Details and Specs for my LX-328 board are:

 

Two ATmega328p MCU's running on their internal RC oscillators.

 

Two of each: AND, NAND, XOR, XNOR, OR, NOT, and NOR gates for comparing 2 bytes at a time and giving one byte output that is captured into a corresponding 74hc165 shift register.

 

Two dual 2-4 line decoders

Nine 74hc165

Three 74hc164

 

Electronic Assembly DOGM163S-A 3 line FSTN display.

 

Four AT45DB651E 64mbit Adesto DataFlash on two plugin cards.

Two 64k x 1 Cypress 7Y7C187-35PC SRAM

 

Here is a demo video showing one of the MCU's working right after I uploaded firmware and bootloader to the blank MCU: http://youtu.be/KezzU8PZMIc

 

I've also attached a document describing how to program the ATmega328(p) manually through ISP with SPI from another MCU.

You simply redirect the opcodes to the target from the host MCU through USB with ChipSelect on the target's Reset pin.

 

Here's a brief on what the board does and how it is working the digital logic internally: https://www.youtube.com/watch?v=no6mcuZ7e48

imageimageimageimage

Attachments:
ATmega328CompleteProgrammingGuide.rtf
  • Sign in to reply
  • Cancel

Top Replies

  • toxxn
    toxxn over 11 years ago in reply to iexpress +1
    Communication over internet between two of these would be phenomenal idea, especially for a Mini DIY kit like I mentioned above. This could allow two or more boards to chat with one another or even play…
  • toxxn
    toxxn over 11 years ago in reply to iexpress +1
    The NES was a little more advanced, especially with custom made components and the time period which separates basic 8-bit computers and the NES is pretty significant. There is not really any reason to…
  • toxxn
    toxxn over 11 years ago in reply to iexpress +1
    I prefer a nice appearance myself, not only for as you mentioned, making it easy to maneuver, but also because I like ascetics in keeping a clean and crisp project. Appearance is not always everything…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    I am curious, What is it your trying to do with this, you don't say

     

    All the logic your replicating in the 74 series TTL chips is available in the ATMEGA328's already so I'm not sure of your goal

     

    Thanks

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to Robert Peter Oakes

    Not sure of it intended function overall, but if I had a guess, I would say a homemade 8-bit computer of his own design. It looks to be a more complex TTL CPU complete with his own upgrades, which wonderfully demonstrates the use of simple logic gates, buffers, a binary adder, registers, multiplexors, decoders, flip-flops, and more. 7400 IC's are very common in TTL CPU projects, so it is interesting seeing this approach to say the very least.

     

    Jason, could you share a little more about it and it intended function(s)?

     

    Thanks,

    Cory

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    I think it would be pretty awesome to add basic button inputs for 8-bit gaming purposes simply to add another twist to 8-bit computer projects such as this.

     

    As for Audio I have seen an example of i2s DAC with Class D Output which was an entry in a 7400 contest. As it so happens I have the link handy, maybe it could be of some use.

    http://willhb.com/?p=155

     

    As for Video, you are in some luck. I know of the ADV7125. It has three separate high speed 8-bit video DACs with a standard TTL input interface. It has additional video signal options such as composite SYNC and BLANK as well. Might be a little more than what you need, albeit could be something to check into. Here is a spreadsheet of the ADV7125; http://www.analog.com/static/imported-files/data_sheets/ADV7125.pdf

     

     

    A mini DIY kit of this would be an awesome project for anyone looking to play with and/or learn digital logic not to mention the opportunity for someone to build their own little 8-bit computer. I could see something like this being on kickstarter or even as a kit on sites such as E14 or Adafruit.

     

    Looking forward to seeing updates.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    Communication over internet between two of these would be phenomenal idea, especially for a Mini DIY kit like I mentioned above.

    This could allow two or more boards to chat with one another or even play 8-bit games together using the also mentioned button inputs idea.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • iexpress
    iexpress over 11 years ago in reply to toxxn

    SUre, it could be feasible to make a small kit preloaded with firmware so all they have to do is plug it into USB and then use an app that does the data transfer and board control. aybe I can interface an NES controller port. I believe they are 8-bit, and could check for button presses. Maybe give the lcd display a command prompt or graphical user interface With several different options.

     

    There should be enough RAM and ROM. The SPI flash has two 256 byte data buffers each giving 2046 bytes SRAM scratchpad memory. Today I will probably finish up most of the Visual Basic.Net app. i'll have it access all memories, and then work having it keep track of where it puts data into flash using a sort of binary file. This way it would save space on the SPI flash. Create a small defragmenter for it when files are deleted but let the user defrag when they want. I guess that would be a memory controller. One of the goals might be to keep everything in binary so there are no gaps in flash or filesystems.

     

    Should have the majority of the board finished in a day or two, then can add onto it from there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    You are correct the NES was 8-bit.

    The NTSC version had a 8-bit Microprocessor which ran at a 1.79 MHz clock rate, contained 2KiB of onboard work RAM, and 2 KiB of VRAM, 28bytes of pallette ram and 256 bytes of OAM for it's custom-made PPU (picture processing unit). The system supported up to 32 KiB of program ROM, which could be expanded by a process of bank switching. The games themselves varied in memory but the most common ran around 130-400KiB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iexpress
    iexpress over 11 years ago in reply to toxxn

    I suppose it could be possible to put a PPU in the circuit for NTCS output along with a 6502 CPU for analog audio.

    They might be 5 volt but I think they could be controlled by a shift register. That might be fairly advanced though, it would be simpler to add an SPI based display. if there was a PPU in the circuit, some displays can take composite video as input. I could possibly create dynamic callobration where the delay value is in ram instead of rom, and could be changed by the microsecond.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    The NES was a little more advanced, especially with custom made components and the time period which separates basic 8-bit computers and the NES is pretty significant.

    There is not really any reason to go too complex with an 8-bit computer, however it is cool to see new ideas.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • iexpress
    iexpress over 11 years ago in reply to toxxn

    Right on, it would be a little difficult to add those components. I'll keep building and programming to see about getting the current hardware working a bit better. I might take a break for a bit to think on the programming aspect. It is a little complicating, especially with the additional hex chars so data gets routed correctly. I'll be in touch soon.

     

    Currently, the specs are:

     

    0xC0 Unselect Selected SPI CS

    0xC1 SPI0 Chip Select

    0xC2 SPI1 Chip Select

    0xC3 SPI2 Chip Select

    0xC4 SPI3 Chip Select

     

    0x90 SPI0 MOSI uint8_t

    0x91 SPI1 MOSI uint8_t

    0x92 SPI2 MOSI uint8_t

    0x93 SPI3 MOSI uint8_t

    0x94 Write SRAM1 LSB Address Byte uint8_t

    0x95 Write SRAM1 MSB Address Byte uint8_t

    0x96 Shift Register MOSI uint8_t

    0x97 LCD Display MOSI uint8_t

     

    0xB0 SPI0 MISO uint8_t

    0xB1 SPI1 MISO uint8_t

    0xB2 SPI2 MISO uint8_t

    0xB3 SPI3 MISO uint8_t

    0xB4 reserved

    0xB5 reserved

    0XB6 Shift Register MISO uint8_t

    0xB7 SRAM1 MISO uint8_t

     

    0xD0 Deselects all addresses

    0xD1 AddressA SRAM1 MOSI

    0xD2 AddressB SRAM1 READ/WRITE

    0xD3 AddressC SRAM1 Chip Select

    0xD4 AddressD LCD Display RS DATA COMMAND

     

    0x0 Set uint8_t

    0x1 Set uint16_t

    0x2 Set uint32_t

    0x3 Set SRAM0 Address uint8_t

    0x4 Set SDRAM0 Address uint32_t

    0x5 Set SRAM0[Address] uint8_t

    0x6 Set SDRAM0[Address] uint8_t

    0x7 Increment SRAM0 Address with Wrap-Around

    0x8 Increment SDRAM0 Address with Wrap-Around

    0x9 Data Output uint8_t

    0xA Data Input uint8_t Mode 0: Clock, Data (multiply byte by two)

    0xB Data Input uint8_t Mode 1: Data, Clock

    0XC Chip Select uint8_t

    0xD SRAM1 Controller: 0x1 Write Data High, 0x0 Write Data Low, 0x3 Output Enabled, 0x2 not used.

    0xE Toggle LCD Display RS Data/Command Pin

    0xF Extended Opcode List

     

    0xF0 Increment SRAM1 Offset with Wrap-Around

    0xF1 Increment SRAM1 Segment with Wrap-Around

     

    And tons more to come.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    It is always good to take a break once in awhile. Programming can get pretty stressful at times and there is no reason to overwork yourself. : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iexpress
    iexpress over 11 years ago in reply to toxxn

    I spent the day rewiring the board twisting groups of wires together into braids to make the appearance a little nicer. It also helped to make the board easier to get around. I placed the MCU's on the SPI bus so now the MCU's can be selected in ISP mode directly. I might hand it a boot option where users can select which device they'd like to boot from, like SPI0-SPI3, EEPOM0-EEPROM1(MCU EEPROM). This might come in handy being able to select the MCU's to read and write from EEPROM contents without disturbing each MCU's flash. I can give them the option to Save EEPROM so upgrading flash won't format the EEPROM data. There might not be a need to update flash firmware, but with access to the MCU flash, some users might be enticed to update but it could make the board inoperable. For this, I can create forbidden opcodes unless the user is in some sort of Administrator mode. This could be accomplished by a boolean, IsAdmin. If IsAdmn == true.... I'll be creating the command prompt over the next few days. There will be 6 devices the user can boot from, any of the SPI loading from 0x0000 or from either MCU EEPROM. With a list of opcode instructions available to the user, they can freely develop their own operating system contolling data flow. The other thing is you could still read and write to the boot device. Perhaps the bootloader could be 256 or 512 bytes. 1 or 2 pages in the boot section of the device. Maybe I could place a byte at the end of EEPROM in one of the MCU's that shows which device to boot from, and how many 256 byte pages the bootloader is since it can be written to 100,000 times. High 4 bits show which device to boot from, and Low 4 bits show how many pages the bootloader is. Guess it could have up to 16 pages of 256 bytes available in each page.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    I prefer a nice appearance myself, not only for as you mentioned, making it easy to maneuver, but also because I like ascetics in keeping a clean and crisp project. Appearance is not always everything, but it really does help.

     

    I like your idea of adding a boot option allowing the user to select which device they would like to boot from. I like having options rather than just being subjected to a single thing, if options are available. This is why if you use any one of my SD Cards for my Raspberry Pi's, you will find at least two OS options.. that is unless what I am working on requires only one, such as the Raspberry Pi arcade project I am working on.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    I prefer a nice appearance myself, not only for as you mentioned, making it easy to maneuver, but also because I like ascetics in keeping a clean and crisp project. Appearance is not always everything, but it really does help.

     

    I like your idea of adding a boot option allowing the user to select which device they would like to boot from. I like having options rather than just being subjected to a single thing, if options are available. This is why if you use any one of my SD Cards for my Raspberry Pi's, you will find at least two OS options.. that is unless what I am working on requires only one, such as the Raspberry Pi arcade project I am working on.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • iexpress
    iexpress over 11 years ago in reply to toxxn

    Was working on a control panel in Visual Basic.Net today to access all memories on the board. I'll be handing it an automated and a manual mode where manual mode would allow controlling the board through data entry entering hex chars, and the automated mode would operate automatically incrementing stack and instruction pointers. One more week and the majority should be finished. There's an SPI based display headed this way so I'll definitely integrate that into one of the SPI channels.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to iexpress

    Oh. This gives me an idea with what I am playing with! Windows programming hardware on remote boards. Love it. image

     

    Thanks,

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • iexpress
    iexpress over 11 years ago in reply to clem57

    Yay! I'm very excited, but I've been controlling it in real time entering hex chars through the keyboard. With the hardware working, I can go ahead and create a way to increment and retrieve data from flash or either of the MCU's EEPROM. Also working to develop some sort of command prompt, but I'll probably have to make some custom peripherals for data entry if the board is used in standalone automated mode.

     

    The board should give beginners a chance to understand the 7400 series logic with the addition of SPI-based storage solutions.

     

    Creating a user guide might take about a week, but I'll cover everything from running the board in real time using the opcodes, to creating apps that run automatically from any of the storage devices on the board. Currently there are 6 non-volatile memories, but the SPI-Flash also has two 256 byte buffers a piece available to the user.

     

    Still not sure if there is a way to access MCU SRAM in ISP programming mode, but this is how I'll be having it access Flash and EEPROM.

    Perhaps the drive labels could correspond with the devices, SPI0:\ EEPROM0:\ etc.

     

    We'll get there, it'll take about a week to finish a bootloader but the user guide will even cover this.

    For updating MCU Flash, I'll just have the VB.Net app handle ISP programming in circuit through USB CDC.

     

    No more wondering how to get code onto the MCU's that are blank and don't have their own bootloaders.

    I spent a day or two understanding how bytes are written to the ATmega328P Flash, 2 bytes per address.

    Hex files show one byte per address, but the loading address is the first address shown in the hex file.

    From there, I can have the VB.Net app upload data into either of the MCU's.

     

    I also made them removable so they can be replaced and reprogrammed very quickly.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    A new SPI display? Please do post a new picture after this has been integrated. I would love to see new changes as they are implemented.

     

    Good idea on making the MSU's removable.

    I have had a few ATmega's and even a couple 555 timers burn out on me. Having those DIP sockets really do prevent the tedious work of having to de-solder when this happens.

     

    As I mentioned before, boards like this are great educational pieces when learning not only 7400, but basic logic in general.