Arduino
  • Products
  • More
Arduino
Arduino Forum LX-328 - 8 Bit Digital Logic Processor with two ATmega328P MCU's
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 419 subscribers
  • Views 3206 views
  • Users 0 members are here
  • avr
  • atmega328
  • avr32
  • arduino
  • atmel
Related

LX-328 - 8 Bit Digital Logic Processor with two ATmega328P MCU's

iexpress
iexpress over 11 years ago

Hi Everyone!

 

I've been making a digital logic processor that has two ATmega328p MCU's on-board.

 

So far, I have the unit working through USB using a USB CDC protocol and have the

board processing digital logic through 7400 series logic.

 

I just got the firmware programmed into the MCU's today using a UC3A3 Xplained as the ISP through SPI

 

The board also has an LCD display, and I've started programming up a game for it called Super Micro Man

where the character is one character in size. https://www.youtube.com/watch?v=WD7Nmx1yU0E

 

Details and Specs for my LX-328 board are:

 

Two ATmega328p MCU's running on their internal RC oscillators.

 

Two of each: AND, NAND, XOR, XNOR, OR, NOT, and NOR gates for comparing 2 bytes at a time and giving one byte output that is captured into a corresponding 74hc165 shift register.

 

Two dual 2-4 line decoders

Nine 74hc165

Three 74hc164

 

Electronic Assembly DOGM163S-A 3 line FSTN display.

 

Four AT45DB651E 64mbit Adesto DataFlash on two plugin cards.

Two 64k x 1 Cypress 7Y7C187-35PC SRAM

 

Here is a demo video showing one of the MCU's working right after I uploaded firmware and bootloader to the blank MCU: http://youtu.be/KezzU8PZMIc

 

I've also attached a document describing how to program the ATmega328(p) manually through ISP with SPI from another MCU.

You simply redirect the opcodes to the target from the host MCU through USB with ChipSelect on the target's Reset pin.

 

Here's a brief on what the board does and how it is working the digital logic internally: https://www.youtube.com/watch?v=no6mcuZ7e48

imageimageimageimage

Attachments:
ATmega328CompleteProgrammingGuide.rtf
  • Sign in to reply
  • Cancel

Top Replies

  • toxxn
    toxxn over 11 years ago in reply to iexpress +1
    Communication over internet between two of these would be phenomenal idea, especially for a Mini DIY kit like I mentioned above. This could allow two or more boards to chat with one another or even play…
  • toxxn
    toxxn over 11 years ago in reply to iexpress +1
    The NES was a little more advanced, especially with custom made components and the time period which separates basic 8-bit computers and the NES is pretty significant. There is not really any reason to…
  • toxxn
    toxxn over 11 years ago in reply to iexpress +1
    I prefer a nice appearance myself, not only for as you mentioned, making it easy to maneuver, but also because I like ascetics in keeping a clean and crisp project. Appearance is not always everything…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    I am curious, What is it your trying to do with this, you don't say

     

    All the logic your replicating in the 74 series TTL chips is available in the ATMEGA328's already so I'm not sure of your goal

     

    Thanks

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    I am curious, What is it your trying to do with this, you don't say

     

    All the logic your replicating in the 74 series TTL chips is available in the ATMEGA328's already so I'm not sure of your goal

     

    Thanks

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • toxxn
    toxxn over 11 years ago in reply to Robert Peter Oakes

    Not sure of it intended function overall, but if I had a guess, I would say a homemade 8-bit computer of his own design. It looks to be a more complex TTL CPU complete with his own upgrades, which wonderfully demonstrates the use of simple logic gates, buffers, a binary adder, registers, multiplexors, decoders, flip-flops, and more. 7400 IC's are very common in TTL CPU projects, so it is interesting seeing this approach to say the very least.

     

    Jason, could you share a little more about it and it intended function(s)?

     

    Thanks,

    Cory

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iexpress
    iexpress over 11 years ago in reply to toxxn

    Great guess Cory. The board is an 8-bit computer. Granted modern MCU's and CPU's handle logic internally, but I wanted to pose a challenge to myself to see if I could get something like this working.

     

    This is my first hardware project but I've added on a bunch of SPI components, each on their own dedicated line. The 64k x 1 SRAM is unique, and nicely, I am reading and writing to it using basic gpio functions while using adc pins for reading. In all data is handled by pin toggling.

     

    The board has one 8-bit input and an 8 bit output. Depending on which custom opcode comes in through the input 74hc164, one MCU handles which register receives the next incoming byte, and then it sends data on it's way to the appropriate logic gate. I have it sending the bytes out to all gates at the same time, but parallel loading one of nine 74hc165's at a time. When one is loaded, all the other output registers are 0x00 and have no effect on the one output register that has actual data.

     

    The second atmega328p handles peripheral IO, such as saving data to the four SPI flash roms, writing flash or sending data out through 8 channels or reading data into any of the 8 inputs.

     

    Even though I am more of a VB.Net programmer, it helped to understand what the C language was for. All of the components are working, even the LCD display. The hardest thing for me to do was program the application and bootloader code into the MCU flash manually by decyphering the Intel hex files to get the data and then start writing data to the appropriate locations in flash.

     

    Trouble is, I still don't have a connection to the PC for updating firmware on the MCU's so I can use the ISP interface at any time to update the program code. I do have a USB CDC connection with a UC3A3 Xplained evaluation board connected to the PC to run programming in real time in a sort of debug mode, but the opcode interrut language is a bit complicating because the unit listens for hex chars, then takes an action per letter it receives.

     

    For this board, the commands are 4 bit meaning 1 byte = 2 commands except when it requests data entry which is fed into the unit by keyboard on a host PC. You can think of the input as an SPI connection with clock and data line. implementing SPI with GPIO is a matter of toggling the data and clock pins in the right order. In my first attempt, all the values coming from SPI devices were multiplying the bytes by 0x02, even the shift registers all because I toggled the clock line first before checking if the corresponding adc pin was high before issuing clock.

     

    It was a matter of gpio_set_gpio_pin() and  gpio_clr_gpio_pin() functions where one pin is assigned SCK, MISO and MOSI along with a chip select line Per device. 8 data out lines, 8 data input lines, 4 chip selects, 8 clock lines and a 4 bit address bus that handles writing data to the SRAM just by setting an address.

     

    I gave the board 16 priliminary opcode instructions 0-F

    They set a uint8, uint16 and uint32 for SDRAM and SRAM data and addresses, select chips, write data, and read data.

     

    I'm definitely working on putting a user guide together, but in debug mode, what could be easier than just typing in hex chars to make the board do something.

     

    For example, if I wanted to read a byte from SPI Flash, I would select one of four. Selecting one deselects the others. I would enter:

    C10D190000900009000090B03

    C1 selects chip at location C1

    0D1 sets uint8 D1

    90 sends the uint byte D1 to the spi chip on C1 (SPI0)

    followed by 3 0x00 bytes sent to the chip on C1

    B0 reads a byte from SPI0 that is on C1

    3 prints the hex value of the byte read.

    C0 unselects all SPI chips setting the CS lines high.

     

    I could then store it in a temp 74hc165 by sending it with the 96 command which is Output Data Channel 7.

    9 means output while the following hex char tells it which channel to export the bye at 0-F although I was currently only using outputs 0-7.

    97 is write byte to LCD display. It's pretty unique. 0EE97 = set uint8 EE and send it to the LCD display.

     

    I'll definitely make a list of opcode commands. At the rate of developement, the list can continue of acceptable commands. In debug mode, the board listens for chars with scanf() then converts them into numbers.

     

    Outside debug mode, the whole process is automated rather than taking manual typed data entry. I can load data into ram from flash and even from MCU EEPROM by placing one MCU in ISP mode to get data with the other Atmega. We have Twice the power with two MCU's.

     

    I'll certainly be giving updates, maybe give this thing micro sdcard. Maybe making a pluging card for it as I have the SPI flash. Maybe create universal memory where interchangeable SRAM, Flash and FRAM cards could be used if the cards had the same ponout. Maybe use 8soic components. It's all very exciting.

     

    I Might even give this thing an R2R DAC for playing 8-bit audio. It is coming along nicely. I would consider things like IDE or compact flash but spi seems to be very stable with the unit.

     

    Glad you like the project. Feel free to check out my videos from the links I have posted in the topic above.

    I'll be giving updates the more features I can add on. Maybe I can even create a sort of command prompt for it. I gave it an OS name, Lilac and model number LX-328 to correspond with 32 MB of SPI flash and 8 bit operation.

     

    The first sixteen opcodes are 4-bit so one byte has two instructions in it. There is also an extended opcode list accessed by 0xF and then a set of another sixteen. It can keep going. The 16 and 32 bit variables are used to set the SDRAM address while the uint16 = uint8 to fill up the 16 bit SDRAM data with MSByte set to 0x00 per address location.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    Thank you for all the provided information Jason!

     

    When you gave the example of making it read bytes from the SPI Flash using Hex it honestly reminded me of the Apple 1 computer developed by Steve Wozniak back in 1976.

    I love your take on the 8-bit computer however and I like seeing these kinds of projects because there is always something new someone can add that just makes it that much more special while still keeping it what it is. I am defiantly interested in checking out updates you make on this project and I will certainly check out the videos you provided.

     

    What are your plans for connecting it via USB for updating the firmware rather than using an evaluation board?

    You mentioned possibly adding Micro SD and 8-bit Audio, are there any other additions you might be making, such as external display options, basic camera/ printer functions similar to that of the Gameboy camera/ printer for example, possibly analog support or another option for controller support for 8-bit games for example something similar to that of the Atari 2600 joystick?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iexpress
    iexpress over 11 years ago in reply to toxxn

    Might not be too hard expanding IO. I started making a couple games for the onboard lcd display which is pretty fun. Reading button presses might be fairly easy to implement. Perhaps I could give it an SPI color display, might have to search for the shift registers with latch to do some parallel output but still stick to the SPI standard. Audio might not be a problem, I made an 8 bit DAC once before but there just might be a 7400 series DAC, and even a VGA or composite video chip.

     

    USB-wise, I am using VB.Net to open the com port and can read/write data having full control over the board in real time sending hex chars to the board.

     

    I'll definitely keep everyone updated. Maybe even make a mini model of this board later on, possibly on shortrun PCB.

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iexpress
    iexpress over 11 years ago in reply to toxxn

    It could even be fun giving the board internet access through USB where the VB.Net app could send data across the internet talking with another like-unit if there were two boards. Could be useful for real-time messaging or data transfer and could be very secure with the range of logic gates the data could go through.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    I think it would be pretty awesome to add basic button inputs for 8-bit gaming purposes simply to add another twist to 8-bit computer projects such as this.

     

    As for Audio I have seen an example of i2s DAC with Class D Output which was an entry in a 7400 contest. As it so happens I have the link handy, maybe it could be of some use.

    http://willhb.com/?p=155

     

    As for Video, you are in some luck. I know of the ADV7125. It has three separate high speed 8-bit video DACs with a standard TTL input interface. It has additional video signal options such as composite SYNC and BLANK as well. Might be a little more than what you need, albeit could be something to check into. Here is a spreadsheet of the ADV7125; http://www.analog.com/static/imported-files/data_sheets/ADV7125.pdf

     

     

    A mini DIY kit of this would be an awesome project for anyone looking to play with and/or learn digital logic not to mention the opportunity for someone to build their own little 8-bit computer. I could see something like this being on kickstarter or even as a kit on sites such as E14 or Adafruit.

     

    Looking forward to seeing updates.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    Communication over internet between two of these would be phenomenal idea, especially for a Mini DIY kit like I mentioned above.

    This could allow two or more boards to chat with one another or even play 8-bit games together using the also mentioned button inputs idea.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • iexpress
    iexpress over 11 years ago in reply to toxxn

    SUre, it could be feasible to make a small kit preloaded with firmware so all they have to do is plug it into USB and then use an app that does the data transfer and board control. aybe I can interface an NES controller port. I believe they are 8-bit, and could check for button presses. Maybe give the lcd display a command prompt or graphical user interface With several different options.

     

    There should be enough RAM and ROM. The SPI flash has two 256 byte data buffers each giving 2046 bytes SRAM scratchpad memory. Today I will probably finish up most of the Visual Basic.Net app. i'll have it access all memories, and then work having it keep track of where it puts data into flash using a sort of binary file. This way it would save space on the SPI flash. Create a small defragmenter for it when files are deleted but let the user defrag when they want. I guess that would be a memory controller. One of the goals might be to keep everything in binary so there are no gaps in flash or filesystems.

     

    Should have the majority of the board finished in a day or two, then can add onto it from there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to iexpress

    You are correct the NES was 8-bit.

    The NTSC version had a 8-bit Microprocessor which ran at a 1.79 MHz clock rate, contained 2KiB of onboard work RAM, and 2 KiB of VRAM, 28bytes of pallette ram and 256 bytes of OAM for it's custom-made PPU (picture processing unit). The system supported up to 32 KiB of program ROM, which could be expanded by a process of bank switching. The games themselves varied in memory but the most common ran around 130-400KiB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iexpress
    iexpress over 11 years ago in reply to toxxn

    I suppose it could be possible to put a PPU in the circuit for NTCS output along with a 6502 CPU for analog audio.

    They might be 5 volt but I think they could be controlled by a shift register. That might be fairly advanced though, it would be simpler to add an SPI based display. if there was a PPU in the circuit, some displays can take composite video as input. I could possibly create dynamic callobration where the delay value is in ram instead of rom, and could be changed by the microsecond.