Arduino Forum How to program USB host shield?
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
  • Replies 10 replies
  • Subscribers 403 subscribers
  • Views 2140 views
  • Users 0 members are here
Related

How to program USB host shield?

Former Member
Former Member over 10 years ago

Hello

I need your help as soon as possible.

I have a Arduino Mega board and a USB host shield (like this : http://www.ebay.es/itm/like/261880660401?limghlpsr=true&hlpht=true&ul_noapp=true&hlpv=2&chn=ps&lpid=115&ops=true&viphx=1).

I need send some information from PC using Serial communication to Arduino mega by its programing port, and send this information by the USB host shield using Serial communication too.

It must run like a bridge, I send information from pc this information passes through the board and it is sent through the USB host shield.

 

 

PC=======>Arduino MEGA====>USB HOST SHIELD=====>OTHER MACHINE

 

 

All using serial communication.

 

 

It seems easy, but I couldn't find someone who tell me how I could do it.

I need some example code or something. It is very important because I need do it for a work.

Sorry for my English.Thanks in advanced

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago in reply to Former Member +1
    Understood - The post that Clem left has excellent information on using the USB Host Shield; especially some gotchas with clocking the data. Here is the Github link for the shield (lots of example code…
Parents
  • Former Member
    Former Member over 10 years ago

    With no more information than you have in the post it's difficult to give you an answer.  I'm assuming you want to end up sending data from a Windows or Linux PC to an Android device.  Since I don't know whether the Mega (is it a Mega, Mega 2560, or Mega ADK?) is just a data conduit or actually doing something I can't give you any help there.  I would tell you to check SainSmart's documentation and code examples on their website: SainSmart USB Host Android ADK Shield 2.0 For Arduino UNO MEGA R3 Mega2560 Duemilanove Nano Robot 3D Printing, Arduino, …

    The documentation pack I downloaded had quite a bit of sample code (including USB), and a copy of the eBook "Beginning Android ADK with Arduino".  Their website also lists compatible Android devices; which seems to be somewhat limited to those most widely used.

    Serial communication, as you're finding out, can be difficult.

     

    No need to apologize for your English.  There are plenty of posters, for whom English is their first language, whose grammar is much worse. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago

    With no more information than you have in the post it's difficult to give you an answer.  I'm assuming you want to end up sending data from a Windows or Linux PC to an Android device.  Since I don't know whether the Mega (is it a Mega, Mega 2560, or Mega ADK?) is just a data conduit or actually doing something I can't give you any help there.  I would tell you to check SainSmart's documentation and code examples on their website: SainSmart USB Host Android ADK Shield 2.0 For Arduino UNO MEGA R3 Mega2560 Duemilanove Nano Robot 3D Printing, Arduino, …

    The documentation pack I downloaded had quite a bit of sample code (including USB), and a copy of the eBook "Beginning Android ADK with Arduino".  Their website also lists compatible Android devices; which seems to be somewhat limited to those most widely used.

    Serial communication, as you're finding out, can be difficult.

     

    No need to apologize for your English.  There are plenty of posters, for whom English is their first language, whose grammar is much worse. image