Arduino
  • Products
  • More
Arduino
Arduino Forum MQTT client program not showing any results with Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 49 replies
  • Subscribers 420 subscribers
  • Views 6401 views
  • Users 0 members are here
Related

MQTT client program not showing any results with Arduino

e14 Contributor
e14 Contributor over 11 years ago

I modified the MQTT example present under MQTT library pubsubclient for Arduino.

My MQTT server address is 192.168.1.6 with port 8081.

To this MQTT server,another MQTT client in my mobile is able to connect.

But this is not working with Arduino.There is no error shown during compilation or during uploading.

Infact,I am not able to see the connection result messages such as "Connected" or "Not connected" which i given in Serial.println() in setup function.

I am resetting Arduino before uploading the program.Please let me know why this is not showing any output....

 

#include <SPI.h>

#include <Ethernet.h>

#include <PubSubClient.h>

// Update these with values suitable for your network.

byte mac[]    = {  0xDE, 0xED, 0xBA, 0xFE, 0xFE, 0xED };

byte server[] = {192, 168, 1, 6 };

//byte ip[]     = { 172, 16, 0, 100 };

 

 

void callback(char* topic, byte* payload, unsigned int length) {

  // handle message arrived

}

EthernetClient ethClient;

PubSubClient client(server, 8081, callback, ethClient);

void setup()

{

  Ethernet.begin(mac);

  if (client.connect("*")) {

     Serial.begin(9600);

    Serial.println("Connected to MQTT Server");

    client.publish("outTopic","hello world");

   // client.subscribe("inTopic");

  }

  else

  {

   Serial.println("Could not connect to MQTT Server");

  }

}

void loop()

{

  //client.loop();

 

}

  • Sign in to reply
  • Cancel

Top Replies

  • neilk
    neilk over 11 years ago in reply to e14 Contributor +3
    generk4 and organtin Hi Radhamani and Giovanni - I had 30 minutes to spare so I copied the program from comment 19 and posted it into the Arduino IDE (I am using 1.6.1), compiled and uploaded it to a genuine…
  • e14 Contributor
    e14 Contributor over 11 years ago +3
    Hi Bob, Neil and Clem, I tried LM35 Temperature sensor with MQTT Arduino sketch and it works fine for me I am sooo happy Thanks once again for your wonderful support and help
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bobcroft +2
    Hi bob,Neil,Clem and many others who have helped and guided me in this issue, I have successfully completed MQTT program and Arduino is successfully publishing and subscribing messages Next step,I am going…
Parents
  • bobcroft
    bobcroft over 11 years ago

    Radhamani,

                             you do not appear to have set an IP address for your Ethernet shield and you do not appear to be using DHCP to get an IP address.  So you are not sending anything to the MQTT server.  You can prove whether or not your   Ethernet card / shield is working once you have an IP address by either 'pinging' from a Windows 'cmd' line.  Type cmd in the Windows search box, this will bring up cmd.exe, click on that to bring up the command window and in the window type "ping 192.168.1.xx" Do not type the ""  and enter your own IP address at xx.

     

    Hope that helps

     

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bobcroft

    Thanks Bob...

    I tried the below program and connected RJ45 cable to my router.

     

    imageimage

    #include <SPI.h>

    #include <Ethernet.h>

    #include <PubSubClient.h>

     

    // Update these with values suitable for your network.

    byte mac[]    = {  0xDE, 0xED, 0xBA, 0xFE, 0xFE, 0xED };

    byte server[] = {192, 168, 1, 6 };

    byte ip[]     = { 192, 168, 1, 20 };

    byte gateway[]     = { 192, 168, 1, 1 };

    byte subnet[]     = { 255, 255, 255, 0 };

     

    void callback(char* topic, byte* payload, unsigned int length) {

      // handle message arrived

    }

     

    EthernetClient ethClient;

    //PubSubClient client(server, 8081, callback, ethClient);

    EthernetServer Eserver(80);

    void setup()

    {

      Ethernet.begin(mac,ip,gateway,subnet);

       Serial.println(Ethernet.localIP());

       if (Ethernet.begin(mac) == 0) {

        Serial.println("Failed to configure Ethernet using DHCP");

        }

      // print your local IP address:

     

     

     

    /*  if (client.connect("*")) {

         Serial.begin(9600);

        Serial.println("Connected to MQTT Server");

        client.publish("outTopic","hello world");

       // client.subscribe("inTopic");

      }

      else

      {

       Serial.println("Could not connect to MQTT Server");

      }*/

     

    }

     

     

    void loop()

    {

      //client.loop();

     

    }

     

    I uploaded the sketch without any issues.But there is no output still and no results in Serial monitor.

    I tried ping,

    C:\Users\Radhamani>ping 192.168.1.20

     

    Pinging 192.168.1.20 with 32 bytes of data:

    Reply from 192.168.1.6: Destination host unreachable.

    Reply from 192.168.1.6: Destination host unreachable.

    Reply from 192.168.1.6: Destination host unreachable.

    Reply from 192.168.1.6: Destination host unreachable.

    Ping statistics for 192.168.1.20:

        Packets: Sent = 4, Received = 4, Lost = 0 (0% loss),

     

    Results of ipconfig is:

    Wireless LAN adapter Wi-Fi:

       Connection-specific DNS Suffix  . :

       Link-local IPv6 Address . . . . . : fe80::901:3297:48ad:9e7d%3

       IPv4 Address. . . . . . . . . . . : 192.168.1.6

       Subnet Mask . . . . . . . . . . . : 255.255.255.0

       Default Gateway . . . . . . . . . : 192.168.1.1

     

    Not sure whether IP address is still not getting set for Ethernet address.

    Arduino is still not showing any output regarding Serial.println image .I am missing something here...Kindly help me....

    Let me know if you need any more details...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    Is this the exact code your using, if so then you still have most of the significant code commented out, it is probably showing green on your IDE

     

    Based on what is commented out, I'm not surprised its not showing anything

     

    for instance

     

    /*  if (client.connect("*")) {
         Serial.begin(9600);
        Serial.println("Connected to MQTT Server");
        client.publish("outTopic","hello world");
       // client.subscribe("inTopic");
      }
      else
      {
       Serial.println("Could not connect to MQTT Server");
      }*/

    will do nothing as it is all commented out

     

    Can you confirm exactly what your uploading

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Hi Peter,

    I am trying to first setup MAC and IP address for the EthernetShield .Thatswhy I have commented out the MQTT portion of code in the sketch.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Hi Peter,

    I am trying to first setup MAC and IP address for the EthernetShield .Thatswhy I have commented out the MQTT portion of code in the sketch.