Arduino
  • Products
  • More
Arduino
Arduino Forum MQTT client program not showing any results with Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 49 replies
  • Subscribers 412 subscribers
  • Views 5401 views
  • Users 0 members are here
Related

MQTT client program not showing any results with Arduino

Former Member
Former Member over 11 years ago

I modified the MQTT example present under MQTT library pubsubclient for Arduino.

My MQTT server address is 192.168.1.6 with port 8081.

To this MQTT server,another MQTT client in my mobile is able to connect.

But this is not working with Arduino.There is no error shown during compilation or during uploading.

Infact,I am not able to see the connection result messages such as "Connected" or "Not connected" which i given in Serial.println() in setup function.

I am resetting Arduino before uploading the program.Please let me know why this is not showing any output....

 

#include <SPI.h>

#include <Ethernet.h>

#include <PubSubClient.h>

// Update these with values suitable for your network.

byte mac[]    = {  0xDE, 0xED, 0xBA, 0xFE, 0xFE, 0xED };

byte server[] = {192, 168, 1, 6 };

//byte ip[]     = { 172, 16, 0, 100 };

 

 

void callback(char* topic, byte* payload, unsigned int length) {

  // handle message arrived

}

EthernetClient ethClient;

PubSubClient client(server, 8081, callback, ethClient);

void setup()

{

  Ethernet.begin(mac);

  if (client.connect("*")) {

     Serial.begin(9600);

    Serial.println("Connected to MQTT Server");

    client.publish("outTopic","hello world");

   // client.subscribe("inTopic");

  }

  else

  {

   Serial.println("Could not connect to MQTT Server");

  }

}

void loop()

{

  //client.loop();

 

}

  • Sign in to reply
  • Cancel

Top Replies

  • neilk
    neilk over 11 years ago in reply to Former Member +3
    generk4 and organtin Hi Radhamani and Giovanni - I had 30 minutes to spare so I copied the program from comment 19 and posted it into the Arduino IDE (I am using 1.6.1), compiled and uploaded it to a genuine…
  • Former Member
    Former Member over 11 years ago +3
    Hi Bob, Neil and Clem, I tried LM35 Temperature sensor with MQTT Arduino sketch and it works fine for me I am sooo happy Thanks once again for your wonderful support and help
  • Former Member
    Former Member over 11 years ago in reply to bobcroft +2
    Hi bob,Neil,Clem and many others who have helped and guided me in this issue, I have successfully completed MQTT program and Arduino is successfully publishing and subscribing messages Next step,I am going…
Parents
  • Former Member
    Former Member over 10 years ago

    #include <SPI.h>

    #include <PubSubClient.h>

    #include <Ethernet.h>

     

     

    // Pins

    // Analog 0 is the input pin

     

     

    // Variables

    const int Tempin = 0;

    int value;

    float temp,tempC;

    String pubstring;

    unsigned long time;

    char message_buffer[100];

     

     

    // Network Settings

    // MAC address of ethernet shield

    // Look for it on a sticket at the bottom of the shield.

    // Old Arduino Ethernet Shields or clones may not have a dedicated MAC address. Set any hex values here.

    byte MAC_ADDRESS[] = {  0x78, 0x45, 0xC4, 0xAA, 0xE5, 0x6F };

     

     

    // IP address of MQTT server

    //byte MQTT_SERVER[] = {0,0,0,0};

    //byte ip[] = {10,107,1,115};

    EthernetClient ethClient;

    PubSubClient client;

     

     

     

     

    void setup()

    { 

      // Initilize serial link for debugging

      Serial.begin(9600);

     

      Ethernet.begin(MAC_ADDRESS);

      Serial.print("Local IP=");

      Serial.println(Ethernet.localIP());

      client  = PubSubClient("0.0.0.0", 1883, callback, ethClient);

    }

     

     

    void loop()

    {

      if (!client.connected())

      {

        //client.connect("clientID", "mqtt_username", "mqtt_password");

        client.connect("sfo-arduino");

        client.publish("sfo/arduino/alive", "I'm alive!");

      }

      else{

        client.connect("arduino/temperature");

        Serial.println("here i am connected");

        }

     

      //tempC = dtostrf(tempF,5,2,message_buffer);

     

      // Publish sensor reading every X milliseconds

     

     

      if (millis() > (time + 5000)) {

        time = millis();

        value = analogRead(Tempin);

        temp = (value/1024.0)*5000;

        tempC = temp/10;

        pubstring = String(tempC);

         pubstring.toCharArray(message_buffer, pubstring.length() + 1);

        client.publish("arduino/temperature",message_buffer);

        //Serial.println("published!");

        //Serial.println(message_buffer);

    }

       

      // MQTT client loop processing

      client.loop();

    }

     

     

    // Handles messages arrived on subscribed topic(s)

    void callback(char* topic, byte* payload, unsigned int length) {

    }

    hey i am trying a project on reading lm35 temperature sensor and publish in a mqtt broker using arduino.. I am stuck at subscribe mid1:0 after which it starts pinging..may i know what am i doing wrong here??

     

    Thanks in advance..kindly reply asap

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to Former Member

    Did you set the server address?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 10 years ago in reply to Former Member

    Did you set the server address?

    Clem