Arduino Forum Servo Problem
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
  • Replies 7 replies
  • Subscribers 403 subscribers
  • Views 472 views
  • Users 0 members are here
  • pwm
  • servo
Related

Servo Problem

rishi2628
rishi2628 over 10 years ago

i have a custom avr atmega328 board to which two seven segment, a servo and a crystal with capacitor is attached. when only the seven segment is connected, the microcontroller works perfectly.But when i attach the servo along with the seven segment, it starts blinking very rapidly and the servo moves to the extreme end. i have programmed the servo to rotate 0 to 90 and then 90 to zero and the seven segment to show its angle. My code is fine, i have verified it using the arduino. i guess the crystal is causing some interference or there is anything else needed for the pwm operation that i am missing to use the servo. can anyone help me out...??????.....please!!!

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +4
    Where is the power for the servo coming from? A diagram of connections would help greatly. a meter showing current would help if you have one handy. Clem
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +4
    Can you provide schematic to show how everything is connected and also the sketch, this will allow us to hep you better
Parents
  • clem57
    clem57 over 10 years ago

    Where is the power for the servo coming from? A diagram of connections would help greatly. a meter showing current would help if you have one handy.

    Clem

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • rishi2628
    rishi2628 over 10 years ago in reply to clem57

    i have a nine volt battery, that i have attached to a 7805 ic. the output from this ic is connected to both the microcontroller and the servo. both are connected parallel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rishi2628
    rishi2628 over 10 years ago in reply to clem57

    i have a nine volt battery, that i have attached to a 7805 ic. the output from this ic is connected to both the microcontroller and the servo. both are connected parallel