Arduino Forum Couldn't read the transmitted string through laser on the receiver side
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
  • Replies 5 replies
  • Subscribers 392 subscribers
  • Views 398 views
  • Users 0 members are here
  • frontpage
Related

Couldn't read the transmitted string through laser on the receiver side

nivin_13101994
nivin_13101994 over 10 years ago

Hi all,

      I am a beginner to arduino trying to transfer data through LASER in arduino.but I couldn't read the transfered String and i am getting garbage values.I am using photodiode on the receiver side to detect the transmitted signal.I have connected the LASER and photodiode to Tx and Rx of two arduinos respectively.Should I use any modulation algorithms to transfer the data through LASER?? or Can it be transfered simply through Tx without any modulation??? Plz help me out

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    Most modern optical transceivers I have come across use some form of modulation as this helps to eliminate the effects of normal visible and invisible light from interfering with the signal This is exactly…
  • clem57
    clem57 over 10 years ago +1
    Do you mean infra red and not laser? Need the actual part numbers to know what specs they are. Clem PS Like this Connecting a Photoresistor to an Arduino
  • gadget.iom
    gadget.iom over 10 years ago +1
    What Serial baud rate are you using? Try lowering it to 300 or 600 and then see if you can get a result.
Parents
  • gadget.iom
    gadget.iom over 10 years ago

    What Serial baud rate are you using?

    Try lowering it to 300 or 600 and then see if you can get a result.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 10 years ago

    What Serial baud rate are you using?

    Try lowering it to 300 or 600 and then see if you can get a result.