Arduino Forum Couldn't read the transmitted string through laser on the receiver side
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
  • Replies 5 replies
  • Subscribers 392 subscribers
  • Views 398 views
  • Users 0 members are here
  • frontpage
Related

Couldn't read the transmitted string through laser on the receiver side

nivin_13101994
nivin_13101994 over 10 years ago

Hi all,

      I am a beginner to arduino trying to transfer data through LASER in arduino.but I couldn't read the transfered String and i am getting garbage values.I am using photodiode on the receiver side to detect the transmitted signal.I have connected the LASER and photodiode to Tx and Rx of two arduinos respectively.Should I use any modulation algorithms to transfer the data through LASER?? or Can it be transfered simply through Tx without any modulation??? Plz help me out

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    Most modern optical transceivers I have come across use some form of modulation as this helps to eliminate the effects of normal visible and invisible light from interfering with the signal This is exactly…
  • clem57
    clem57 over 10 years ago +1
    Do you mean infra red and not laser? Need the actual part numbers to know what specs they are. Clem PS Like this Connecting a Photoresistor to an Arduino
  • gadget.iom
    gadget.iom over 10 years ago +1
    What Serial baud rate are you using? Try lowering it to 300 or 600 and then see if you can get a result.
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    Most modern optical transceivers I have come across use some form of modulation as this helps to eliminate the effects of normal visible and invisible light from interfering with the signal

     

    This is exactly what all modern TV remote controls do, they modulate the signal with a 38Khz carrier and the receiver filters out everything except this frequency before decoding the signal

     

    like this where you have a carrier for the "0" and no carrier for the ones, there are many ways to modulate, this is just one of them

    image

     

    Hope this helps

     

    Peter

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    Most modern optical transceivers I have come across use some form of modulation as this helps to eliminate the effects of normal visible and invisible light from interfering with the signal

     

    This is exactly what all modern TV remote controls do, they modulate the signal with a 38Khz carrier and the receiver filters out everything except this frequency before decoding the signal

     

    like this where you have a carrier for the "0" and no carrier for the ones, there are many ways to modulate, this is just one of them

    image

     

    Hope this helps

     

    Peter

    • Cancel
    • Vote Up +3 Vote Down