Arduino
  • Products
  • More
Arduino
Arduino Forum Problem with Arduino Mega
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 411 subscribers
  • Views 1655 views
  • Users 0 members are here
  • mega2560
  • arduino
Related

Problem with Arduino Mega

Former Member
Former Member over 10 years ago

Hi all,

 

I own an Arduino mega 2560 and have been having problems with it recently. When I load a sketch, this error comes up :

avrdude: stk500v2_ReceiveMessage(): timeout

avrdude: stk500v2_ReceiveMessage(): timeout

 

I can't figure out what it is ( I've read that its a problem with the communication with the computer). When I plug it in the green power LED turns on and so does the orange pin 13 LED. I think that the sketches we're uploading at one point ( I'm not 100% sure as I didn't get it doing anything due to my lack of arduino knowledge ). I am on mac running OS X Yosemite.

 

Any help will be greatly appreciated!

 

thanks

 

Kelan

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 10 years ago

    Thanks for the advice, I selected the right board ans processor but still nothingimage. I think the problem is the Port, I read somewhere that is should be port " /dev/tty.usbmodem1411 " but I only have "/dev/cu". Any more ideas?

     

    Thanks

     

    p.s. the LEDs don't flash when programming

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to Former Member

    I think you need to look at udev and set one up for the Mega, Foir an example of how Arduino Playground - Udev

    The ATmega16U2 (or 8U2 in the rev1 and rev2 boards) firmware source code is available in the Arduino repository. The ATmega16U2/8U2 is loaded with a DFU bootloader, which can be activated by:

    • On Rev1 boards: connecting the solder jumper on the back of the board (near the map of Italy) and then resetting the 8U2.
    • On Rev2 or later boards: there is a resistor that pulling the 8U2/16U2 HWB line to ground, making it easier to put into DFU mode. You can then use Atmel's FLIP software (Windows) or the DFU programmer (Mac OS X and Linux) to load a new firmware. Or you can use the ISP header with an external programmer (overwriting the DFU bootloader). See this user-contributed tutorial for more information.

     

    If this does not work you may need to put back the DFU boot loader for the support chip that handles USB.  See oddWires: Repairing an Arduino Mega or Uno USB port

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 10 years ago in reply to Former Member

    I think you need to look at udev and set one up for the Mega, Foir an example of how Arduino Playground - Udev

    The ATmega16U2 (or 8U2 in the rev1 and rev2 boards) firmware source code is available in the Arduino repository. The ATmega16U2/8U2 is loaded with a DFU bootloader, which can be activated by:

    • On Rev1 boards: connecting the solder jumper on the back of the board (near the map of Italy) and then resetting the 8U2.
    • On Rev2 or later boards: there is a resistor that pulling the 8U2/16U2 HWB line to ground, making it easier to put into DFU mode. You can then use Atmel's FLIP software (Windows) or the DFU programmer (Mac OS X and Linux) to load a new firmware. Or you can use the ISP header with an external programmer (overwriting the DFU bootloader). See this user-contributed tutorial for more information.

     

    If this does not work you may need to put back the DFU boot loader for the support chip that handles USB.  See oddWires: Repairing an Arduino Mega or Uno USB port