Arduino
  • Products
  • More
Arduino
Arduino Forum Problem with Arduino Mega
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 411 subscribers
  • Views 1632 views
  • Users 0 members are here
  • mega2560
  • arduino
Related

Problem with Arduino Mega

Former Member
Former Member over 10 years ago

Hi all,

 

I own an Arduino mega 2560 and have been having problems with it recently. When I load a sketch, this error comes up :

avrdude: stk500v2_ReceiveMessage(): timeout

avrdude: stk500v2_ReceiveMessage(): timeout

 

I can't figure out what it is ( I've read that its a problem with the communication with the computer). When I plug it in the green power LED turns on and so does the orange pin 13 LED. I think that the sketches we're uploading at one point ( I'm not 100% sure as I didn't get it doing anything due to my lack of arduino knowledge ). I am on mac running OS X Yosemite.

 

Any help will be greatly appreciated!

 

thanks

 

Kelan

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 10 years ago

    Thanks for the advice, I selected the right board ans processor but still nothingimage. I think the problem is the Port, I read somewhere that is should be port " /dev/tty.usbmodem1411 " but I only have "/dev/cu". Any more ideas?

     

    Thanks

     

    p.s. the LEDs don't flash when programming

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago

    Thanks for the advice, I selected the right board ans processor but still nothingimage. I think the problem is the Port, I read somewhere that is should be port " /dev/tty.usbmodem1411 " but I only have "/dev/cu". Any more ideas?

     

    Thanks

     

    p.s. the LEDs don't flash when programming

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Former Member

    Is AVRISP the right programmer ?I know this is the default now and once I can find my Mega I will try it but that seems to be the 6 pin port from memory

     

    Regards

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to Former Member

    I think you need to look at udev and set one up for the Mega, Foir an example of how Arduino Playground - Udev

    The ATmega16U2 (or 8U2 in the rev1 and rev2 boards) firmware source code is available in the Arduino repository. The ATmega16U2/8U2 is loaded with a DFU bootloader, which can be activated by:

    • On Rev1 boards: connecting the solder jumper on the back of the board (near the map of Italy) and then resetting the 8U2.
    • On Rev2 or later boards: there is a resistor that pulling the 8U2/16U2 HWB line to ground, making it easier to put into DFU mode. You can then use Atmel's FLIP software (Windows) or the DFU programmer (Mac OS X and Linux) to load a new firmware. Or you can use the ISP header with an external programmer (overwriting the DFU bootloader). See this user-contributed tutorial for more information.

     

    If this does not work you may need to put back the DFU boot loader for the support chip that handles USB.  See oddWires: Repairing an Arduino Mega or Uno USB port

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Robert Peter Oakes

    I tried all the other programmers and nothing is working

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to Former Member

    It seems there are some issues with the wrong driver being installed.

    This link here had some useful thoughts

    http://arduino.stackexchange.com/questions/3324/arduino-compatibles-serial-port-not-showing-mac-osx

     

    Sparkfun is most likely to be with genuine Arduino products, but might help

    https://learn.sparkfun.com/tutorials/how-to-install-ftdi-drivers/mac

     

    This one here gave a whole lot of other thoughts.

    image

     

     

     

    Mark