Arduino Forum Arduino using Visual Studio
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
  • Replies 29 replies
  • Subscribers 404 subscribers
  • Views 3018 views
  • Users 0 members are here
Related

Arduino using Visual Studio

Workshopshed
Workshopshed over 10 years ago

Here's a free training course from Microsoft about using Visual Studio with the Arduino

 

https://www.microsoftvirtualacademy.com/en-US/training-courses/programming-robotic-systems-with-visual-studio-8321/?prid…

 

I'm not sure of the licensing implications but there does seem to be a free download of Visual Studio Community edition

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    Visual Studio is an excelent tool for creating AVR (Arduino and Native) applications for the ATMEGA328 chips etc. and it is free. Atmel provide a completly free version of it directly from their site and…
  • bobcroft
    bobcroft over 10 years ago +2
    Another brilliant piece of software for programming Arduino's and the various derivatives is Visual Micro. The basic version is free and runs under Atmel Studio (certainly version 6.2) or Visual Studio…
  • balearicdynamics
    balearicdynamics over 10 years ago +1
    I suggest not to use it There are other better ways and as usual MS arrives bad and later. Enrico
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    Visual Studio is an excelent tool for creating AVR (Arduino and Native) applications for the ATMEGA328 chips etc. and it is free.

     

    Atmel provide a completly free version of it directly from their site and this has been available for free for YEARS. so its not too late and Bad, maybe just not as well known.

     

    ATMEL Studio 6.1, all ready to rock and roll on AVR development

     

    Microsoft is now also on board with thier version of Arduino development but if you want to be coding like you do with the Arduino IDE then the ATMEL Studio is the one you should look at first.

     

    there is nothing wrong with the Arduino IDE, but as soon as you want to get to more complex applications you will want something like ATMEL Studio (Which as I said, is Visual Studio)

     

    Peter

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Robert Peter Oakes

    That is what I started writing in my previous post in this discussion. I am using AVR studio and it is a (free) version os visual studio very well tailored just for the AVR devices, includes support for the standard Arduino libraries, with the only problem that the sketches become unusable by the old ide. The Arduino IDE should be installed but it is just to get some configuration information, nothing more. AVR Studio is not comparable with the Arduino IDE that is a super-filtered mechanism that makes all simple and a lot not feasable at all.

     

    The big advantage of the AVR studio is that includes all the online and off line examples and documentation for the AVR chips, the possibility to program them with USE via bootloader (works with the Arduino boorloader) or direct programming with ICSP and AVR MK III (other may work but I have never saw them working really). There are lot of advantages because it is a full development environment and it can co-exist on the same PC with the standard Visual Studio for other developments (but I discourage to do this).

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Robert Peter Oakes

    That is what I started writing in my previous post in this discussion. I am using AVR studio and it is a (free) version os visual studio very well tailored just for the AVR devices, includes support for the standard Arduino libraries, with the only problem that the sketches become unusable by the old ide. The Arduino IDE should be installed but it is just to get some configuration information, nothing more. AVR Studio is not comparable with the Arduino IDE that is a super-filtered mechanism that makes all simple and a lot not feasable at all.

     

    The big advantage of the AVR studio is that includes all the online and off line examples and documentation for the AVR chips, the possibility to program them with USE via bootloader (works with the Arduino boorloader) or direct programming with ICSP and AVR MK III (other may work but I have never saw them working really). There are lot of advantages because it is a full development environment and it can co-exist on the same PC with the standard Visual Studio for other developments (but I discourage to do this).

     

    Enrico