Arduino Forum Arduino using Visual Studio
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
  • Replies 29 replies
  • Subscribers 404 subscribers
  • Views 3028 views
  • Users 0 members are here
Related

Arduino using Visual Studio

Workshopshed
Workshopshed over 10 years ago

Here's a free training course from Microsoft about using Visual Studio with the Arduino

 

https://www.microsoftvirtualacademy.com/en-US/training-courses/programming-robotic-systems-with-visual-studio-8321/?prid…

 

I'm not sure of the licensing implications but there does seem to be a free download of Visual Studio Community edition

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    Visual Studio is an excelent tool for creating AVR (Arduino and Native) applications for the ATMEGA328 chips etc. and it is free. Atmel provide a completly free version of it directly from their site and…
  • bobcroft
    bobcroft over 10 years ago +2
    Another brilliant piece of software for programming Arduino's and the various derivatives is Visual Micro. The basic version is free and runs under Atmel Studio (certainly version 6.2) or Visual Studio…
  • balearicdynamics
    balearicdynamics over 10 years ago +1
    I suggest not to use it There are other better ways and as usual MS arrives bad and later. Enrico
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    Visual Studio is an excelent tool for creating AVR (Arduino and Native) applications for the ATMEGA328 chips etc. and it is free.

     

    Atmel provide a completly free version of it directly from their site and this has been available for free for YEARS. so its not too late and Bad, maybe just not as well known.

     

    ATMEL Studio 6.1, all ready to rock and roll on AVR development

     

    Microsoft is now also on board with thier version of Arduino development but if you want to be coding like you do with the Arduino IDE then the ATMEL Studio is the one you should look at first.

     

    there is nothing wrong with the Arduino IDE, but as soon as you want to get to more complex applications you will want something like ATMEL Studio (Which as I said, is Visual Studio)

     

    Peter

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Robert Peter Oakes

    I've read somewhere (but can't recall where) that the new version 7 of the Atmel Studio will also support SAMA5D4.

    There is a Beta program running at the moment...

     

    http://atmel-studio.s3-website-us-west-2.amazonaws.com/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Jan Cumps

    Just started the install:

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Jan Cumps

    The install has finished, and I can't find the SAMA5D4 listed. I'll re-search  the information and see if it was maybe announced for 7.1...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Jan Cumps

    Hi,

    Now it's released and the beta period is over. With Atmel Studio 7.0, it should be lot easier to import sketches and work with them. You can either use the

    1. Bootloader mode with Visual Micro plugin or

    2. Debugging mode with the Atmel Studio Sketch Import feature (File -> New -> Create Project from Arduino Sketch) and the Debug Shield.

    https://www.youtube.com/watch?v=3fjrKEJCE40

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago in reply to Jan Cumps

    Hi,

    Now it's released and the beta period is over. With Atmel Studio 7.0, it should be lot easier to import sketches and work with them. You can either use the

    1. Bootloader mode with Visual Micro plugin or

    2. Debugging mode with the Atmel Studio Sketch Import feature (File -> New -> Create Project from Arduino Sketch) and the Debug Shield.

    https://www.youtube.com/watch?v=3fjrKEJCE40

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Former Member

    Correct.

     

    Excluding the option Windows 10 - that is too young (especially for the Microsoft guys) to be used seriously and proficiently - IMHO needs at least six months before a new version of Windows can be usable - Why make a lot of tricks with Visual Studio while there is the super flexible and efficient AVR Studio 6.5 and now recently release version 7? It's free, without charge and has a lot of specific advantages vs the Atmel MCU.

     

    Obviously by the point of view of the MS Guys their advantage is that - in theory - you should buy Visual Studio while AVR studio (based on Visual Studio and very well tailored) is free.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to balearicdynamics

    Visual Studio is also free for the community edition and I have been using it for months now creating Raspberry PI apps under widows 10, and running on Windows 10 IoT without any issues

     

    Atmel Studion as you said is also heavily based on Visual Studio... probably a generation behind the current Microsoft Version in order for MS to keep the "Compettitive" Edge image

     

    I have not needed to try Atmel Studio 7 yet but I will be soon, I hope they have not released a version that will not work with Windows 10 as this is being very aggressivly pushed by MS and will upset alot of folks if it wont run

     

    Has anyone tried it yet?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Robert Peter Oakes

    Hi,

    Atmel Studio is based on the latest version of Visual Studio i.e VS 2015. So it's not far behind and should work well with Windows 10. :-), without issues.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Former Member

    Just finished installing it and yet it is indeed based on the Vidual Studio 2015 framework with all the cool ATMEL add ons

     

    I will be trying it out over the next few days im sure and yes im running on Windows 10 to do all this

     

    Regards

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    Thanks for the Visual Micro mention. Just add add that upload via bootloader or hardware programmer is supported along with support for Arduino .ino files and Arduino usb/bluetooth/rf debugging image