Arduino
  • Products
  • More
Arduino
Arduino Forum Stepper motor wiring help(and a few other small questions from an instructable)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 55 replies
  • Answers 1 answer
  • Subscribers 420 subscribers
  • Views 7008 views
  • Users 0 members are here
  • wiring
  • steppers
  • arduino
Related

Stepper motor wiring help(and a few other small questions from an instructable)

gub11
gub11 over 10 years ago

This instructable really interested me, Frameless Laser Harp - 4 , but i've never worked with steppers before.  the stepper i got has 4 wires, but the stepper in the instructable has 6.  on page 2 there is a wiring guide, but that wasn't very helpful to me, i didn't really understand what i'm supposed to do with the wires.  This is the stepper i have, https://www.sparkfun.com/products/10551?gclid=Cj0KEQiApruyBRCFqoDu1pbk9rkBEiQAF8EFdVmEBorGt6koPmFkaibEpRmZ94Z6r8BWhmTqAL… .  Any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to gub11 +2 suggested
    reverse... to change direction lol now more seriously... then you wire up the stepper motor, if it is not going in the direction you expect for the command your giving then you can change the code or simply…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    Here is an excelent resource regarding steppers and how they work http://www.geckodrive.com/support.html I found this to be very helpfull in setting up my CNC project your stepper is a classic 4 wire …
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to gub11 +1
    All Grounds (0V) should go together, the ground of the 12V, the 5V etc all are connected together at a common point the 5V goes to all those pins because it is 5V logic input to the chip and those pins…
  • D_Hersey
    0 D_Hersey over 10 years ago

    If you want insight into the pattern read about 'quadrature.'  There are 5-phase steppers that operate in a pentagram pattern.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gub11
    0 gub11 over 10 years ago in reply to D_Hersey

    after reading a bit, i'm still unsure.  I understand more about what GND actually is, but for my purposes, to i need to hookup the arduino GND to the chips GND, or just the psu GND

    Robert Peter Oakes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to gub11

    Arduino GND, Chip GND, PSU Gnd all connect together in your system

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 10 years ago in reply to gub11

    "... or do i connect the stepperpsu ground to one ground terminal on the chip, and the arduino ground to a different ground pin on the chip?"

     

    Connect all the GND pins of the stepper chip together at the chip. That's what TI intended for you to do. (On a PCB the pins would come down to an area of copper that would tie them solidly together and also provide for some heatsinking. In your case (400mA), it looks as though what you're doing falls within the capability of the device to dissipate power from the package alone, though you might want to add some heatsinking anyway in case you want to use it at a higher current or simply to improve the long-term reliability)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gub11
    0 gub11 over 10 years ago in reply to jc2048

    jc2048 where do I get heatsinking?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to gub11

    an old motherboard and pull one from the small chips on the board is one possibility if you have access, if not there are plenty available from element14 (Newark / Farnell) or even ebay, search for stepper controller heatsinks and it should bring something up but as Gabriel stated, for the low current your switching, you probably wont need one, when you are running it, feel the top of the chip with the back of your hand or carefully with a finger, if you cant keep you skin in contact for more than  a few seconds then you need a heatsink, otherwise your probably good to go

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to Robert Peter Oakes

    I always like the wet finger.

    It gives extra time for the slow brain to register the finger is saying "S..T THIS IS HOT" ...image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to mcb1

    and the sound of sizzling probably will reach the brain faster too image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to Robert Peter Oakes

    Funny you should say that because I have witnessed that. image

     

    A funnier thing was a guy at work who was so used to working with transistors and fingering them, that the first valve receiver he worked on, he got a belt of the grid cap ...image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 10 years ago in reply to jc2048

    In case it helps, this is how the temperature calculation works for the chip. If you are working with different currents to what I've assumed here (400mA in each coil) you can rework it accordingly.

     

    The bridge has an upper transistor and a lower transistor on each end of the coil. For this application, if an upper transistor is on you also have the opposite lower transistor on. If the lower transistor is on, the opposite upper is on. That's how you get the current to flow in one direction or the other through the coil.

     

    Note from that there is always one upper and one lower on at any time.

     

    Looking at page 6 of the datasheet [section 7.6 Typical Characteristics] you can see that for 400mA the upper transistor drops about 1.1V.

     

    So that's a dissipation of 1.1V x 0.4A = 0.44W. That ends up as heat in the chip.

     

    The bottom transistor drops about 0.9V, so that one is a dissipation of 0.9V x 0.4A = 0.36W

     

    Total for the two is 0.8W. Since there are two coils that gives a grand total of 1.6W.

     

    Although the output transistors are most of the dissipation, the rest of the circuitry does take some current too. The datasheet gives a max of 70mA on the +5V supply, but that's for all outputs low; let's average the figures for all low and all high and go for 50mA which adds 5V x 0.05A = .25W to our dissipation.

     

    So the total for the chip is 1.85W.

     

    That's a lot for a DIL package. You wouldn't expect an IC to disspate more than 0.5-1W without extra help (very variable, depending on how the chip is mounted inside, so always refer to the datasheet and don't guess).

     

    The datasheet says the thermal resistance of the part is 60C/W. So, if we have 1.85W of heat flowing from the chip to the outside, we'll have a temperature rise of 111C. That's a temperature rise above whatever the ambient temperature around the package is. For an ambient of 25C, that means the chip inside will reach a temperature of 136C. The datasheet recommends a junction temperature of no more than 125C, so it looks like you should use some heatsinking.

     

    The problem for you, even if you're happy to run it above the recommended figure, is that if you have it in a confined space (without forced cooling) the ambient temperature will rise and may take you to the point where it shuts down. (You won't damage the part because it has a temperature sensor and shuts itself down when the chip gets to 150C or so, but it's always a bit mysterious when you have a chip that doesn't work for a while and then suddenly springs into life again when it's cooled down a bit.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>