Arduino
  • Products
  • More
Arduino
Arduino Forum New a FGPA emulates UNO with extra's
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 418 subscribers
  • Views 1060 views
  • Users 0 members are here
  • kickstarter
  • fpga
  • arduino
Related

New a FGPA emulates UNO with extra's

clem57
clem57 over 10 years ago

I was out of the country since October and saw this this XLR8 FPGA-Accelerated Arduino Clone Kickstarter is Live | EE Times. After reading the article , they said;

If you have a project that's using an Uno, you can swap in an XLR8 board right out of the box, and it will just work. You won't even know you're actually running your sketch on an FPGA, at least not until you fire up one of the accelerated functions... and then the magic happens.

Interesting so I looked up the https://www.kickstarter.com/projects/814866572/xlr8-arduino-compatible-fpga-based-application-acc

and sad to see the goal may not be reached, Anyone have comments why?

Clem

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 10 years ago +1
    It makes sense to compare XLR8 to the Papilio DUO, which is US$88. The DUO has a real ATmega32U4 chip, a Xilinx Spartan-6 LX9, and 512KB of SRAM (there's a more expensive version with 2MB). It also has…
  • Jan Cumps
    0 Jan Cumps over 10 years ago

    I think not enough noise  so that not a lot of people know about it (I didn't know about this campaign although I'm following FPGA related blogs/tweets),

    a price of $65 is maybe too high for an impulsive click on the "Back this Project" button (although it is a normal price for an FPGA dev board),

    and the fact that FPGA isn't that popular -  so the pool of possible crowdfunders may be low.

     

    Maybe let's check how many FPGA dev board kickstarters actually got funded?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to Jan Cumps

    17 FPGA projects.

    2 most likely will not get funded (Mango and the XLR8 you mention - both very similar projects)

    9 unsuccessful

    6 successful, including one that has everything that XLR8 and Mango are doing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Jan Cumps

    Which are the successful ones? Thanks Jan

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to clem57

    I searched kickstarter for the word FPGA, and then checked the ones that reached their funding goal - both for the completed and active projects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to Jan Cumps

    IT looks like this one is going to fail, with only 20% reached and 4 or less days to go, it looks nice but way too expensive when trying to attract the UNO folks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 10 years ago

    It makes sense to compare XLR8 to the Papilio DUO, which is US$88.  The DUO has a real ATmega32U4 chip, a Xilinx Spartan-6 LX9, and 512KB of SRAM (there's a more expensive version with 2MB).  It also has 54 I/Os, some of which have an Arduino footprint and the rest set up for Gadget Factory Papilio Wings.  I have a Kickstarter DUO ($75 early bird) and it's a very nice board.  I haven't used the Arduino part.

     

    I'm not familiar with the Altera MAX10 FPGA that's on XLR8, so I don't know how it compares to a Spartan-6 LX9.  Even if the chips are comparable, I think the DUO's I/Os and SRAM make it a lot more versatile.

     

    It's really a shame that there are no FPGA boards with pricing anything like RasPi Zero image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 10 years ago in reply to Jan Cumps

    Mango seems like a decent board but it's pretty expensive when you include the USB programmer (US$129 total).  You might be able to do better with a $79 early bird plus a USB programmer from somewhere else.  OTOH, a Papilio DUO includes the USB programmer on-board: you just need a Mini USB cable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 10 years ago

    If you want an Arduino format FPGA board, I'd check out the Gameduino which is US$30 at LinkSprite: http://store.linksprite.com/gameduino-for-arduino-a-game-adapter-for-microcontrollers/

     

    It has a 200K Spartan-3A, which is a very nice chip.

     

    Olimex has an alternate version (Gameduino is OSHW) with more I/O and optional 32MB SDRAM.