Arduino
  • Products
  • More
Arduino
Arduino Forum PWM controlled ammeter question?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 409 subscribers
  • Views 861 views
  • Users 0 members are here
  • pwm
  • arduino
Related

PWM controlled ammeter question?

Former Member
Former Member over 10 years ago

HI everyone,

 

i am trying to control a zero centered ammeter with a PWM signal from an arduino.  The ammeter displays a voltage from -12v to +12v where zero volts is in the center. The needle is centered when zero.  Now the Arduino can only supply a voltage from 0 to 5 volts simulated by a PWM signal with a value from 0 to 255, where 255 is the full 5 volts.  My problem is I need to drive the ammeter from a -12v to a +12v.  I'm thinking of some kind of external circuit with a transistor to switch on and off a 12 volt source, but that will only get me half the meter to swing.  How can I get a -12v to be driven by the Arduino?  I would like to supply a PWM value of zero to the Arduino pin which would correspond to -12v, and PWM value of 128 would be 0 volts on the ammeter, and PWM value of 255 would be +12v.  Hopefully this all makes some sense.  Any help would be appreciated!

 

THanks Mark

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    using a simple op-amp with the + connected to the arduino output, the negative biased to 2.5V ish (You could use a pot to get it better), then supply the opamp with +- 15V (Easier than trying to use a…
  • ravi_butani
    ravi_butani over 10 years ago +2
    Here is very simple way to convert 0-5 V PWM to -2.5 to +2.5 V (avg value) converter.. the circuit below is just high pass filter which remove DC portion of PWM to make it negative and positive both..…
  • jc2048
    jc2048 over 10 years ago in reply to Robert Peter Oakes +2
    Is it easier than doing it with transistors? The above isn't a whole lot more complicated than using an op-amp (plus you don't have the problem of trying to trim the zero and getting the gain right for…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    using a simple op-amp with the + connected to the arduino output, the negative biased to 2.5V ish (You could use a pot to get it better), then supply the opamp with +- 15V (Easier than trying to use a rail to rail opamp or do it with transistors)

     

    this will provide you with the +- swing nice and easy. you could also use a simple analogue comparitor the schematic would look the same

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to Robert Peter Oakes

    Thanks Peter.  i do have some op amps at home i can try and use, maybe even some comparators.  i will give this a shot tonight.  ohh and by the way I really enjoy your you tube channel!

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago in reply to Robert Peter Oakes

    Thanks Peter.  i do have some op amps at home i can try and use, maybe even some comparators.  i will give this a shot tonight.  ohh and by the way I really enjoy your you tube channel!

     

    Mark