Arduino Forum abut arduino
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
  • State Not Answered
  • Replies 12 replies
  • Subscribers 394 subscribers
  • Views 818 views
  • Users 0 members are here
Related

abut arduino

Former Member
Former Member over 9 years ago

a sine wave is applied at a0 using a diode,so that it geets rectified and then after pwm the square obatIned is only with wrt positive cycle ,i need to generate pwm  even during negative cycle and one way is to do it by full bridge rectifier .so is there any way by arduino coding i could get it

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +1
    Yes just measure both positive and negative values during entire cycle.
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1
    How about offset the sine wave to 50% of VRef (Capacitor coupled will do it, and a divider network), then simply read the whole waveform as a positive value this way 0V = 511 decimal from ADC, -2.5V will…
Parents
  • peterjcs23
    0 peterjcs23 over 9 years ago

    do you have a problem with using a full-wave rectifier as that sounds like your best bet?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • peterjcs23
    0 peterjcs23 over 9 years ago

    do you have a problem with using a full-wave rectifier as that sounds like your best bet?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 9 years ago in reply to peterjcs23

    now we just thought its better to use codes than more diodes ,just much simpler way of codes of arduino