Arduino Forum abut arduino
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
  • State Not Answered
  • Replies 12 replies
  • Subscribers 394 subscribers
  • Views 818 views
  • Users 0 members are here
Related

abut arduino

Former Member
Former Member over 9 years ago

a sine wave is applied at a0 using a diode,so that it geets rectified and then after pwm the square obatIned is only with wrt positive cycle ,i need to generate pwm  even during negative cycle and one way is to do it by full bridge rectifier .so is there any way by arduino coding i could get it

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +1
    Yes just measure both positive and negative values during entire cycle.
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1
    How about offset the sine wave to 50% of VRef (Capacitor coupled will do it, and a divider network), then simply read the whole waveform as a positive value this way 0V = 511 decimal from ADC, -2.5V will…
Parents
  • michaelkellett
    0 michaelkellett over 9 years ago

    Are you trying to generate pulses of controlled width, one per half cycle of an incoming sine wave ?

     

    If so then please tell us the frequency of the input sine wave, the range of pulse widths you need coming out, where the sine wave comes from and what hardware you have. Some diagrams would be nice. With some additional information it will be possible to help you. If my guess at what you are trying to do is correct it is possible in principle.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to michaelkellett

    #include<PWM.h>

    int32_t frequency =100000;

    void setup()

    {

    InitTimersSafe() ;

    bool success = SetPinFrequencySafe(9, frequency);

    if(success) {

      pinMode(13, OUTPUT);

      digitalWrite(13,HIGH);

    }

    }

     

     

    void loop() {

    int sensorValue= analogRead(A0);

    pwmWrite(9, sensorValue /4);

    delay(30);

     

     

    }

     

     

     

                                                                                              from the signal generator i have  provide a supply of  5 v pp and 50 hz frequency, +ve part provided to the  diode and the diode is connected to the  a0 pin in the arduino uno  and-ve part of signal generator to ground the .then is have taken output from 9 pin and at this point i am getting pwm of  only +ve cycle of sine wave input as reference(as i have used a diode)image

    now i need to generate pwm of -ve cycle

    1. i want arduino code to store the +ve cycle pwm wave  in other pin and then during -ve cycle i want to output it through this pin .by this i would get  pwm for both +ve and -ve cycle of sine wave  and  it would be helpful if any way is there to distinguish the pwm for +ve and -ve cycle

    2 in a simple way i need to generate a pwm for -ve cycle and need to do it by arduino code only and not by rectifier (less circuit part  and more part must be done in coding)

    any way u could help me to do this it would be of great help. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to michaelkellett

    #include<PWM.h>

    int32_t frequency =100000;

    void setup()

    {

    InitTimersSafe() ;

    bool success = SetPinFrequencySafe(9, frequency);

    if(success) {

      pinMode(13, OUTPUT);

      digitalWrite(13,HIGH);

    }

    }

     

     

    void loop() {

    int sensorValue= analogRead(A0);

    pwmWrite(9, sensorValue /4);

    delay(30);

     

     

    }

     

     

     

                                                                                              from the signal generator i have  provide a supply of  5 v pp and 50 hz frequency, +ve part provided to the  diode and the diode is connected to the  a0 pin in the arduino uno  and-ve part of signal generator to ground the .then is have taken output from 9 pin and at this point i am getting pwm of  only +ve cycle of sine wave input as reference(as i have used a diode)image

    now i need to generate pwm of -ve cycle

    1. i want arduino code to store the +ve cycle pwm wave  in other pin and then during -ve cycle i want to output it through this pin .by this i would get  pwm for both +ve and -ve cycle of sine wave  and  it would be helpful if any way is there to distinguish the pwm for +ve and -ve cycle

    2 in a simple way i need to generate a pwm for -ve cycle and need to do it by arduino code only and not by rectifier (less circuit part  and more part must be done in coding)

    any way u could help me to do this it would be of great help. image