Arduino Forum Data output from OV7670
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
  • State Not Answered
  • Replies 13 replies
  • Subscribers 402 subscribers
  • Views 2487 views
  • Users 0 members are here
Related

Data output from OV7670

Former Member
Former Member over 9 years ago

Hi All.

 

I have been trying to get some useful data from the OV7670 camera module but it seems that it is not outputting the correct data. I have been using this code: https://github.com/ComputerNerd/ov7670-no-ram-arduino-uno and everything seems fine from a software point of view but what I am getting out is not as expected. With the lens covered I should get a stream of repetitive data like [0,80,0,80,0,80....] but I dont regardless of whether it is covered or not. I have tried various register settings and still no joy. Even with default register settings I should be able to see a basic image. I have also viewed the data from the device on a logic analyzer and it is clear that the data is random. The pic below is the camera module output data with the lens covered and it can be seen that the data is totally random.

 

image

 

Anyone know why this is happening or has seen it before?

 

Thanks,

 

Mark.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +1
    9 times out of 10, the connections are not right. Please double check these: Connections Order Arduino ov7670 A5->SIOC A4<->SIOD Note what I have just described (above) are I2C connections you will need…
  • Former Member
    Former Member over 9 years ago in reply to shabaz +1
    Below is a capture from the oscilloscope. Blue is the pixel clock and yellow is one of the data pins. I was clocking the logic analyzer using a trigger from inside my code when the HREF went high. As you…
Parents
  • clem57
    0 clem57 over 9 years ago

    9 times out of 10, the connections are not right. Please double check these:

    Connections

    Order Arduino ov7670

    A5->SIOC

    A4<->SIOD

    Note what I have just described (above) are I2C connections you will need pullup resistors to 3.3v for both SIOC and SIOD.

    You must not connect the resistors to 5v.

    I have found that certain resistor values do not work such as 1K and 2.2K but found 4.7K and 10K to work.

    11-> (convert 5v to 3.3v) XCLK

    A0<-0

    A1<-1

    A2<-2

    A3<-3

    4<-4

    5<-5

    6<-6

    7<-7

    3<-VSYNC

    2<-PCLK

    GND->PWDN

    3.3->RESET

    GND->GND

    3.3v->3.3v

    Do you have a way to check all the voltage levels?

    Clem

    PS check the address of I2C is correct also.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago

    9 times out of 10, the connections are not right. Please double check these:

    Connections

    Order Arduino ov7670

    A5->SIOC

    A4<->SIOD

    Note what I have just described (above) are I2C connections you will need pullup resistors to 3.3v for both SIOC and SIOD.

    You must not connect the resistors to 5v.

    I have found that certain resistor values do not work such as 1K and 2.2K but found 4.7K and 10K to work.

    11-> (convert 5v to 3.3v) XCLK

    A0<-0

    A1<-1

    A2<-2

    A3<-3

    4<-4

    5<-5

    6<-6

    7<-7

    3<-VSYNC

    2<-PCLK

    GND->PWDN

    3.3->RESET

    GND->GND

    3.3v->3.3v

    Do you have a way to check all the voltage levels?

    Clem

    PS check the address of I2C is correct also.