Arduino Forum Data output from OV7670
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
  • State Not Answered
  • Replies 13 replies
  • Subscribers 402 subscribers
  • Views 2487 views
  • Users 0 members are here
Related

Data output from OV7670

Former Member
Former Member over 9 years ago

Hi All.

 

I have been trying to get some useful data from the OV7670 camera module but it seems that it is not outputting the correct data. I have been using this code: https://github.com/ComputerNerd/ov7670-no-ram-arduino-uno and everything seems fine from a software point of view but what I am getting out is not as expected. With the lens covered I should get a stream of repetitive data like [0,80,0,80,0,80....] but I dont regardless of whether it is covered or not. I have tried various register settings and still no joy. Even with default register settings I should be able to see a basic image. I have also viewed the data from the device on a logic analyzer and it is clear that the data is random. The pic below is the camera module output data with the lens covered and it can be seen that the data is totally random.

 

image

 

Anyone know why this is happening or has seen it before?

 

Thanks,

 

Mark.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +1
    9 times out of 10, the connections are not right. Please double check these: Connections Order Arduino ov7670 A5->SIOC A4<->SIOD Note what I have just described (above) are I2C connections you will need…
  • Former Member
    Former Member over 9 years ago in reply to shabaz +1
    Below is a capture from the oscilloscope. Blue is the pixel clock and yellow is one of the data pins. I was clocking the logic analyzer using a trigger from inside my code when the HREF went high. As you…
Parents
  • shabaz
    0 shabaz over 9 years ago

    Also, as well as the checks clem57 has mentioned, I'd strongly advise connecting up an oscilloscope (not logic analyser)

    to at least a few of the connections, to see the waveform shape. There could be all sorts of issues.

    It is also not an ideal project to follow because it is operating outside of the specs slightly (the OV7670 is designed for 3V max).

    Also, wire lengths will matter, and maybe even a buffer is needed.

     

    See here for a project that used a different OmniVision part, (and doesn't use the Arduino) but probably you can glean some tips from it:

    BBB - Imaging with a PRU connected Camera

    If it is an ebay type camera board, examine it and make sure they didn't shortcut like using poor choice of decoupling capacitors.

    It is critical with these cameras.

    If you're using the Uno, to be honest it may be better to find an alternative way of using imaging (e.g. Pi 3 and associated camera)

    because the Arduino Uno is lacking in resources : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to shabaz

    The voltage levels are all correct, I have checked with scope and meter. I have also checked various registers via I2C and they seem ok. The device is spitting out data upon power up with the given clock and so would suggest that wiring configuration is ok. This project has been undertaken a lot with arduinos with success so I would say that the voltages and speeds are ok.

     

    At this moment I would just be happy to see the correct data coming from the device, whether I use a scope or logic analyzer. I am not to concerned with data storage and transmission or MCU at the moment. With the correct voltages and clock I should output image data but for some reason it dosn't.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to Former Member

    What did the waveforms look like on the scope? Any noise or glitches on the oscilloscope analog traces?

    Do you have a screen grab from oscilloscope analog traces (not logic traces).

    How was your logic analyser configured? Clocking on the pixel clock, or free-running capture from the logic analyzer's own clock?

    Also a photo of the setup would help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to Former Member

    Also, is it an assumption that the data is random, or have you checked?

    i.e. can you plot it in a graphic view (an entire frame if possible), to see if there is any signal in the noise?

    It doesn't look entirely random to me. I can see the most significant bits alternated on every other byte for the first 16 bytes. It is to be expected for the least significant ones to possibly have variations due to sensor noise.

    I don't know what format is expected, but it doesn't appear random.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to shabaz

    Below is a capture from the oscilloscope. Blue is the pixel clock and yellow is one of the data pins. I was clocking the logic analyzer using a trigger from inside my code when the HREF went high.

     

    image

     

    As you say the MSB alternates to begin with but the rest seem to be way to random. For a 2 byte pixel for a black image they should repeat every 2 bytes but clearly doesn't.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to shabaz

    Below is a capture from the oscilloscope. Blue is the pixel clock and yellow is one of the data pins. I was clocking the logic analyzer using a trigger from inside my code when the HREF went high.

     

    image

     

    As you say the MSB alternates to begin with but the rest seem to be way to random. For a 2 byte pixel for a black image they should repeat every 2 bytes but clearly doesn't.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 9 years ago in reply to Former Member

    Hi Mark,

     

    You're triggering on HREF, but once triggered, is the data captured by your analyser based on the pixel clocking in the data into your analyser, or based on an internal oscillator inside the logic analyser capturing at a higher rate? There is a difference, and it would help to know which one. If the latter, what clock rate are you capturing at?

     

    Also, the data snapshot on your oscilloscope isn't random. Could you plot the image for an entire frame?

    Perhaps AGC is kicking in, or some bursts of noise that partially affect the image, or misconfigured registers could be having an unusual affect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to shabaz

    I am capturing off the pixel clock.

     

    Here is what the image looks like (a section of it):

     

    image

     

    As you said "Perhaps the AGC is kicking in". I do believe it is a register setting. I am fairly confident that the hardware is ok. I have tried various register settings but to no avail. When I try to run the test pattern the output is not what is expected but it is consistent in its "randomness" if that makes sense. Note: these are only 24 pixels wide so are just chunks.

     

    This is supposed to represent a colour bar and is the same each time so it must be functioning correctly but is just delivering the wrong data.

     

    image

     

    Mark.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to Former Member

    Is the Arduino code definitely tried-and-tested by others? Perhaps the 4MHz pixel clock is quite high, for Arduino code to handle without skipping occasionally maybe.

    If you can, for now try to reduce even further to the minimum image size that the camera supports, i.e. lowest pixel clock, down to 1 or 2MHz maybe.

    When there are regular patterns like the colour bar but where there are multiple repeats of it, it sometimes means that pixels, or entire lines, are being skipped (e.g. 2-in-3 HREFs have been skipped perhaps).

    Also, if the colours are wrong, possibly the RGB is being read back-to-front maybe (i.e. MSB may be LSB per R, G and B bit width) - but not sure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 9 years ago in reply to Former Member

    From a very quick glance at the code you point to, it looks like the camera chip can serve up the data with different codings (including YUV422, YUV444, and RGB packed into a 16-bit word). You need to understand which you're asking for when the registers are set up to know how to interpret what comes back to you. I'd go back to first principles - look at the datasheet for the device, understand what's being set up, and then you'll know how to interpret it. You could just experiment with the data until you get it right, but if you understand what's going on you'll be in a much better position to change it and modify it to better suit what you're doing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to jc2048

    That's the problem no matter what coding I use the, 16 bits representing the pixel looks wrong. It is more that likely that I have set up the registers wrong and by what I have read online many others have had difficulties with them to. According to the following page the default format is YCbCr422, Embedded Programmer: Hacking the OV7670 camera module (SCCB cheat sheet inside) so even before I set the registers I should recieve the following to represent a black image [0,80,0,80,0,80....]. If it's wrong an the registers have to be set accordingly my question is: does anyone out there have any experience setting up the registers?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to Former Member

    Hi Mark,

     

    I've not used the OV7670 but have used a different part from the same mnfr. It is likely the registers may have some similarity.

    The link I mentioned earlier has the source code, so you could check the registers and compare with the OV7670 datasheet and try to create a list

    of registers and values that you will need to configure. Or, you might need to talk to the mnfr and ask them for configuration values, usually

    they will have this information.

    The link you provided shows that the person was using it with an STM processor, not Arduino, and he mentions that data rate by default (no configuration)

    is VGA, which is very high for a small microcontroller. So I suspect your Arduino Uno is skipping lines, possibly pixels too (and this is inline with the

    findings from the colour bar data you plotted).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to shabaz

    I am not really concerned with the arduino and what its doing. The data from the the actual pins of the device as viewed on an oscilloscope and logic analyzer are not as they should be. The only thing that is not really ideal is the clock input. Perhaps this is causing the device to behave improperly. Anyway I will be parking this for a while, I got a different camera with usb and works fine.

     

    Thanks

     

    Mark.