Arduino Forum Need help on motion sensor...
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 393 subscribers
  • Views 254 views
  • Users 0 members are here
Related

Need help on motion sensor...

Former Member
Former Member over 9 years ago

Hello Friends,

 

I am planing to do some best for public places and,  Is there any sensor available to detect human presence . I am aware from PIR Motion sensor but this is not useful as the sensor detect several motions and not working fine due to frequently hanged.

 

I would like to use this 24 Hrs for 150 Sqft welcome desk (Reception) area, Where if any guest or passenger take the access in particular area, A welcome tone of hotel with hospitality message flash for 40-50 Seconds and when guest moved out from particular range, Same will off immediately. Kindly suggest me a better solution .

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +3
    Actually if you want a "smart sensor", I would look at Grid-Eye from Panasonic Panasonics' infrared array sensor is a thermopile-type infrared sensor which detects quantity of infrared ray. These high…
  • mudz
    mudz over 9 years ago +2
    If PIR is not an option, why don't you try a camera with your customized algorithms to detect multiple persons or give commands( to do such things)? It would be more accurate and have great potential to…
Parents
  • mudz
    0 mudz over 9 years ago

    If PIR is not an option, why don't you try a camera with your customized algorithms to detect multiple persons or give commands( to do such things)?

    It would be more accurate and have great potential to do numerous things.

    and the best part is you don't even have to interface it to computer to do such things, You can do that with several cheap developments kits available in market (Hint: RASPBERRYPI3-MODB-1GBRASPBERRYPI3-MODB-1GB and the camera(of course) : RPI CAMERA BOARDRPI CAMERA BOARD )

    Good Luck image

     

    mudz

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mudz
    0 mudz over 9 years ago

    If PIR is not an option, why don't you try a camera with your customized algorithms to detect multiple persons or give commands( to do such things)?

    It would be more accurate and have great potential to do numerous things.

    and the best part is you don't even have to interface it to computer to do such things, You can do that with several cheap developments kits available in market (Hint: RASPBERRYPI3-MODB-1GBRASPBERRYPI3-MODB-1GB and the camera(of course) : RPI CAMERA BOARDRPI CAMERA BOARD )

    Good Luck image

     

    mudz

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 9 years ago in reply to mudz

    Dear Mudz,

     

    Appreciating for your good revert and help.

     

    Can you advise me any more cheap and best process on my project.

    I would like to make public address alarm through help of any of best motion sensor. Some one advises me to take people count device and then add with same. I am too confused and hoping very best for my project.

     

    I woulds like to use this at, Hotels / Resort's reception or at welcome desk for play welcome tone for guests. I am very ambitious to make the same and expecting good info and advise for same.