Arduino Forum Need help on motion sensor...
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 393 subscribers
  • Views 254 views
  • Users 0 members are here
Related

Need help on motion sensor...

Former Member
Former Member over 9 years ago

Hello Friends,

 

I am planing to do some best for public places and,  Is there any sensor available to detect human presence . I am aware from PIR Motion sensor but this is not useful as the sensor detect several motions and not working fine due to frequently hanged.

 

I would like to use this 24 Hrs for 150 Sqft welcome desk (Reception) area, Where if any guest or passenger take the access in particular area, A welcome tone of hotel with hospitality message flash for 40-50 Seconds and when guest moved out from particular range, Same will off immediately. Kindly suggest me a better solution .

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +3
    Actually if you want a "smart sensor", I would look at Grid-Eye from Panasonic Panasonics' infrared array sensor is a thermopile-type infrared sensor which detects quantity of infrared ray. These high…
  • mudz
    mudz over 9 years ago +2
    If PIR is not an option, why don't you try a camera with your customized algorithms to detect multiple persons or give commands( to do such things)? It would be more accurate and have great potential to…
Parents
  • clem57
    0 clem57 over 9 years ago

    Actually if you want a "smart sensor", I would look at Grid-Eye from Panasonic

     

    Panasonics' infrared array sensor is a thermopile-type infrared sensor which detects quantity of infrared ray. These high precision sensors, based on advanced MEMS technology, have temperature detection, achieved on a two dimensional area, digital output, and have a miniature SMD package.

    Check out Panasonic Grid-EYE Infra-Red Sensor Evaluation Kit | Farnell element14 It has the ability to detect the difference between human and a dog(animal). image

     

    Clem

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago

    Actually if you want a "smart sensor", I would look at Grid-Eye from Panasonic

     

    Panasonics' infrared array sensor is a thermopile-type infrared sensor which detects quantity of infrared ray. These high precision sensors, based on advanced MEMS technology, have temperature detection, achieved on a two dimensional area, digital output, and have a miniature SMD package.

    Check out Panasonic Grid-EYE Infra-Red Sensor Evaluation Kit | Farnell element14 It has the ability to detect the difference between human and a dog(animal). image

     

    Clem

    • Cancel
    • Vote Up +3 Vote Down