Arduino
  • Products
  • More
Arduino
Arduino Forum Help!! Arduino camera (as video)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 1388 views
  • Users 0 members are here
  • camera.
  • arduino_development_environment
  • arduino
Related

Help!! Arduino camera (as video)

e14 Contributor
e14 Contributor over 10 years ago

Hi everybody!! I am working on my graduation project, and I want need to record a light coming from an optical cable with Arduino, i'm don't know much about arduino.

Could somebody help??
I noticed that with Arduino Uno you can use the camera for pictures. Is it possible to record??

Help please.

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 10 years ago in reply to e14 Contributor +2
    If you are shining a 850nm laser directly down the fibre then you could detect it with a laser light detector such as: https://www.finisar.com/optical-components/hfd3180-103
  • clem57
    clem57 over 10 years ago +1
    Fiber optic cables have different frequencies from the light you and me see. That is why you are warned never look t the light! It will burn the retina severely depending on time of exposure. Please read…
  • strb
    strb over 10 years ago +1 suggested
    I agree too with Clem. Anyway yes camera sensors are a little more sensitive than the human eye so they can see a piece of IR spectrum, (you can verify it with your phone and the tv remote, just point…
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Are you wanting to record a video feed,  or just data points when light is present on the cable output?

    Regardless;  what kind of output  (TOSLink, fiber, other)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    well...it will be from an end of a fiber. That end should be near the camera so it can record some spots( two points coming out of the camera). It should be a video feed. I think that will use a lot od space in the computer.
    Any idea??
    Thanks a lot!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    well...it will be from an end of a fiber. That end should be near the camera so it can record some spots( two points coming out of the camera). It should be a video feed. I think that will use a lot od space in the computer.
    Any idea??
    Thanks a lot!!