Arduino
  • Products
  • More
Arduino
Arduino Forum Learning about H-bridges and transistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 38 replies
  • Answers 8 answers
  • Subscribers 422 subscribers
  • Views 4714 views
  • Users 0 members are here
  • frontpage
  • h-bridge
  • transistors
Related

Learning about H-bridges and transistors

ovidiub13
ovidiub13 over 10 years ago

I'm trying to learn about transistors and H bridges towards a final goal of controlling a bipolar stepper motor with Arduino.

 

I've done the following half H-bridge in the process of learning:

image

My first question: Why can't I use a single resistor to connect the base of both transistors to ground?

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 10 years ago +1 suggested
    I'm not sure that this schematic works... the led isn't reverse polarized? Anyway use a pnp as pullup transistor and a npn as pulldown, it's a good thing to put also a limiter resistor to control the current…
  • strb
    strb over 10 years ago in reply to clem57 +1
    Great "how link" clem57
  • mcb1
    mcb1 over 10 years ago in reply to ovidiub13 +1 suggested
    What I'm having issues understanding is how transistors work You can consider a transistor as a switch (in this case they are either ON or OFF) The control part of the switch is the base to emitter (NPN…
Parents
  • ovidiub13
    0 ovidiub13 over 10 years ago

    Thank you for your feedback.

     

    I'm not sure that this schematic works... the led isn't reverse polarized?

    It works.

     

    I've read about how H-bridges work. I understand the general concept. What I'm having issues understanding is how transistors work. Here I'm just using them like switches.

     

    What I've shown previously was, as I've said, half an H-bridge.

     

    Here's the full H-bridge:

     

    image

     

    I've tested this on my breadboard and it works ( I can make a video if necessary).

     

    What I've noticed on the full H-Bridge is that I have 2,77 V on LED1 and 3,40 V on LED2. I don't understand why. SInce the two halves are basically mirrored, I expected them to be the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ovidiub13
    0 ovidiub13 over 10 years ago in reply to ovidiub13

    I've replaced one of the transistors, and now the voltages are the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ovidiub13
    0 ovidiub13 over 10 years ago in reply to ovidiub13

    I've replaced one of the transistors, and now the voltages are the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • strb
    0 strb over 10 years ago in reply to ovidiub13

    Yes you're using it like switch but in the wrong way, q1 and q2 can't reach the saturation region and burn more power.

    Hint: the arrow in the emitter show you the direction of the current, the same is for diode, than take a look to your first schematic and you can easily see that the led is connected wrong because current can't flow in both direction.

    It's hard to explain here how bjt works, try to take a look here https://en.wikipedia.org/wiki/Bipolar_junction_transistor , don't read the physical functioning, you have to learn just the relation between base/collector current/voltage.

    The full bridge works but probably you're turning on the "wrong led" when you push a button, try to use two different coloured leds.

    You have to know how basic components work before doing anything, simply because it's hard to do something right if you don't know how it works.