Arduino Forum Learning about H-bridges and transistors
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
  • State Verified Answer
  • Replies 38 replies
  • Answers 8 answers
  • Subscribers 397 subscribers
  • Views 2960 views
  • Users 0 members are here
  • frontpage
  • h-bridge
  • transistors
Related

Learning about H-bridges and transistors

ovidiub13
ovidiub13 over 9 years ago

I'm trying to learn about transistors and H bridges towards a final goal of controlling a bipolar stepper motor with Arduino.

 

I've done the following half H-bridge in the process of learning:

image

My first question: Why can't I use a single resistor to connect the base of both transistors to ground?

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 9 years ago +1 suggested
    I'm not sure that this schematic works... the led isn't reverse polarized? Anyway use a pnp as pullup transistor and a npn as pulldown, it's a good thing to put also a limiter resistor to control the current…
  • strb
    strb over 9 years ago in reply to clem57 +1
    Great "how link" clem57
  • mcb1
    mcb1 over 9 years ago in reply to ovidiub13 +1 suggested
    What I'm having issues understanding is how transistors work You can consider a transistor as a switch (in this case they are either ON or OFF) The control part of the switch is the base to emitter (NPN…
Parents
  • D_Hersey
    0 D_Hersey over 9 years ago

    There are unipolar and bipolar motors. Bipolar motors want the current in the coils to be reversed.  Five volt six or eight wire unipolar stepper motors can be used as ten volt bipolar motors.  4-phase unipolar motors use four coils, bipolar motors use two coils, but four phases 'cuz +/-.

     

    There are five phase motors.  These are less likely to 'cog' or resonate, but they are expensive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 9 years ago

    There are unipolar and bipolar motors. Bipolar motors want the current in the coils to be reversed.  Five volt six or eight wire unipolar stepper motors can be used as ten volt bipolar motors.  4-phase unipolar motors use four coils, bipolar motors use two coils, but four phases 'cuz +/-.

     

    There are five phase motors.  These are less likely to 'cog' or resonate, but they are expensive.