Arduino
  • Products
  • More
Arduino
Arduino Forum Learning about H-bridges and transistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 38 replies
  • Answers 8 answers
  • Subscribers 422 subscribers
  • Views 4736 views
  • Users 0 members are here
  • frontpage
  • h-bridge
  • transistors
Related

Learning about H-bridges and transistors

ovidiub13
ovidiub13 over 10 years ago

I'm trying to learn about transistors and H bridges towards a final goal of controlling a bipolar stepper motor with Arduino.

 

I've done the following half H-bridge in the process of learning:

image

My first question: Why can't I use a single resistor to connect the base of both transistors to ground?

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 10 years ago +1 suggested
    I'm not sure that this schematic works... the led isn't reverse polarized? Anyway use a pnp as pullup transistor and a npn as pulldown, it's a good thing to put also a limiter resistor to control the current…
  • strb
    strb over 10 years ago in reply to clem57 +1
    Great "how link" clem57
  • mcb1
    mcb1 over 10 years ago in reply to ovidiub13 +1 suggested
    What I'm having issues understanding is how transistors work You can consider a transistor as a switch (in this case they are either ON or OFF) The control part of the switch is the base to emitter (NPN…
Parents
  • Problemchild
    0 Problemchild over 10 years ago

    If you have a practical purpose for the stepper when you are done try the A4988 controllers you can get cheaply that work with the Arduino and have very good current handling etc

     

    http://www.ebay.co.uk/sch/i.html?_from=R40&_trksid=m570.l1313&_nkw=A4988&_sacat=0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to Problemchild

    Even MagPi's article a couple of years ago got it wrong, they've subsequently revised their schematic in the PDF, but the thread that originally discussed it is here:

    The MagPi Magazine - Aimed at learners - Printed edition Kickstarter

    Quite a lot of hobbyists think its fine to stick 4 identical BJTs together and they'll have a H-bridge and save the costs of an IC.. forgetting that the IC actually works.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 10 years ago in reply to shabaz

    Yes except they are rarely identical unless you are limiting the gain with resistors  and the switching logic and drive for the bridge is often not considered so you end up with a system that can short out or not have enough gain to turn on properly or have too low voltage to do the same.

     

    Failing that just dealing with back EMFs etc is just an annoyance. Beyond proving you can do it you are better off with the chip unless you are switching mega-amps or something image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Problemchild
    0 Problemchild over 10 years ago in reply to shabaz

    That said he should be commended for trying the circuit out with "real" components first, much as I said that those70's -80's books I! bought were interesting for demonstrating concepts  with real components rather than just using an Arduino thingy mabob shield to do it all

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 10 years ago in reply to shabaz

    That said he should be commended for trying the circuit out with "real" components first, much as I said that those70's -80's books I! bought were interesting for demonstrating concepts  with real components rather than just using an Arduino thingy mabob shield to do it all