Arduino
  • Products
  • More
Arduino
Arduino Forum Learning about H-bridges and transistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 38 replies
  • Answers 8 answers
  • Subscribers 422 subscribers
  • Views 4755 views
  • Users 0 members are here
  • frontpage
  • h-bridge
  • transistors
Related

Learning about H-bridges and transistors

ovidiub13
ovidiub13 over 10 years ago

I'm trying to learn about transistors and H bridges towards a final goal of controlling a bipolar stepper motor with Arduino.

 

I've done the following half H-bridge in the process of learning:

image

My first question: Why can't I use a single resistor to connect the base of both transistors to ground?

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 10 years ago +1 suggested
    I'm not sure that this schematic works... the led isn't reverse polarized? Anyway use a pnp as pullup transistor and a npn as pulldown, it's a good thing to put also a limiter resistor to control the current…
  • strb
    strb over 10 years ago in reply to clem57 +1
    Great "how link" clem57
  • mcb1
    mcb1 over 10 years ago in reply to ovidiub13 +1 suggested
    What I'm having issues understanding is how transistors work You can consider a transistor as a switch (in this case they are either ON or OFF) The control part of the switch is the base to emitter (NPN…
Parents
  • D_Hersey
    0 D_Hersey over 10 years ago

    People afraid of discretes.  We had names for them back in the day, but they are no longer politically correct.  You should try to assemble a SM drive even if you eventually go off-the-shelf.  It would make you a better specsman.

     

    The H drive is a topology.  The elements are the load, represented by the horizontal bar of the H, and four SPST switches represented by the vertical elements.  Let's enumerate them in the mathematically positive (counter-clockwise) direction.  The control for the even numbered switches are coupled as are the odd numbered switches.  You don't want the 1 and 2 switch, or the 3 and 4 switch to close simultaneously.  No current limit.  In the case of a SM drive, though, we probably want to put a current source at the top or a current sink at the bottom.  If we do this, our worries about punch-through will be profoundly diminished.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 10 years ago

    People afraid of discretes.  We had names for them back in the day, but they are no longer politically correct.  You should try to assemble a SM drive even if you eventually go off-the-shelf.  It would make you a better specsman.

     

    The H drive is a topology.  The elements are the load, represented by the horizontal bar of the H, and four SPST switches represented by the vertical elements.  Let's enumerate them in the mathematically positive (counter-clockwise) direction.  The control for the even numbered switches are coupled as are the odd numbered switches.  You don't want the 1 and 2 switch, or the 3 and 4 switch to close simultaneously.  No current limit.  In the case of a SM drive, though, we probably want to put a current source at the top or a current sink at the bottom.  If we do this, our worries about punch-through will be profoundly diminished.