Arduino
  • Products
  • More
Arduino
Arduino Forum Learning about H-bridges and transistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 38 replies
  • Answers 8 answers
  • Subscribers 422 subscribers
  • Views 4777 views
  • Users 0 members are here
  • frontpage
  • h-bridge
  • transistors
Related

Learning about H-bridges and transistors

ovidiub13
ovidiub13 over 10 years ago

I'm trying to learn about transistors and H bridges towards a final goal of controlling a bipolar stepper motor with Arduino.

 

I've done the following half H-bridge in the process of learning:

image

My first question: Why can't I use a single resistor to connect the base of both transistors to ground?

  • Sign in to reply
  • Cancel

Top Replies

  • strb
    strb over 10 years ago +1 suggested
    I'm not sure that this schematic works... the led isn't reverse polarized? Anyway use a pnp as pullup transistor and a npn as pulldown, it's a good thing to put also a limiter resistor to control the current…
  • strb
    strb over 10 years ago in reply to clem57 +1
    Great "how link" clem57
  • mcb1
    mcb1 over 10 years ago in reply to ovidiub13 +1 suggested
    What I'm having issues understanding is how transistors work You can consider a transistor as a switch (in this case they are either ON or OFF) The control part of the switch is the base to emitter (NPN…
Parents
  • D_Hersey
    0 D_Hersey over 10 years ago

    The inductive kickback will start when the switch is closed.  The spike current will be then at its maximum, equal to the coil current at that moment.  The coil will act to oppose current changes in the switch by creating a potential spike.  This tells us that the max current rating on the diode has to be above the load current.  The faster this diode is, the better.  Use UltraFast or Shottky.  The SMPS industry uses lotsa these in flyback supplies and the like, so it won't be hard to find some for cheap.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 10 years ago

    The inductive kickback will start when the switch is closed.  The spike current will be then at its maximum, equal to the coil current at that moment.  The coil will act to oppose current changes in the switch by creating a potential spike.  This tells us that the max current rating on the diode has to be above the load current.  The faster this diode is, the better.  Use UltraFast or Shottky.  The SMPS industry uses lotsa these in flyback supplies and the like, so it won't be hard to find some for cheap.