Arduino Forum buttons
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
  • State Suggested Answer
  • Replies 15 replies
  • Answers 5 answers
  • Subscribers 405 subscribers
  • Views 1276 views
  • Users 0 members are here
Related

buttons

Former Member
Former Member over 9 years ago

I want to us 7 buttons with my arduino uno which will send out different values. For example if i press one button i will get the value of 10, if i press a different button i will get 20, if i press another i will get 30 etc. I haven't found a way to separate the results sent to the serial port.

  • Sign in to reply
  • Cancel

Top Replies

  • Nate1616
    Nate1616 over 9 years ago +2 suggested
    Simon- What does you current code look like? It seems like you are printing all the button states in one line. Is this correct? What you could do is have a line that checks if the button state is high…
  • mrchunckuee
    mrchunckuee over 9 years ago +2 suggested
    Simon in the function setup not defined buttons as input. const int bt = 2; const int bt1 = 4; int btState = 1; int lastState = 1; void setup(){ pinMode(bt, INPUT); pinMode(bt1, INPUT); Serial.begin(9600…
  • Nate1616
    Nate1616 over 9 years ago in reply to Former Member +2
    Pedro beat me to it.
Parents
  • mrchunckuee
    0 mrchunckuee over 9 years ago

    Simon in the function setup not defined buttons as input.

     

    const int bt = 2;

    const int bt1 = 4;

     

    int btState = 1;

    int lastState = 1;

     

    void setup(){

      pinMode(bt, INPUT);

      pinMode(bt1, INPUT);

      Serial.begin(9600);

    }

     

    void loop()

    {

      btState = digitalRead(bt);

      if (btState != lastState)

      {

        if (btState == HIGH)

           Serial.println(440);

        delay(30);

        lastState = btState;

      }

      btState = digitalRead(bt1);

      if (btState != lastState)

      {

        if (btState == HIGH)

          Serial.println(392);

        delay(30);

        lastState = btState;

      }

    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to mrchunckuee

    HI Pedro this helped but when I press the button connected to pin 2 I get 440 out of it and sometimes 392 it does not always give me 440 only out. it is the same with the second button

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to mrchunckuee

    HI Pedro this helped but when I press the button connected to pin 2 I get 440 out of it and sometimes 392 it does not always give me 440 only out. it is the same with the second button

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Nate1616
    0 Nate1616 over 9 years ago in reply to Former Member

    Try this link to solve your problem Simon.  https://www.arduino.cc/en/Tutorial/Debounce

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer