Arduino Forum buttons
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
  • State Suggested Answer
  • Replies 15 replies
  • Answers 5 answers
  • Subscribers 405 subscribers
  • Views 1298 views
  • Users 0 members are here
Related

buttons

Former Member
Former Member over 9 years ago

I want to us 7 buttons with my arduino uno which will send out different values. For example if i press one button i will get the value of 10, if i press a different button i will get 20, if i press another i will get 30 etc. I haven't found a way to separate the results sent to the serial port.

  • Sign in to reply
  • Cancel

Top Replies

  • Nate1616
    Nate1616 over 9 years ago +2 suggested
    Simon- What does you current code look like? It seems like you are printing all the button states in one line. Is this correct? What you could do is have a line that checks if the button state is high…
  • mrchunckuee
    mrchunckuee over 9 years ago +2 suggested
    Simon in the function setup not defined buttons as input. const int bt = 2; const int bt1 = 4; int btState = 1; int lastState = 1; void setup(){ pinMode(bt, INPUT); pinMode(bt1, INPUT); Serial.begin(9600…
  • Nate1616
    Nate1616 over 9 years ago in reply to Former Member +2
    Pedro beat me to it.
Parents
  • clem57
    0 clem57 over 9 years ago

    What is the endgame here? If we knew that, there are techniques of multiplexing the buttons.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to clem57

    The end result i want is to have 7 buttons connected to my arduino.

     

    If button 1 is pressed it will send the value 261 to the serial port once.

    If button 2 is pressed it will send the value 293 to the serial port once.

    If button 3 is pressed it will send the value 329 to the serial port once.

    If button 4 is pressed it will send the value 349 to the serial port once.

    If button 5 is pressed it will send the value 392 to the serial port once.

    If button 6 is pressed it will send the value 440 to the serial port once.

    If button 7 is pressed it will send the value 493 to the serial port once.

     

    Hope that makes sense

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to Former Member

    int myChar[] = {"261", "293", "329", "349", "392", "440", "493" };

    int butArray[] = {2, 3, 4, 5, 6, 7, 8};

    int count = 0;

    int timer = 50;

    void setup(){

    Serial.begin(9600);

       while (!Serial);

    for (count=0;count<6;count++) {

      pinMode(butArray[count], INPUT);

    }

    void loop() {

      for (count=0;count<7;count++) {

    /* read value of buton based on butArray see Arduino - Debounce */

      If butArray[count] = 'HIGH' {

         Serial.print(myChar[count]);

         }

      delay(timer);

      }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to clem57

    Thanks for the code Clem but it says that there is an invalid conversion from 'const char' to 'int'

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to Former Member

    Take out the " marks on the first line. You need to complete the comment into code reading Arduino - Debounce

    for the details how.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago in reply to Former Member

    Take out the " marks on the first line. You need to complete the comment into code reading Arduino - Debounce

    for the details how.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 9 years ago in reply to clem57

    do you have an example of that i don't understand what you mean