Arduino Forum Arduino digital IO pins numbering
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
  • State Suggested Answer
  • Replies 8 replies
  • Answers 5 answers
  • Subscribers 402 subscribers
  • Views 920 views
  • Users 0 members are here
Related

Arduino digital IO pins numbering

roineust
roineust over 9 years ago

Hello!

There is something about Arduino boards that i'm having trouble to understand.

 

Here is a description of the Arduino Uno:

https://www.arduino.cc/en/Main/ArduinoBoardUno

 

Here is a description of the Arduino Micro:

https://www.arduino.cc/en/Main/ArduinoBoardMicro

 

Under the Uno's technical specs table, it declares 14 digital IO pins and under the Micro's technical specs table it declares 20 digital IO pins.

 

Doesn't it mean that while the Uno has pinholes 0-13, under the Micro there should be pin-holes 0-19 ??

But yet, also under the Micro there are only pinholes 0-13..

 

This is confusing...can anyone please explain this to me?

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1 suggested
    These 2 boards use a different chip, as such they have different pinouts. the UNO has a 28 pin Plastic Dual Inline Package (PDIP) which is an ATMEGA328 and the Micro has a 44 pin chip (Quad Flatpack no…
  • beacon_dave
    beacon_dave over 9 years ago in reply to roineust +1 suggested
    This will probably be going to the other extreme but if need be you can get more info on the Atmel ATmega328 device here: ATmega328P The complete datasheet is around 600 pages however so expect to be skipping…
  • beacon_dave
    beacon_dave over 9 years ago in reply to roineust +1 suggested
    What sort of size are you actually hoping for ? Are you using PWM on your L293D enable line for motor speed control as the Uno / ATmega328 only has 6 PWM outputs whereas the Leonardo / ATmega32u4 has 7…
Parents
  • beacon_dave
    0 beacon_dave over 9 years ago

    Some of the pins are multi-functional.

     

    On the UNO you have the digital pins 0-13 however the analogue input pins 0-5 can also be configured for digital IO.

     

    On the Micro you have the digital pins 0-13 and analogue input pins 0-5, however in addition digital pins 4,6,8,9,10, & 12 can also be configured as analogue inputs.

     

    Perhaps think of it as 20 Digital IO pins of which 6 (UNO) or 12 (Micro) can be configured as analogue inputs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • roineust
    0 roineust over 9 years ago in reply to beacon_dave

    Not that you are to be blamed in any way Dave, of course you are only trying to help and thanks for that, but to me it sounds like not being clear enough on the part of Arduino, when selling to beginners level in prototyping like i am, to say a board has 20 IOD and not 14 IOD, while they actually mean it has 12 analog instead of 6...i could have use the Uno or Pro-mini which i already have and not buy a new Micro, if i had known that actually they have 20 IOD, just like the Micro has.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • roineust
    0 roineust over 9 years ago in reply to beacon_dave

    Not that you are to be blamed in any way Dave, of course you are only trying to help and thanks for that, but to me it sounds like not being clear enough on the part of Arduino, when selling to beginners level in prototyping like i am, to say a board has 20 IOD and not 14 IOD, while they actually mean it has 12 analog instead of 6...i could have use the Uno or Pro-mini which i already have and not buy a new Micro, if i had known that actually they have 20 IOD, just like the Micro has.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to roineust

    This will probably be going to the other extreme but if need be you can get more info on the Atmel ATmega328 device here:

    ATmega328P

     

    The complete datasheet is around 600 pages however so expect to be skipping over a few pages until you get more familiar. However it goes into a lot more detail about  the IO port configuration options.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer