Arduino Forum Arduino digital IO pins numbering
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
  • State Suggested Answer
  • Replies 8 replies
  • Answers 5 answers
  • Subscribers 402 subscribers
  • Views 916 views
  • Users 0 members are here
Related

Arduino digital IO pins numbering

roineust
roineust over 9 years ago

Hello!

There is something about Arduino boards that i'm having trouble to understand.

 

Here is a description of the Arduino Uno:

https://www.arduino.cc/en/Main/ArduinoBoardUno

 

Here is a description of the Arduino Micro:

https://www.arduino.cc/en/Main/ArduinoBoardMicro

 

Under the Uno's technical specs table, it declares 14 digital IO pins and under the Micro's technical specs table it declares 20 digital IO pins.

 

Doesn't it mean that while the Uno has pinholes 0-13, under the Micro there should be pin-holes 0-19 ??

But yet, also under the Micro there are only pinholes 0-13..

 

This is confusing...can anyone please explain this to me?

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1 suggested
    These 2 boards use a different chip, as such they have different pinouts. the UNO has a 28 pin Plastic Dual Inline Package (PDIP) which is an ATMEGA328 and the Micro has a 44 pin chip (Quad Flatpack no…
  • beacon_dave
    beacon_dave over 9 years ago in reply to roineust +1 suggested
    This will probably be going to the other extreme but if need be you can get more info on the Atmel ATmega328 device here: ATmega328P The complete datasheet is around 600 pages however so expect to be skipping…
  • beacon_dave
    beacon_dave over 9 years ago in reply to roineust +1 suggested
    What sort of size are you actually hoping for ? Are you using PWM on your L293D enable line for motor speed control as the Uno / ATmega328 only has 6 PWM outputs whereas the Leonardo / ATmega32u4 has 7…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    These 2 boards use a different chip, as such they have different pinouts. the UNO has a 28 pin Plastic Dual Inline Package (PDIP) which is an ATMEGA328 and the Micro has a 44 pin chip (Quad Flatpack no leads (QFN) which is the ATmega32U4

     

    the two chips also have different internal functionality, the ATmega32U4 having quite a bit more than the 328

     

    the Wiring based  IDE hides most of these details from you but does allow access to the common functionality through the commands like digitalWrite, digitalRead, AnalogRead etc.

    ATmega328

    image

     

    ATmega32U4

    image

    hope this answers your question

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • roineust
    0 roineust over 9 years ago in reply to Robert Peter Oakes

    Peter - your explanation is at a high level and too much for me to understand, can you please try to help me if possible, by answering the following question:

     

    i have on a robot i'm building, the following components:

     

    1. 2 X L293D chips, which turn 4 motors and require 9 outputs (the 9th is the enable pin on all sides of both L293D, which i made common to all 4 motors).

    2. 6 X servos which require 6 outputs.

    3. 1 X relay which turns another type of motor, which requires 1 output.

    4. 1 X bluetooth dongle, which requires RX and TX.

     

    This is all working well on an Arduino Mega - but now i need to put it all together in a much smaller box - so anything even close to the size of a Mega won't do.

     

    The question is: What would me the smallest Arduino board, which can handle the connections described above?

     

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to roineust

    What sort of size are you actually hoping for ?

     

    Are you using PWM on your L293D enable line for motor speed control as the Uno / ATmega328 only has 6 PWM outputs whereas the Leonardo / ATmega32u4 has 7 which could be crucial in your project.

     

    You could perhaps consider just using an Atmel microcontroller on its own to get the size down.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to roineust

    What sort of size are you actually hoping for ?

     

    Are you using PWM on your L293D enable line for motor speed control as the Uno / ATmega328 only has 6 PWM outputs whereas the Leonardo / ATmega32u4 has 7 which could be crucial in your project.

     

    You could perhaps consider just using an Atmel microcontroller on its own to get the size down.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to beacon_dave

    If you don't require the 7th PWM output for the L293D then you may be interested in the Adafruit Pro Trinket

    https://www.adafruit.com/product/2000

    It's like a miniature version of the UNO. You lose D2 & D7 but you gain A6 & A7.

     

    Size comparison between UNO, Pro Trinket and Trinket

    https://cdn-shop.adafruit.com/970x728/2000-10.jpg

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • roineust
    0 roineust over 9 years ago in reply to beacon_dave

    Interesting boards..actually i got a bunch of Arduino pro-mini, which might even comply to the project needs, if i will also use the analog IO. But since the pro-mini are more sensitive and tend to fry more easily, i'm trying the Arduino Micro.