Arduino
  • Products
  • More
Arduino
Arduino Forum potentiometer instead of rotary encoder
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 4 answers
  • Subscribers 420 subscribers
  • Views 4122 views
  • Users 0 members are here
  • help
  • digital
  • me
  • pulse
  • please
  • arduino
  • analog
Related

potentiometer instead of rotary encoder

tomstr21
tomstr21 over 10 years ago

Hello,

I have an project where i don't wanna use a rotary encoder because it has "unlimited" range of motion.

So i thought about using a potentiometer and somehow convert the analog input to digital pulse -what I mean: I need the range of pot to mean 170 pulses (if you would have a 170 ohm pot then 1ohm will be one pulse on the output)-if you're increasing the resistance it will pulse one pin and if you'll decrease it will pulse another pin-also it'll be awesome if you can change the "pulse range" with a dip switch (maybe something like 150-170-190).

I'm not programmer so I would be thankful for help.

 

 

Thanks,

Tomas Vostradovsky

  • Sign in to reply
  • Cancel

Top Replies

  • fvan
    fvan over 10 years ago +2 suggested
    Why not try the following: * take a 10k pot * use analogRead on the Arduino to read the value * divide the measured value by 6 (1024 / 170), giving you your pulse value Something like that ? int potentiometer_pin…
  • beacon_dave
    beacon_dave over 10 years ago in reply to tomstr21 +2 suggested
    Ok, go here and watch tutorials 1 to 4: Jeremy Blum Arduino Tutorials and you will no longer be a 'total noob' Tutorial 4 shows you how to check the current analogue value and do something with it, but…
  • beacon_dave
    beacon_dave over 10 years ago +1 suggested
    Perhaps take a look at this tutorial: https://www.arduino.cc/en/Tutorial/AnalogInOutSerial Connect the potentiometer wiper to the analogue input and then use the map() function to scale the range from…
Parents
  • fvan
    0 fvan over 10 years ago

    Why not try the following:

     

    * take a 10k pot

    * use analogRead on the Arduino to read the value

    * divide the measured value by 6 (1024 / 170), giving you your pulse value

     

    Something like that ?

     

    int potentiometer_pin = A0;
    int potentiometer_value = 0;
    int pulse_value = 0;
    
    void setup() {
    }
    
    void loop() {
      potentiometer_value = analogRead(potentiometer_pin);
      pulse_value = potentiometer_value / 6;
      
      delay(10);
    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • fvan
    0 fvan over 10 years ago

    Why not try the following:

     

    * take a 10k pot

    * use analogRead on the Arduino to read the value

    * divide the measured value by 6 (1024 / 170), giving you your pulse value

     

    Something like that ?

     

    int potentiometer_pin = A0;
    int potentiometer_value = 0;
    int pulse_value = 0;
    
    void setup() {
    }
    
    void loop() {
      potentiometer_value = analogRead(potentiometer_pin);
      pulse_value = potentiometer_value / 6;
      
      delay(10);
    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • tomstr21
    0 tomstr21 over 10 years ago in reply to fvan

    that's pretty much it but only thing that i don't see in that sketch is that I need to pulse two differrent pins -one if I'm increasing and one if I'm decreasing