Arduino Forum potentiometer instead of rotary encoder
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
  • State Suggested Answer
  • Replies 14 replies
  • Answers 4 answers
  • Subscribers 405 subscribers
  • Views 3457 views
  • Users 0 members are here
  • help
  • digital
  • me
  • pulse
  • please
  • arduino
  • analog
Related

potentiometer instead of rotary encoder

tomstr21
tomstr21 over 9 years ago

Hello,

I have an project where i don't wanna use a rotary encoder because it has "unlimited" range of motion.

So i thought about using a potentiometer and somehow convert the analog input to digital pulse -what I mean: I need the range of pot to mean 170 pulses (if you would have a 170 ohm pot then 1ohm will be one pulse on the output)-if you're increasing the resistance it will pulse one pin and if you'll decrease it will pulse another pin-also it'll be awesome if you can change the "pulse range" with a dip switch (maybe something like 150-170-190).

I'm not programmer so I would be thankful for help.

 

 

Thanks,

Tomas Vostradovsky

  • Sign in to reply
  • Cancel

Top Replies

  • fvan
    fvan over 9 years ago +2 suggested
    Why not try the following: * take a 10k pot * use analogRead on the Arduino to read the value * divide the measured value by 6 (1024 / 170), giving you your pulse value Something like that ? int potentiometer_pin…
  • beacon_dave
    beacon_dave over 9 years ago in reply to tomstr21 +2 suggested
    Ok, go here and watch tutorials 1 to 4: Jeremy Blum Arduino Tutorials and you will no longer be a 'total noob' Tutorial 4 shows you how to check the current analogue value and do something with it, but…
  • beacon_dave
    beacon_dave over 9 years ago +1 suggested
    Perhaps take a look at this tutorial: https://www.arduino.cc/en/Tutorial/AnalogInOutSerial Connect the potentiometer wiper to the analogue input and then use the map() function to scale the range from…
Parents
  • beacon_dave
    0 beacon_dave over 9 years ago

    Perhaps take a look at this tutorial:

    https://www.arduino.cc/en/Tutorial/AnalogInOutSerial

     

    Connect the potentiometer wiper to the analogue input and then use the map() function to scale the range from  0-1023 down to 0-170

     

    You can then use code to check whether the current input value from the pot is greater or less than the previous measured value and generate your pulses.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • beacon_dave
    0 beacon_dave over 9 years ago

    Perhaps take a look at this tutorial:

    https://www.arduino.cc/en/Tutorial/AnalogInOutSerial

     

    Connect the potentiometer wiper to the analogue input and then use the map() function to scale the range from  0-1023 down to 0-170

     

    You can then use code to check whether the current input value from the pot is greater or less than the previous measured value and generate your pulses.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • tomstr21
    0 tomstr21 over 9 years ago in reply to beacon_dave

    Great .. but I'm total noob so I don't know how to check the current value .. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to tomstr21

    Ok, go here and watch tutorials 1 to 4:

     

    Jeremy Blum Arduino Tutorials

     

    and you will no longer be a 'total noob'  image

     

    Tutorial 4 shows you how to check the current analogue value and do something with it, but it sounds like you will be better of starting at the beginning.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer