Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino connection help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 38 replies
  • Answers 11 answers
  • Subscribers 420 subscribers
  • Views 4476 views
  • Users 0 members are here
Related

Arduino connection help

alexparker2002
alexparker2002 over 9 years ago

I have made an integrated arduino monitoring system with 3 sensors....

I have used leds to show their values

But i want to add a lcd to it and an ethernet shield to it..... Is it possible?

Let me tell you that I am a beginner.....

Ive attached the schematics please modify it and tell me...... Please!!!!!!

Attachments:
imageFA5RM0AHX1W2JT3.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +2 suggested
    You should be able to do it but You will need to use a WS5100 type ethernet shield as it will offload some of the software to the hardware. It will plug into the Arduino UNO, it uses pins 10,11,12,13 you…
  • beacon_dave
    beacon_dave over 9 years ago in reply to beacon_dave +2 suggested
    Also perhaps be aware that the power rails on some breadboards are not continuous but instead are interrupted half way along. You may find that you need to place a jumper on your ground rail between block…
  • mcb1
    mcb1 over 9 years ago in reply to alexparker2002 +2 suggested
    alexparker2002 Part of learning is the LEARNING part. Having someone do all the work for you is not learning, but copying . I suggest you explore the examples that are provided in the Arduino IDE. There…
Parents
  • dwinhold
    0 dwinhold over 9 years ago

    Like everyone is saying, we are here to guide and help everyone, we were all beginners at one time. There are lots of great books out there as well as information on the internet, you said you are a beginner, start with something easier (a comfortable level for you) and work your way up. I find myself getting in over my head with the complexity of my project, what I do is set them aside until I have built up the knowledge to continue it. Some have been sitting for years but I haven't given up on them. As you see with the many responses and helpful information we are here to guide you in the right direction. It is more gratifying to complete the project with little help then to have it done for you. Start with the basics, not the top.

     

    Dale

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to dwinhold

    Can I use sensor shield to connect the sensors and lcd to arduino?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to alexparker2002

    Depends on a number of things such as the type of sensor shield, the type of sensors, the type of LCD etc.

    Perhaps if you can provide some information / links to the devices you are looking at ?

     

    Have you considered the likes of the Grove Starter Kit for Arduino ?

    https://www.seeedstudio.com/Grove-Starter-Kit-for-Arduino-p-1855.html

    Grove - Starter Kit v3 - Seeed Wiki

     

    It provides a base shield with connectors which makes it very easy for beginners to connect devices to.

    It comes with a 2-line LCD display

    Grove - LCD RGB Backlight - Seeed Wiki

    a LED module

    Grove - LED Socket Kit - Seeed Wiki

    a light sensor

    Grove - Light Sensor - Seeed Wiki

    and a temperature sensor module

    Grove - Temperature Sensor - Seeed Wiki

     

    You could then add a moisture sensor

    Grove - Moisture Sensor - Seeed Wiki

    and two more LED modules.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to beacon_dave

    Sensor Shield V5.0 sensor expansion board for arduino: Amazon.in: Electronics

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to beacon_dave

    Sensor Shield V5.0 sensor expansion board for arduino: Amazon.in: Electronics