Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino connection help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 38 replies
  • Answers 11 answers
  • Subscribers 419 subscribers
  • Views 4641 views
  • Users 0 members are here
Related

Arduino connection help

alexparker2002
alexparker2002 over 9 years ago

I have made an integrated arduino monitoring system with 3 sensors....

I have used leds to show their values

But i want to add a lcd to it and an ethernet shield to it..... Is it possible?

Let me tell you that I am a beginner.....

Ive attached the schematics please modify it and tell me...... Please!!!!!!

Attachments:
imageFA5RM0AHX1W2JT3.pdf
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +2 suggested
    You should be able to do it but You will need to use a WS5100 type ethernet shield as it will offload some of the software to the hardware. It will plug into the Arduino UNO, it uses pins 10,11,12,13 you…
  • beacon_dave
    beacon_dave over 9 years ago in reply to beacon_dave +2 suggested
    Also perhaps be aware that the power rails on some breadboards are not continuous but instead are interrupted half way along. You may find that you need to place a jumper on your ground rail between block…
  • mcb1
    mcb1 over 9 years ago in reply to alexparker2002 +2 suggested
    alexparker2002 Part of learning is the LEARNING part. Having someone do all the work for you is not learning, but copying . I suggest you explore the examples that are provided in the Arduino IDE. There…
  • clem57
    0 clem57 over 9 years ago

    The problem is the limited memory resources both SDRAM and flash. Have you looked at how much is currently used? You may want to approach this from another angle. If you tie in a Raspberry Pi 3, you can use UART to communicate and handle the higher level functions on the Pi 3 IMHO.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to clem57

    See.... In my schematics... Along with the leds i want to display the sensor values on a lcd screen... Is it possible?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to alexparker2002

    Possible if you look at the above comment

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    You should be able to do it but

     

    You will need to use a WS5100 type ethernet shield as it will offload some of the software to the hardware. It will plug into the Arduino UNO, it uses pins 10,11,12,13

    you will need to move the LEDs to other pins as the ethernet shield will use the ones your currently using

    you can get an LCD display that can use I2C interface (A4, A5) to display status etc. A 16x2 or a 20x4

     

    Memory will be tight but it is doable

     

    All libraries and hardware are plentiful, just search for "I2C arduino display", or "Arduino Ethernet Shield 5100" you will find plenty of info

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to Robert Peter Oakes

    Can you please give me a drawn schematic?

    Hand drawn or out of a computer?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to alexparker2002

    Perhaps take a look at this Arduino tutorial on LCD displays to get started:

    Tutorial 13 for Arduino: Liquid Crystal Displays

     

    If you want something more graphical then you could perhaps take a look at one of these type of displays:

    Resistive 4.3" GEMmodule

    which off-load the graphics processing onto the display module only requiring the data updates to be sent over a UART serial connection from the Arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to beacon_dave

    As for the Ethernet shield, have you taken a look at:

    https://www.arduino.cc/en/Guide/ArduinoEthernetShield

     

    Tom Igoe has written an interesting book called 'Making Things Talk' which covers this sort of area, so you may want to try and get hold of a copy. The 3rd edition is due to be published soon:

    https://www.amazon.co.uk/Making-Things-Talk-Sensors-Networks/dp/1680452150/ref=la_B001K8AUGU_1_5

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago

    Looking at your breadboard layout your analogue inputs don't look correct to me.

     

    Firstly it looks like you have misaligned the lower ground connection from the Arduino to the breadboard power rail in such a way that the 10k resistors are not tied to ground but just to each other.

     

    Secondly if the 10k resistors were tied to ground then your three analogue inputs would also all be tied to ground which would not be of much use.

     

    The photo resistor for example is normally set up as a potential divider circuit so your analogue input would be  taken from the midpoint between the resistor and the photo resistor as per this circuit:

    https://www.arduino.cc/en/Tutorial/AnalogInput

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to beacon_dave

    Also perhaps be aware that the power rails on some breadboards are not continuous but instead are interrupted half way along. You may find that you need to place a jumper on your ground rail between block 5 and block 6 to continue the ground rail to reach the 10k resistors. Alternatively move your ground wire from the Arduino two blocks to the right.

     

    The same may apply to your +5v rail at the top as it may not reach the components at the right hand side of the breadboard.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • alexparker2002
    0 alexparker2002 over 9 years ago in reply to beacon_dave

    Can u please give me a hand drawn schematic of the modified connections? Please give

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>