Arduino Forum Imported Arduino Project Not Working
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
  • State Suggested Answer
  • Replies 16 replies
  • Answers 8 answers
  • Subscribers 392 subscribers
  • Views 1396 views
  • Users 0 members are here
  • energia
  • tiva c
  • grideye
  • msp430
  • arduino
Related

Imported Arduino Project Not Working

kas.lewis
kas.lewis over 8 years ago

Hello,

 

I am attempting to run an Arduino project on on of my TI boards. I have a Maxim 1-Wire demo board that uses an Arduino for as its platform, not having one I decided to try a TI board. I load the required Libraries but I get an interesting issue. Even though there are two OneWire and I point it to the one I want to use it only finds some header files and not others. I have tried pointing to teh needed files with exact paths with no luck. To be sure I tried complaining teh same project in the Arduino IDE and there are no issues at all, include the needed libraries and it compiles. If someone could help explain what I am missing and why it finds some library files and not others that would be great.

 

Thanks

Kas

 

I know this is a repost but as I was unsure where to post it I have reposted it, If you could clarify the correct place I would be more than happy to remove any duplicate posts.

 

C:\Users\Kas\Desktop\energia-1.6.10E18\arduino-builder -dump-prefs -logger=machine -hardware "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware" -hardware "C:\Users\Kas\AppData\Local\Energia15\packages" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\tools-builder" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430" -tools "C:\Users\Kas\AppData\Local\Energia15\packages" -built-in-libraries "C:\Users\Kas\Desktop\energia-1.6.10E18\libraries" -libraries "C:\Users\Kas\Documents\Energia\libraries" -fqbn=energia:msp430:MSP-EXP430F5529LP -ide-version=10610 -build-path "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp" -warnings=default -prefs=build.warn_data_percentage=75 -verbose "C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_976722\MAXREFDES131_GUI_Firmware.ino"
C:\Users\Kas\Desktop\energia-1.6.10E18\arduino-builder -compile -logger=machine -hardware "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware" -hardware "C:\Users\Kas\AppData\Local\Energia15\packages" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\tools-builder" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430" -tools "C:\Users\Kas\AppData\Local\Energia15\packages" -built-in-libraries "C:\Users\Kas\Desktop\energia-1.6.10E18\libraries" -libraries "C:\Users\Kas\Documents\Energia\libraries" -fqbn=energia:msp430:MSP-EXP430F5529LP -ide-version=10610 -build-path "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp" -warnings=default -prefs=build.warn_data_percentage=75 -verbose "C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_976722\MAXREFDES131_GUI_Firmware.ino"
Using board 'MSP-EXP430F5529LP' from platform in folder: C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430
Using core 'msp430' from platform in folder: C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430
Detecting libraries used...
"C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
"C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
Generating function prototypes...
"C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\preproc\ctags_target_for_gcc_minus_e.cpp"
In file included from C:\Users\Kas\Documents\Energia\libraries\OneWire-master\src\OneWire.h:37:0,

                 from C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_976722\MAXREFDES131_GUI_Firmware.ino:40:

C:\Users\Kas\Documents\Energia\libraries\OneWire-master\src\/Masters/Masters.h:38:42: fatal error: Masters/DS248x/DS2484/DS2484.h: No such file or directory

compilation terminated.

exit status 1
Error compiling for board  MSP-EXP430F5529LPMSP-EXP430F5529LP

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +3 suggested
    Hi Kas, I reckon possibly what's going on is that the path should be DS248x/... in the #include if the #include is using double-quotes, otherwise it is expecting the folder path to have two 'Masters' folders…
  • balearicdynamics
    balearicdynamics over 8 years ago +1 suggested
    Hello Kas, I have used in past (and already I have it installed on my computer) both energia (developed by TI from the original Arduino IDE) and the original Arduino IDE. Please edit your post and set…
  • rsc
    rsc over 8 years ago +1 suggested
    There's a typo in this line "master\src\/Masters/Masters.h:38:42: fatal error:" look at "src\/" Scott
Parents
  • rsc
    0 rsc over 8 years ago

    There's a typo in this line

    "master\src\/Masters/Masters.h:38:42: fatal error:"

    look at "src\/"

    Scott

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 8 years ago in reply to rsc

    Hello Scott, Enrico and Shabaz

     

    It appears the issue is based on the file system and how file locations are referenced. After directly referencing the header files and getting some of them to work I end up with the output below. More specifically the warning on line 14. I would still like to try get a bit further and the only way I can see that happening is to rename the library and place it with all the other libraries. The issue I am unsure of is 1) how to rename a library (but I'm sure I can look this up) 2) how do I ensure that by renaming a library I don't mess up all links within it (other #include that may point to it. If there are pointers to help with issue #2 I would be happy to hear them.

     

    Thanks for the help so far

    Kas

     

     

    C:\Users\Kas\Desktop\energia-1.6.10E18\arduino-builder -dump-prefs -logger=machine -hardware "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware" -hardware "C:\Users\Kas\AppData\Local\Energia15\packages" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\tools-builder" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430" -tools "C:\Users\Kas\AppData\Local\Energia15\packages" -built-in-libraries "C:\Users\Kas\Desktop\energia-1.6.10E18\libraries" -libraries "C:\Users\Kas\Documents\Energia\libraries" -fqbn=energia:msp430:MSP-EXP430F5529LP -ide-version=10610 -build-path "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp" -warnings=default -prefs=build.warn_data_percentage=75 -verbose "C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_726814\MAXREFDES131_GUI_Firmware.ino"
    C:\Users\Kas\Desktop\energia-1.6.10E18\arduino-builder -compile -logger=machine -hardware "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware" -hardware "C:\Users\Kas\AppData\Local\Energia15\packages" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\tools-builder" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430" -tools "C:\Users\Kas\AppData\Local\Energia15\packages" -built-in-libraries "C:\Users\Kas\Desktop\energia-1.6.10E18\libraries" -libraries "C:\Users\Kas\Documents\Energia\libraries" -fqbn=energia:msp430:MSP-EXP430F5529LP -ide-version=10610 -build-path "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp" -warnings=default -prefs=build.warn_data_percentage=75 -verbose "C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_726814\MAXREFDES131_GUI_Firmware.ino"
    Using board 'MSP-EXP430F5529LP' from platform in folder: C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430
    Using core 'msp430' from platform in folder: C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430
    Detecting libraries used...
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src\API_Level_1\grideye_api_lv1.c" -o "nul"
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src\API_Level_2\grideye_api_lv2.c" -o "nul"
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src\OWGridEye.cpp" -o "nul"
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
    WARNING: library OWGridEye-master claims to run on [avr] architecture(s) and may be incompatible with your current board which runs on [msp430] architecture(s).
    Generating function prototypes...
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\preproc\ctags_target_for_gcc_minus_e.cpp"
    In file included from C:\Users\Kas\Downloads\RoadTest\OneWire-master\OneWire-master\src\Slaves\Bridges\DS28E17\DS28E17.h:38:0,
    
    
                     from C:\Users\Kas\Downloads\RoadTest\OneWire-master\OneWire-master\src\Slaves\Bridges\Bridges.h:37,
    
    
                     from C:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src/OWGridEye.h:38,
    
    
                     from C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_726814\MAXREFDES131_GUI_Firmware.ino:42:
    
    
    C:\Users\Kas\Downloads\RoadTest\OneWire-master\OneWire-master\src\Slaves\OneWireSlave.h:38:25: fatal error: RomId/RomId.h: No such file or directory
    
    
    compilation terminated.
    
    
    Using library OWGridEye-master at version 1.0.0 in folder: C:\Users\Kas\Documents\Energia\libraries\OWGridEye-master 
    exit status 1
    Error compiling for board  MSP-EXP430F5529LP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • kas.lewis
    0 kas.lewis over 8 years ago in reply to rsc

    Hello Scott, Enrico and Shabaz

     

    It appears the issue is based on the file system and how file locations are referenced. After directly referencing the header files and getting some of them to work I end up with the output below. More specifically the warning on line 14. I would still like to try get a bit further and the only way I can see that happening is to rename the library and place it with all the other libraries. The issue I am unsure of is 1) how to rename a library (but I'm sure I can look this up) 2) how do I ensure that by renaming a library I don't mess up all links within it (other #include that may point to it. If there are pointers to help with issue #2 I would be happy to hear them.

     

    Thanks for the help so far

    Kas

     

     

    C:\Users\Kas\Desktop\energia-1.6.10E18\arduino-builder -dump-prefs -logger=machine -hardware "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware" -hardware "C:\Users\Kas\AppData\Local\Energia15\packages" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\tools-builder" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430" -tools "C:\Users\Kas\AppData\Local\Energia15\packages" -built-in-libraries "C:\Users\Kas\Desktop\energia-1.6.10E18\libraries" -libraries "C:\Users\Kas\Documents\Energia\libraries" -fqbn=energia:msp430:MSP-EXP430F5529LP -ide-version=10610 -build-path "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp" -warnings=default -prefs=build.warn_data_percentage=75 -verbose "C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_726814\MAXREFDES131_GUI_Firmware.ino"
    C:\Users\Kas\Desktop\energia-1.6.10E18\arduino-builder -compile -logger=machine -hardware "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware" -hardware "C:\Users\Kas\AppData\Local\Energia15\packages" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\tools-builder" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430" -tools "C:\Users\Kas\AppData\Local\Energia15\packages" -built-in-libraries "C:\Users\Kas\Desktop\energia-1.6.10E18\libraries" -libraries "C:\Users\Kas\Documents\Energia\libraries" -fqbn=energia:msp430:MSP-EXP430F5529LP -ide-version=10610 -build-path "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp" -warnings=default -prefs=build.warn_data_percentage=75 -verbose "C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_726814\MAXREFDES131_GUI_Firmware.ino"
    Using board 'MSP-EXP430F5529LP' from platform in folder: C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430
    Using core 'msp430' from platform in folder: C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430
    Detecting libraries used...
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src\API_Level_1\grideye_api_lv1.c" -o "nul"
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src\API_Level_2\grideye_api_lv2.c" -o "nul"
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src\OWGridEye.cpp" -o "nul"
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
    WARNING: library OWGridEye-master claims to run on [avr] architecture(s) and may be incompatible with your current board which runs on [msp430] architecture(s).
    Generating function prototypes...
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "-IC:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\preproc\ctags_target_for_gcc_minus_e.cpp"
    In file included from C:\Users\Kas\Downloads\RoadTest\OneWire-master\OneWire-master\src\Slaves\Bridges\DS28E17\DS28E17.h:38:0,
    
    
                     from C:\Users\Kas\Downloads\RoadTest\OneWire-master\OneWire-master\src\Slaves\Bridges\Bridges.h:37,
    
    
                     from C:\Users\Kas\Documents\Energia\libraries\OWGridEye-master\src/OWGridEye.h:38,
    
    
                     from C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_726814\MAXREFDES131_GUI_Firmware.ino:42:
    
    
    C:\Users\Kas\Downloads\RoadTest\OneWire-master\OneWire-master\src\Slaves\OneWireSlave.h:38:25: fatal error: RomId/RomId.h: No such file or directory
    
    
    compilation terminated.
    
    
    Using library OWGridEye-master at version 1.0.0 in folder: C:\Users\Kas\Documents\Energia\libraries\OWGridEye-master 
    exit status 1
    Error compiling for board  MSP-EXP430F5529LP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 8 years ago in reply to kas.lewis

    Hi Kas,

     

    It sounds like it is moving further, but there seem to be a couple of issues. One of them, the 'RomId.h not found' issue might have a similar solution as the earlier one, if there is some #include that uses '<>' instead of double-quotes. However, the other problem is more worrisome, because it states that some pre-compiled library is for AVR architecture. It means that either the source code is not present, or (more likely and more hopefully) that the source code is present but the make system didn't think it needed building.

    If the former (source code not present) then that is fairly unsolvable without finding where that code came from. If the latter, then there are two scenarios. The first is that you just need to remove (e.g. rename it temporarily) the library built for AVR, or select 'make clean' if you can find it anywhere in the settings (no idea if this is possible with Energia, but hopefully it is). The other scenario (worse) is that there is no makefile and then that is quite hard to figure out how to build the library.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer