Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Uno circuit fault finding
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 4 answers
  • Subscribers 416 subscribers
  • Views 2325 views
  • Users 0 members are here
  • lcd
  • keypad
  • digital code lock
  • uno
  • newbie
  • question
Related

Uno circuit fault finding

Fevvahz
Fevvahz over 9 years ago

Hi, i'm new to Arduino, and I'm having a few issues with my first project.  I decided to try and recreate the Digital Code Lock project posted on Digital Digest.  I'm struggling with configuring the circuit itself.

 

I've successfully uploaded the code to the Uno, but there's a few issues;

 

-the buzzer sounds constantly.

- the LCD display doesn't power up

 

I've tried to lay the circuit out in a way that's straightforward to follow, but as I say, i'm pretty new to this.  I found the circuit diagram hard to follow, as some of the connections shown differed slightly with my hardware (I tried to get as close to what the original poster listed as possible), especially the keypad.  I suspect I've connected it up wrong, or put a component the wrong way round.  I've dont some fault finding with my multi meter, and power seems to be getting to the components.

 

I've attached some images.  Can anyone tell me firstly if it looks like I've connected it up wrong?

 

Message was edited by: Chris Swann - pictures added.

Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 9 years ago +4 suggested
    Fevvahz wrote: -the buzzer sounds constantly. It looks from the pictures that you may have 3.3V permanently applied over the buzzer. If you follow the connection of the 3V3 and GND signals from the Arduino…
  • Fevvahz
    Fevvahz over 9 years ago +3 suggested
    Well the beer flowed, and was welcome. Now, its time to conclude my tale.... Firstly, I had the jumpers from outputs 8,9,10 and 11 on the Arduino to the pins 12, 13, 14 and 15 respectively, instead of…
  • gadget.iom
    gadget.iom over 9 years ago +2 suggested
    Hello Fevvahz I cannot see the images you attached. If you could post them on here I'll take a look at the circuit for you. Paul
Parents
  • Fevvahz
    0 Fevvahz over 9 years ago

    So thanks to your guidance, I ordered some female 0.1 headers, 220 ohm resistors, and took another look at the wiring diagram.  I also tested the LCD display using a spare Uno I now have, using the adafruit tutorial here and can confirm that it does indeed work.  After a little soldering, I think I'm nearly there.

     

    image

    image

     

    The problem I have at the moment is that the LCD display doesn't display text at all, but it does light up its backlight for a second or so.  I had previously successfully  the sketch, and it appears that the keypad etc is working.  If I type in four digits, the buzzer sounds, as if its an incorrect code, and the LCD backlight lights up breifly, but still no text.

     

    So in the adafruit tutorial I used a variable resistor, which I used to adjust until the LCD displayed correctly.  Do you think that this could be the issue causing the screen not to work?

     

    image

    image

     

    [EDIT] Images uploaded.

     

    rachaelp gadget.iom @

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Fevvahz
    0 Fevvahz over 9 years ago

    So thanks to your guidance, I ordered some female 0.1 headers, 220 ohm resistors, and took another look at the wiring diagram.  I also tested the LCD display using a spare Uno I now have, using the adafruit tutorial here and can confirm that it does indeed work.  After a little soldering, I think I'm nearly there.

     

    image

    image

     

    The problem I have at the moment is that the LCD display doesn't display text at all, but it does light up its backlight for a second or so.  I had previously successfully  the sketch, and it appears that the keypad etc is working.  If I type in four digits, the buzzer sounds, as if its an incorrect code, and the LCD backlight lights up breifly, but still no text.

     

    So in the adafruit tutorial I used a variable resistor, which I used to adjust until the LCD displayed correctly.  Do you think that this could be the issue causing the screen not to work?

     

    image

    image

     

    [EDIT] Images uploaded.

     

    rachaelp gadget.iom @