Arduino Forum Using 40 low frequency Mics.
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
  • State Suggested Answer
  • Replies 21 replies
  • Answers 12 answers
  • Subscribers 404 subscribers
  • Views 2820 views
  • Users 0 members are here
Related

Using 40 low frequency Mics.

noblemaster
noblemaster over 8 years ago

Hi,

I am working on a device that takes input from 40 microphones and send data to PC via Arduino.

I want to use low frequency microphones (5Hz onwards) with around 200-250Hz sampling for each mic.

 

For this purpose, my preliminary design is like this...

    40 Mics --> 40 PreAmp circuits --> Mux Shield II --> Arduino DUE --> PC

 

Please suggest me suitable commercial available preAmp circuits and any suggestion on the design is most welcome.

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago in reply to noblemaster +2 suggested
    Your answer suggests you are willing to spend over $1000 per channel to get the best possible. If that is not true, the description needs to be more complete in order to get a helpful answer.
  • michaelkellett
    michaelkellett over 8 years ago in reply to noblemaster +2 suggested
    To measure at up to 100Hz you need to sample each microphone at 500Hz or faster. For each microphone you will need a a buffer amplifier as shown on the Invensys data sheet and an anti-aliasing low pass…
  • rachaelp
    rachaelp over 8 years ago in reply to DAB +2 suggested
    DAB is right, the USB on the Arduino is serial over USB, i.e. it just shows up as a serial port on the PC and you'll probably be maxed out at 115200 baud (I may be wrong here but you should look into it…
Parents
  • rachaelp
    0 rachaelp over 8 years ago

    Most commercial mic pre circuits I believe have DC blocking caps so they are suitable for use with phantom powered mics. As such they have an inherent roll off at low frequencies so you'll be struggling to get a decent level through most sensibly priced ones at 5Hz. There are some exceedingly expensive options such as http://www.studiocare.com/summit-ecs-410-everest-channel-strip.html which are fairly flat down to 5Hz but for your 40 mics it'll set you back nearly £30k..... Given that your design uses an Arduino, I am thinking this is not the price budget you're aiming at....

     

    I think you might be better off designing your own 40-input mic preamp (or a single one 40 times or something in between) which work for your specific requirements. Speaking of which, if you could expand on those with more details (i.e. a little more than "As much as possible") and maybe give some background for your specific application then people might be able to help you more easily.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • noblemaster
    0 noblemaster over 8 years ago in reply to rachaelp

    I am interested in measuring vibrations in 5Hz to 100Hz band and then analysis in MATLAB.. Mic model ICS40300. Signal is good with DC offset at 0.8V and max output at around 1.2V.

    I am using Arduino DUE, it has 12 bit ADC. I have few options in mind...

     

    1. https://www.sparkfun.com/products/9816

    What if I change its input cap at both stages from 1uF to 4.7uF?

     

    2. https://www.sparkfun.com/products/9868

    What if I replace its microphone with my desired model and change its input cap to 27uF?

     

    Which option is better from above two? or something else is required?

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • WarrenW
    0 WarrenW over 8 years ago in reply to noblemaster

    Hi Noble.

    When calculating the low frequency cut off 3dB point you can do some simple maths of 1/(2 x Pi x Freq x Capacitor) to give the reactance and given the 10Kohm input on the 9816 module your reactance would need to be the same for a simple -3dB point (1/2 the amplitude). It's a simple voltage divider at that point.

    The 1uF gives about 33Kohm at 5hz.

    A 4.7uF would be approx. 6Kohm so should be able to amplify you 5 Hz with 'some' reduction in amplitude from the original waveform. DAB suggested superimposing a 1Khz 'carrier' and then filtering this which is a logical solution if you are going to MUX the inputs as the MUX rate will alter you LF waveforms.

     

    Now we take the MIC into account - whoa - it has a 3dB point of 6Hz! That will mean your levels will already be skewed. I hope you are not looking to analyse on amplitude and hope you are analysing freq only (i.e. presence of frequency not how loud).

     

    After about 10Hz things should flatten off.

    Hope this helps.

    Warren.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to noblemaster

    To measure at up to 100Hz you need to sample each microphone at  500Hz or faster. For each microphone you will need a a buffer amplifier as shown on the Invensys data sheet and an anti-aliasing low pass filter which must allow the 100Hz signal thought but reduce the gain by, for example, 60 dB at 400 Hz. This requires 30dB per octave which is a fifth order filter. You could then sample at 800Hz and have no aliasing problems. To sample each of your 40 inputs at this rate is quite feasible but will need a sampling rate of 800 x 40 = 32000 samples per second at the processor. You might find it easier to sample faster and have a  more relaxed spec for the anti-alias filter.

    I don't know of  a commercial pre-amp that would do this - it will need to be custom made - I could do it for you (for money) or else I'm happy to advise you about how to set about it publicly on E14.

    I wouldn't use an Arduino for this - you'll need a custom board anyway so i would go for a processor with plenty of on chip RAM and number crunching.

     

    A board with 40 channels would be quite big - might be simpler to split it over a few boards.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • noblemaster
    0 noblemaster over 8 years ago in reply to michaelkellett

    Thanks a lot for the detailed answer. Actually my input is concentrated below 50Hz and there is no/minimum frequency expectation (i mean not a powerful shoot) above 100 Hz therefore I am not considering anti-alias filter right now.

     

     

    That is why I am only concerned with lower cuttoff.

    In this manner... What do you suggest? Shall I go with just changing capacitor? or any thing else is required to make it compatible with ICS-40300 mic?

    I am thinking to modify this board --> https://www.sparkfun.com/products/9868 by changing mic model and input capacitor upto 27uF....

     

     

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to noblemaster

    If you are using  a microphone then you pretty much HAVE to have an anti alias filter - if you don't then any sound at frequencies above half the sampling rate is converted into signals within the same band as the wanted signals. Unless your application has some feature that ensures unwanted sounds never reach the microphone you will need the filter. Can you tell us  a bit more about the application.

     

    The Sparkfun board could be modified as you suggest.

     

    How far from the multiplexer will the microphones be ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • noblemaster
    0 noblemaster over 8 years ago in reply to michaelkellett

    Yes the environment I am working does filter sound for me.

    I am planning to put mics with around 6inch wired connected to preamp which will be nearly connected to Mux Shield II which will be near to Arduino Due from where data will be fed by serial communication USB to PC. So you can say all setup is placed side-by-side.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • noblemaster
    0 noblemaster over 8 years ago in reply to michaelkellett

    Yes the environment I am working does filter sound for me.

    I am planning to put mics with around 6inch wired connected to preamp which will be nearly connected to Mux Shield II which will be near to Arduino Due from where data will be fed by serial communication USB to PC. So you can say all setup is placed side-by-side.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • DAB
    0 DAB over 8 years ago in reply to noblemaster

    I am not sure the USB can handle the amount of data you can collect from 40 microphones.

    Are you going to do any preprocessing before you send the data, or just send up the raw data?

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • noblemaster
    0 noblemaster over 8 years ago in reply to DAB

    No Sir... I am not doing any preprocessing except preamp. All the processing will be done on recorded data in PC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 8 years ago in reply to DAB

    DAB is right, the USB on the Arduino is serial over USB, i.e. it just shows up as a serial port on the PC and you'll probably be maxed out at 115200 baud (I may be wrong here but you should look into it to make sure before you build everything up). So assuming this is the maximum you can get and you are doing 12-bit sampling so you'll need to spread this over two serial words then with 7 bits, no parity and 1 stop bit you are at 18 bits per sample (two serial words) which is 6400 samples per second maximum which leads to a maximum sample rate of 160 samples per second per microphone which is well short of the 200-250Hz sample rate you were looking for.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • noblemaster
    0 noblemaster over 8 years ago in reply to rachaelp

    I've tested Arduino Due, working good at  624000 Baud over USB. I hope it will be quite good for me. What do you say?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 8 years ago in reply to noblemaster

    Noble M wrote:

     

    I've tested Arduino Due, working good at 624000 Baud over USB. I hope it will be quite good for me. What do you say?

    Ok that sounds promising then. Have you tested it with large continuous data streams to ensure that you don't get any dropped/garbled data if anything doesn't quite sync up right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • noblemaster
    0 noblemaster over 8 years ago in reply to rachaelp

    I did like this... connected 1 Mic and read 40 times in a 5milisecond-loop for a duration of about 5seconds. I applied 2-3 thumb-press signals during recording. Printed 40 results on the same line and sent to PC with this huge baud after every 40 recorded samples. Initial thought was that if all goes well then all 40 recordings will be same.

     

    Analysed 40 time series recordings and calculated correlation coefficients that were 0.99-0.999... So i feel that I've got pretty much success.

    What do you say?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 8 years ago in reply to noblemaster

    I was thinking more along the lines of sending a known data set at rate which is utilizing a reasonable percentage of the link bandwidth, e.g. a counting value or a PRBS sequence incrementing at a set rate and send this over an extended period of time with something on the other end monitoring what it receives continuously and counting errors. I'd set this up and run it for hours or days to be sure something wasn't going to go wrong occasionally.

     

    But at the end of the day it depends on what your application is doing and whether you can tolerate the occasional error once in a while and deal with / recover from it as to whether its worth the effort to validate the data link any further, it might not be so if you are happy with the validation you've done so far then that's great as then it looks like you should have enough bandwidth for what you are trying to do.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer