Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Detecting OFF state of an AC Load
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 36 replies
  • Answers 19 answers
  • Subscribers 418 subscribers
  • Views 6180 views
  • Users 0 members are here
Related

Detecting OFF state of an AC Load

anishkgt
anishkgt over 8 years ago

Hi All,

 

I am trying to switch on a LOAD from its OFF state by detecting a change in the voltage. Here the load is a MOT, the voltage at the primary is 1VAC when OFF.

 

My idea is to switch ON the MOT by detecting the voltage change at the primary when the Secondary are shorted. I can see a voltage drop of .5VAC when shorted. How can i monitor this voltage change with an Arduino.

 

My solution to the problem is shown below.

image

The Live of mains is connected to the MOT through the LIVE_LOAD in the schematic. During the OFF state the Optocoupler is triggered so that the 1VAC is seen by the Precision rectifier LT1078 and is rectified and send to the Analog pin A0 on the Arduino. With a code i could detect the voltage change and use it trigger the MOT again and at the same disable the optocoupler to break the circuit to the LT1078. Basically eliminating the need to press a switch two switch ON the MOT.

 

is there a better way to get this done. I was thinking of using the basic 1N4007 to convert the 1VAC to dc but that would be a problem when the MOT is switched ON allowing the mains 240VAC to flow through the DIODE.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago in reply to anishkgt +4 suggested
    1.3 V rms rectified is 1.8 Vdc minus the drop in a lightly loaded Schottky diode of 0.3 V is 1.5 V dc peak. The zener on the Schottky diode output is just to clamp the signal so it doesn't exceed your…
  • shabaz
    shabaz over 8 years ago in reply to anishkgt +4
    Electrodes? Important information like this is kind of missing in your question.. If you provide half the information, it's not a surprise that it wasn't understandable.
  • shabaz
    shabaz over 8 years ago +3 suggested
    The question (and the circuit) is not understandable I think : ( Could you rephrase the question, or draw a block diagram? The circuit doesn't make sense.
Parents
  • dougw
    0 dougw over 8 years ago

    Obviously you need to be careful connecting directly to 220V and presumably you have the high voltage implications figured out and how to connect the low voltage supply - as in the whole circuit and its power supply needs to be enclosed with no possibility of human contact.

    You can limit the high voltage on the sense line with a zener diode, if you don't want to disconnect it.

    A Schottky diode is enough to rectify the sense signal, followed by an RC filter.

    The current limiting resistor can be higher than 100K.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 8 years ago

    Obviously you need to be careful connecting directly to 220V and presumably you have the high voltage implications figured out and how to connect the low voltage supply - as in the whole circuit and its power supply needs to be enclosed with no possibility of human contact.

    You can limit the high voltage on the sense line with a zener diode, if you don't want to disconnect it.

    A Schottky diode is enough to rectify the sense signal, followed by an RC filter.

    The current limiting resistor can be higher than 100K.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • anishkgt
    0 anishkgt over 8 years ago in reply to dougw

    dougw  wrote:

     

    Obviously you need to be careful connecting directly to 220V and presumably you have the high voltage implications figured out and how to connect the low voltage supply - as in the whole circuit and its power supply needs to be enclosed with no possibility of human contact.

    You can limit the high voltage on the sense line with a zener diode, if you don't want to disconnect it.

    A Schottky diode is enough to rectify the sense signal, followed by an RC filter.

    The current limiting resistor can be higher than 100K.

    Thanks for the concern. yes am well cautious about the mains supply and working with them.

     

    The least nominal voltage for a zerner diode is 1.8v which is quite high for the application. The OFF state voltage is only about 1.3vac max and i presume they are to be placed in series with the LIVE_OUT. A schottky would have a voltage drop as well.

     

    I guess the initial design would be ideal as the voltage drop across the diode is also compensated and being an opamp with slew rate of 0.1v/us i should get quick response as well. I could omit the capacitor as that would take time to charge during voltage variation and maybe the diode as well to cut cost or may be both. All i need is to monitor ANY change in the voltage so without the diode and the cap they should be ok.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to anishkgt

    1.3 V rms rectified is 1.8 Vdc minus the drop in a lightly loaded Schottky diode of 0.3 V is 1.5 V dc peak.

    The zener on the Schottky diode output is just to clamp the signal so it doesn't exceed your arduino power supply when the ac voltage goes to 220. You could use 1N4007's for this if you want - just 2 in series clamps the voltage to 1.4 volts dc.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • anishkgt
    0 anishkgt over 8 years ago in reply to dougw

    can you please show me a schematic of it.