Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Detecting OFF state of an AC Load
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 36 replies
  • Answers 19 answers
  • Subscribers 418 subscribers
  • Views 6180 views
  • Users 0 members are here
Related

Detecting OFF state of an AC Load

anishkgt
anishkgt over 8 years ago

Hi All,

 

I am trying to switch on a LOAD from its OFF state by detecting a change in the voltage. Here the load is a MOT, the voltage at the primary is 1VAC when OFF.

 

My idea is to switch ON the MOT by detecting the voltage change at the primary when the Secondary are shorted. I can see a voltage drop of .5VAC when shorted. How can i monitor this voltage change with an Arduino.

 

My solution to the problem is shown below.

image

The Live of mains is connected to the MOT through the LIVE_LOAD in the schematic. During the OFF state the Optocoupler is triggered so that the 1VAC is seen by the Precision rectifier LT1078 and is rectified and send to the Analog pin A0 on the Arduino. With a code i could detect the voltage change and use it trigger the MOT again and at the same disable the optocoupler to break the circuit to the LT1078. Basically eliminating the need to press a switch two switch ON the MOT.

 

is there a better way to get this done. I was thinking of using the basic 1N4007 to convert the 1VAC to dc but that would be a problem when the MOT is switched ON allowing the mains 240VAC to flow through the DIODE.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago in reply to anishkgt +4 suggested
    1.3 V rms rectified is 1.8 Vdc minus the drop in a lightly loaded Schottky diode of 0.3 V is 1.5 V dc peak. The zener on the Schottky diode output is just to clamp the signal so it doesn't exceed your…
  • shabaz
    shabaz over 8 years ago in reply to anishkgt +4
    Electrodes? Important information like this is kind of missing in your question.. If you provide half the information, it's not a surprise that it wasn't understandable.
  • shabaz
    shabaz over 8 years ago +3 suggested
    The question (and the circuit) is not understandable I think : ( Could you rephrase the question, or draw a block diagram? The circuit doesn't make sense.
Parents
  • mcb1
    0 mcb1 over 8 years ago

    I think the question that everyone is stepping over is :-

    What is the voltage at the Live_Out pin when the MOT is turned ON.?

     

     

    As drawn I can't see how this schematic will provide what you want. (As I understand it)

    The detection circuit (LT1078) can't do any detecting until the Opto-coupler is turned ON by the CS_Enable line being driven High.

     

    It seems to me that you should be detecting the full AC voltage across the MOT and doing your signalling based on that.

    If you're trying to detect a shorted secondary, then measuring the primary current may be a better option.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 8 years ago

    I think the question that everyone is stepping over is :-

    What is the voltage at the Live_Out pin when the MOT is turned ON.?

     

     

    As drawn I can't see how this schematic will provide what you want. (As I understand it)

    The detection circuit (LT1078) can't do any detecting until the Opto-coupler is turned ON by the CS_Enable line being driven High.

     

    It seems to me that you should be detecting the full AC voltage across the MOT and doing your signalling based on that.

    If you're trying to detect a shorted secondary, then measuring the primary current may be a better option.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • anishkgt
    0 anishkgt over 8 years ago in reply to mcb1

    I am sensing the voltage at the primary of the MOT when it is OFF not when the MOT is ON. The actual voltage of 1vac is the leakage current from the SCR from which the MOT is connected to.

     

    When i said "shorted secondary" i meant  as in placing the electrodes on a conducting surface like nickel strips for spot welding.

     

    here is the schematic to better understand

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to anishkgt

    Electrodes? Important information like this is kind of missing in your question..

    If you provide half the information, it's not a surprise that it wasn't understandable.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to anishkgt

    here is the schematic to better understand

    That provides much more information thanks.

     

    I'm still wondering why you need to detect the OFF state when you obviously have the opposite ie ON.

     

    They are a very interesting OptoCoupler.

    MOC3052SR2M OPTOCOUPLER TRIAC OUT 6-SMD Fairchild Optoelectronics Group datasheet pdf data sheet FREE from datasheetz.co…

     

    There is a delay between the LED and the Triac turning OFF, which if not handled correctly, could result in a voltage larger than expected at R36.

     

     

    If you're trying to somehow control the current to the spot welder then there has to be some better methods.

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • anishkgt
    0 anishkgt over 8 years ago in reply to mcb1

    Thanks mark, am already aware of those optocouplers and one of them is used in the schematic as well.

     

    I'll try to explain the whole idea behind this,

     

    Lets assume we have a push button switch to switch ON the spot welder. We press it and that switches ON the MOT and we spot weld nickel tabs to 18650 cells. All looks good and Hunky-Dorey. image  Now lets say you have to build a battery pack of 300 cells and pressing the switch 300 times or a foot switch would be........a little uncomfortable or your legs get exhausted while pressing the pedal 300 times to spot weld those cells.

     

    Here we are replacing the 'SWITCH' by sensing when both electrodes makes a contacts on the nickel tabs. When it does current is drawn from the MOT and that draw will show a voltage drop at the primary and that voltage-drop is something that am trying to sense which would fed into an Arduino to activate the MOT.

     

     

    Hope that's clear. Sorry am not very good at explaining things but i guess would have helped you understand the idea.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to anishkgt

    pressing the switch 300 times or a foot switch would be........a little uncomfortable

    Ah yes that does make sense now.

     

    Sometimes having to explain what you're doing can help with a path towards a solution.

     

     

     

    So to give you an alternative option. ....

    Some of the generators use a small DC current on the output side to detect when the load is connected and ON.

    It then fires up the generator.

     

    You could adopt something similar ..ie detect the cell (or load) and then apply the mains.

     

     

     

    The last time I used a spot welder was way back at school.

    The welding arms were sprung loaded and once it had applied clamping force to hold the pieces together, continued pressure on the handle applied the power.

    Obviously there is some mechanical force clamping the two pieces together, which you can't avoid.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer